Linux Embedded Challenge ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Embedded Challenge Knowledge Base

ディスカッション

ソート順:
In acest video se poate observa cum extragem un cod ISBN de pe coperta unei carti.Am folosit un program si anume,zbar-tools. Am verificat ca ISBN-ul este extras cum trebuie,prin faptul ca ne-a afisat in browser, pagina de pe goodreads cu cartea de pe coperta careia l-am extras .
記事全体を表示
we have implemented a web interface from where the user can: send  a hexadecimal code (the code must begin with "0x") to the board send a code and a date/time that will be scheduled get into learning mode and input names for the codes that will be received by the board
記事全体を表示
Am prezentat in video-ul atasat planul proiectului in linii mari,conexiunea intre udoo si computer, udoo si camera video, conexiunea la wifi si utilizarea VNC-ului.
記事全体を表示
We described the web interface and its functionality.
記事全体を表示
We connected udoo to wireless Installed apache  We added some buttons to control the movement of the robot We had to put the web server on port 81 because we had some issues with apache and port 80
記事全体を表示
Am imbunatatit partea de transmisie seriala pentru a putea trimite si Ack inapoi la server-ul de python pentru a verifica ca datele au fost primite de catre partea de arduino. Am implementat scrierea de semnale PWM pe ESC-uri pentru a putea controla motoarele Am construit drona pentru a putea testa toate componentele si controlul motoarelor Am folosit Neo.Gpio pentru a lua datele de la senzori si a le avea pe server-ul python
記事全体を表示
For this milestone we implemented a program that retrieves video stream from the USB camera using Python. The video illustrates the functionality: the user is connecting to the device and the video stream captured is shown to the laptop.
記事全体を表示
A video showing the first few features of our Adaptive Headlights project. So far, we put together: power on/off buttons LEDs for the low beams, high beams and side lights servos for the high beams When the angle at which the wheel is tilted is greater than a certain threshold, the side lights are turned on progressively, in order to improve vision of the incoming portion of road. When the angle is lower than said threshold, the high beams adapt their position to follow the road.
記事全体を表示
   Realizarea primului milestone presupune realizarea interfetei web, care sa contina atat butoane pentru controlul robotului, cat si o fereastra de feedback de la acesta. Interfata este structurata astfel incat sa contina blocuri pentru: - status-ul de conectare; - live streaming; - feedback de la robot; - controlul robotului de la distanta.    Pentru realizarea interfetei si a comuncarii dintre interfata si Arduino, au fost necesare urmatoarele fisiere: - server.py (programul aflat in acest fisier este responsabil pentru crearea webserver-ului); - serialworker.py; - main.js; - index.html; - css.css; - serial2ws.ino.  
記事全体を表示
On the last milestone we already had a car controlled from the computer. For this milestone we made some tweaks for both the car and the app. For the car we added an extra driver(to not lose power when using both motors at the same time) and finally, batteries. The app controls the car similarly to a video game with the WASD key and there is also an interactive meter to update the speed. The app also has the option of enabling cruise control which moves the car at a constant speed, indicated by the meter.
記事全体を表示
Am uploadat un scurt demo ce cuprinde o descrierea a: - algoritmului folosit. - modul de functionare.
記事全体を表示
In acest filmulet prezentam indeplinirea sarcinilor corespunzatoare primei etape: conectarea senzorilor la placa UDOO.citirea senzorilor(temperatura, umiditate, altitudine, presiune atmosferica si intensitate luminoasa) si afisarea datelor in terminalul Linux. De asemenea, se poate observa ca folosim si un LED care semnalizeaza nivelul de lumina(se aprinde atunci cand nivelul intensitatii scade sub o anumita valoare). Prima parte a filmuletului prezinta realizarea conexiunilor cu placa . Toti senzorii sunt alimentati de la 3.3V conform specificatiilor pentru functionare optima din foile lor de catalog. Totodata, aceasta tensiune este sub pragul de 3.3V ceea ce protejeaza porturile de intrare ale placutei. Conexiunea fizica UDOO - calculator a fost realizata prin USB iar pentru a avea acces la terminal s-a folosit VNC + Putty In partea doua a doua a filmuletului se observa afisarea in consola a datelor citite de la senzori, iar ultima parte reprezinta un bonus prin care dorim sa semnalizam scaderea intensitatii luminoase sub un anumit prag prin aprinderea unei lumini, in cazul de fata un LED.
記事全体を表示
In video este aratat codul pentru recunoasterea unui obiect (cu ajutorul librariilor openCV) dupa o culoare HSV, setata prin slide-urile de range. Dupa ce obiectul este bine delimitat de culoare (rezultatul filtrarii se afla in fereastra Thresholded Image), acesta este identificat si urmarit (punctul de tinta, langa coordonate) in imaginea originala.
記事全体を表示
We connect the camera to the board and wrote a program that detects the text from a picture in order to prove that we decode the information transmitted to the camera. The camera isn't active all the time. In order to power on or off the camera we use the gyroscope sensor (bassicaly we shrink a little the board). 
記事全体を表示
Am pus initial 2 senzori de miscare cu leduri care se aprind cand detecteaza miscarea ,dupa ce am compilat codul doar unul din senzori a mers ,detecta miscare ,avea o latenta de 8 secunde, timp in care ledul se aprindea intermitent , dupa care se stingea atunci cand nu detecta miscare . din pacate am intampinat o problema dupa ce am facut aceasta prima proba si nu am mai putut uploada cod pe placuta .  urmeaza sa mai adaugam 3 senzori unul de miscare unul ultrasonic si unul de lumina . 
記事全体を表示
Stocarea retetelor de bauturi care contin ingredientele si timpul de functionare a pompei pentru fiecare ingredient. Programul permite momentan doar alegerea unei bauturi din lista.
記事全体を表示