LPC Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Microcontrollers Knowledge Base

Discussions

Sort by:
This content was originally contributed to lpcware.com by Brewster LaMacchia   This project shows how to take the filter coefficients created by MDS' QEDesign filter design package and use them for real time audio filtering using the floating point DSP capability of the LPC4350. It's designed to run on the Hitex board and uses the UDA1380 for analog stereo I/O. It also uses the touch buttons, COG LCD, and LEDs for controlling operation.   Keil's Logic Analyzer tool was used for performance measurement. For full details see \doc\gen\html\index.html after unzipping the download.   Updated 16-Mar-12 to correct output rolloff in the UDA1380 due to the deemphasis filter being on by mistake.   Original Attachment has been moved to: MyProj.zip
View full article
This document describes how to create a new LPC project using LPCOpen v2.xx, LPCXpresso v8.2.2 and LPC11U24 LPCXpresso board. In addition describes how to create 2 simple example codes. Blinking LED. Set the LED using a push bottom.  LPCOpen LPCOpen is an extensive collection of free software libraries (drivers and middleware) and example programs that enable developers to create multifunctional products based on LPC microcontrollers. After install LPCXpresso, the LPCOpen packages for supported board(s)/device(s) can be found at the path: <install_path>\lpcxpresso\Examples\LPCOpen > This directory contains a number of LPCOpen software bundles for use with the LPCXpresso IDE and a variety of development boards. Note that LPCOpen bundles are periodically updated, and additional bundles are released. Thus we would always recommend checking the LPCOpen pages to ensure that you are using the latest versions. This example was created using the LPC11U24 LPCXpresso board in this case the drivers selected is lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip Importing libraries In order to create a new project, it is necessary to first import the LPCOpen Chip Library for the device used and optionally the LPCOpen Board Library Project. For do that it is necessary to follow these steps: 1. Click on Import project(s). 2. Select the examples archive file to import. In this case, the projects imported are contained within archives .zip.  3. For this example the LPC11U14 LPCXpresso board is selected. Click Open. Then click Next 4. Select only the LPCOpen Chip Library and LPCOpen Board Library Project. Click Finish. The same steps are required for any LPC device and board you are used. Creating a new LPC project.   The steps to create a new LPC project are described below: 1. In Quickstar Panel, click "New project"   2. Choose a wizard for your MCU. In this case LPC1100/LPC1200 -> LPC11Uxx -> LPCOpen-C Project This option will link the C project to LPCOpen. Then click Next.   3. Select the Project name and click Next.   4. Select the device used (LPC11U24 for this case) and click Next.   5. Select the LPCOpen Chip Library and LPCOpen Board Library, these projects must be present in the workspace.   6. You can set the following option as default clicking Next, then click Finish.   7. At this point, a new project was created. This project has a src (source) folder, the src folder contains: cr_startup_lpc11uxx.c: This is the LPC11Uxx Microcontroller Startup code for use with LPCXpresso IDE. crp.c: Source file to create CRP word expected by LPCXpresso IDE linker. sysinit.c: Common SystemInit function for LPC11xx chips. <name of project> my_first_example: This file contains the main code.     8. LPCXpresso creates a simple C project where it is reading the clock settings and update the system core clock variable, initialized the board and set the LED to the state of "On". 9. At this point you should be able to build and debug this project.   Writing my first project using LPCXpresso, LPCOpen and LPC11U24.   This section describes how to create 2 simple example codes. Blinking LED. Set the LED using a push bottom. The LPCOpen Chip Library (in this case lpc_chip_11uxx_lib) contains the drivers for some LPC peripherals. For these examples, we will use the GPIO Driver. The LPCOpen Board Library Project (in this case nxp_lpcxpresso_11u14_board_lib) contains files with software API functions that provide some simple abstracted functions used across multiple LPCOpen board examples. The board_api.h contains common board definitions that are shared across boards and devices. All of these functions do not need to be implemented for a specific board, but if they are implemented, they should use this API standard.   After create a new project using LPCXpresso and LPCOpen, it is created a simple C project where it is initialized the board and set the LED to the state of "On" using the Board_LED_Set function.   int main(void) {   #if defined (__USE_LPCOPEN)     // Read clock settings and update SystemCoreClock variable     SystemCoreClockUpdate(); #if !defined(NO_BOARD_LIB)     // Set up and initialize all required blocks and     // functions related to the board hardware     Board_Init();     // Set the LED to the state of "On"     Board_LED_Set(0, true); #endif #endif       // TODO: insert code here       // Force the counter to be placed into memory     volatile static int i = 0 ;     // Enter an infinite loop, just incrementing a counter     while(1) {         i++ ;     }     return 0 ; }       a. Blinking LED. In board_api.h file there is an API function that toggle the LED void Board_LED_Toggle(uint8_t LEDNumber);  LEDNumber parameter is the LED number to change the state. The number of the LED for the LPCXpresso LPC11U24 is 0. It is easy to create a delay function using FOR loops. For example: void Delay (unsigned int ms) {         volatile static int x,y;           while (ms)         {                 for (x=0; x<=140; x++)                 {                         y++;                 }                 ms--;         } } In order to have the LED blinking, it is necessary to call these functions in an infinite loop. while(1) {                 Board_LED_Toggle(0);                 Delay (10000);         } Complete code (Blinking LED). int main(void) { #if defined (__USE_LPCOPEN)         // Read clock settings and update SystemCoreClock variable         SystemCoreClockUpdate(); #if !defined(NO_BOARD_LIB)         // Set up and initialize all required blocks and         // functions related to the board hardware         Board_Init();         // Set the LED to the state of "On"         Board_LED_Set(0, true); #endif #endif          while(1) {                 Board_LED_Toggle(0);                 Delay (10000);         }         return 0 ; }  void Delay (unsigned int ms) {         volatile static int x,y;         while (ms)         {                 for (x=0; x<=140; x++)                 {                         y++;                 }                 ms--;         } }      b. Set the LED using a push bottom. For this example it is necessary to configure a pin as input.  The gpio_11xx_1.h file contains all the function definitions for the GPIO Driver. The example uses the pin 16 of port 0 to connect the push bottom. The function Chip_GPIO_SetPinDIRInput(LPC_GPIO_T *pGPIO, uint8_t port, uint8_t pin) sets the GPIO direction for a single GPIO pin to an input. In order to configure the Port 0, pin 16 as input we can use this function: Chip_GPIO_SetPinDIRInput(LPC_GPIO, 0, 16); Then, it is necessary to check the status of this pin to turn-on/turn-off the LED. The function Chip_GPIO_GetPinState(LPC_GPIO_T *pGPIO, uint8_t port, uint8_t pin) gets a GPIO pin state via the GPIO byte register. This function returns true if the GPIO is high, false if low. State_Input=  Chip_GPIO_GetPinState (LPC_GPIO, 0, 16);   Complete code (Set the LED using a push bottom). int main(void) {         bool State_Input;   #if defined (__USE_LPCOPEN)     // Read clock settings and update SystemCoreClock variable     SystemCoreClockUpdate(); #if !defined(NO_BOARD_LIB)     // Set up and initialize all required blocks and     // functions related to the board hardware     Board_Init();     Chip_GPIO_SetPinDIRInput(LPC_GPIO, 0, 16);     // Set the LED to the state of "On"     Board_LED_Set(0, false);  #endif  #endif      while(1) {           State_Input=  Chip_GPIO_GetPinState (LPC_GPIO, 0, 16);              if (State_Input==0){                 Board_LED_Set(0, true);             }             else {                 Board_LED_Set(0, false);             }     }     return 0 ; }   I hope this helps!! Regards Soledad
View full article
This content was originally contributed to lpcware.com by Jerry Durand When I found the M4 core in the LPC43xx series could be used as a hardware Floating Point Unit (FPU) while the actual code ran in the M0 core, I immediately thought of an application; a stand-alone 4-axis CNC control box for use with table-top milling machines.  Currently these machines are almost exclusively controlled by software running on very old PC hardware that has a parallel port and either MS-DOS or Windows XP for an operating system. Control of these milling machines entails tasks such as receiving g-code commands in ASCII text and a large amount of high-precision floating point operations which calls for an FPU.  This all has to occur rapidly and continously as each of the 4 motors has to be updated thousands of times per second. It seemed the M0 core would excel at the basic input/output (I/O) and timing functions while using the M4 as an FPU would speed the floating point operations. I originally hoped to port the entire RS274NGC open source Enhanced Machine Controller (EMC) software to the LPC4350 and run it with and without the FPU enabled, comparing the time to process a sample g-code file.  Problems getting the development software and examples set up caused me to run short of time even though NXP was fairly fast to fix problems as they were found.  Instead I modified one of the example programs (GPIO_LedBlinky) to enable testing the performance and this turned out to have some interesting results I might have otherwise missed. I ran the test code in eight different configurations:      1. FPU disabled, 32-bit float multiplication      2. FPU enabled, 32-bit float multiplication      3. FPUdisabled, 64-bit double multiplication      4. FPU enabled, 64-bit double multiplication      5. FPU disabled, 32-bit float division      6. FPU enabled, 32-bit float division      7. FPUdisabled, 64-bit double division      8. FPU enabled, 64-bit double division All tests were run from internal SRAM so external memory access time would not distort the results.  The optimization level was left at the default of zero (0) as I had problems with the compiler eliding parts of my code if I tried higher levels. Test results (loops per second averaged over 10 seconds):      1. 990,550        float, *      2. 2,768,000        FPU, float, *      3. 284,455        double, *      4. 276,796        FPU, double, *      5. 282,316        float, /      6. 1,894,000        FPU, float, /      7. 85,762        double, /      8. 85,053        FPU, double, / As expected 32-bit floating point operations run a lot faster with the FPU, 2.79 times faster for multiply and 6.7 times faster for division.  I would have expected somewhat better performance but this is still a significant improvement in speed. The 64-bit floating point operations were a different story, for both multiplication and division the operations ran SLOWER with the FPU than they do without it.  This points to an error in the library functions since it should be no worse than equal.  I was very surprised by this result and hope when the problem is fixed the 64-bit operations improve significantly. In conclusion the low cost of these parts and the simplicity of using the FPU allows performance improvement to an existing product that uses 32-bit floating point operations.  There is no long development cycle or fear of breaking something in your code as the changes to use the FPU consist of adding a small initilization routine for the FPU and enabling it in your compiler options.  This also leaves open the option of an even greater improvement with no hardware changes once you've had time to port your critical code to run directly on the M4 core instead of just using it as an FPU. In the case of 64-bit floating point operations, it seems this may not be the best choice if you only use the M4 as an FPU.  Running your critical code directly on the M4 may give a significant improvement but that requires porting the code to run on both cores and isn't something I tested.
View full article
This content was originally contributed to lpcware.com by Massimo Manca Example application for the "LPC4300 Getting started Kit" to learn and to use the multi processor communication and the newest peripherals of LPC43xx MCU family. System resources used and assignment to the cores: The Cortex-M4 core handles the application logic, manages the 4 touch keys and 4 leds (via the PCA9502 I2C 8 bit I7O expander), the lcd display and the real time clock. The Cortex-M0 core is dedicated to the printer management using the RS232 on board interface (in near future SCT and SGPIO will be used to interface a thermal printing head). The cores communicates using inter processor communication mechanisms minimizing the data passed from M4 to M0 and providing a simple security mechanism.
View full article
This content was originally contributed to lpcware.com by Cam Thompson This project is a simple data logging example that takes readings from various sensors, and log the information to a web page. The Cortex-M4 is used to collect and process sample data, and the Cortex-M0 is used to run a web server for supplying data to web clients. This allows data to be viewed on any web browser, including portable devices such as smart phones and tablets. The web data logging example was implemented using the Hitex LPC4300 evaluation board, which has all the necessary components. The LPC43xx has a built-in ethernet controller accessible by either core, and the Hitex evaluation board provides the physical layer. An on-board 128x32 pixel Chip-on-Glass (COG) LCD display, four touch sensors, and several LEDs are used for implementing a simple user interface. The LPC43xx contains a Real-Time Clock (RTC) which is used to record the date and time of data samples.
View full article
This content was originally contributed to lpcware.com by Richard Man This project demonstrates how easy it is to port a commonly used open source FatFS code to the LPC4350 using SDIO and built-in SDMMC support. In the competitive embedded microcontroller market, one way a silicon vendor can differentiate its offerings from the rest is by integrating higher-function peripherals onchip. As such, it is no longer unusual to find chips with built-in LCD, USB, CAN, Ethernet, and in some instances, even hardware support for the SD/MMC memory devices. Such is the case with the NXP LPC4350. With two ARM Cortex cores and many other features, it also sports SD/MMC hardware. Without dedicated SD/MMC support, the firmware typically must use bit banging code which is timing sensitive and adds to the complexity of the code.
View full article
This content was originally contributed to lpcware.com by Dirceu Rodrigues Introduction My work evaluating the SCT peripheral with the Hitex LPC4350 board (ARM Cortex-M4/M0) included the generation of non standard PWM signals for use in Power Electronics. At the end, some results would be compared with solutions based on LPC1114 (Cortex-M0), for example.  The first idea was to apply a concept that I had used when developing universal controllers for laser printer fuser, at 2001. This is a gate drive for MOSFET / IGBT isolated by pulse transformers. Two pulses Gate Drive – LPC1114 solution The circuit is implemented with pulse transformers (20 kHz PWM frequency) using the gate-source capacitance as memory. A Schottky diode avoids the stored charge to leak through windings. Thus, it's possible to achieve duty-cycles near to 0 and 100 %, simply applying 1 µs pulses shifted in time - one for charge, other for discharge. A very simplified schematic is shown in Figure 1.       Figure 1. Simplified circuit. My solution for the LPC1114 - Cortex-M0, uses two timers in a different scheme: Phase-out or lead/lag the counter values. With CT32B0 and CT32B1 32 bit timers, the behavior, including the pulsed outputs, is better understood looking on Figures 2 and 3 for duty-cycles of 75% and 25%. As opposed to common solutions, for each timer, the MR0 and MR1 matching registers values are constant. The difference between them is equivalent to pulse width (1 µs). The MR0 value also defines the period. The duty-cycle it’s determined through the expression:   DC = TC1 / MR0                                   (1) Where, TC1 is the CT32B1 timer value when this one, for the CT32B0, is zero.      In order to change the duty-cycle, the code in foreground task establishes a new TC1 and enables the CT32B0 overflow interrupt, where  this value is effectively loaded on CT32B1 timer in a safe point (to avoid jitter and other dangerous edges on outputs). Also, the CT32B0 ISR disables itself at the end, ensuring low interrupt overhead. For safety, the first applied pulse is a “discharge pulse”. This solution was proven driving a 930 W (120V/8.7 A) single-phase induction motor and it can be seen in reference [1], using a synchronous AC version of circuit shown in Figure 1 (no diode, four mosfets).      Figure 2. LPC1114 Two Pulses Gate Drive solution - DC 75%.  Figure 3. LPC1114 Two Pulses Gate Drive solution - DC 25%.      Two pulses Gate Drive – LPC4350 SCT solution The equivalent SCT implementation for the Two Pulses Gate Driver has the advantage of saving one timer. The pulse generation can be accomplished through a Mealy finite state machine plus the companion SCT counter. The LPC4350 generates 1 µs pulses with repetition rate of 20 kHz on CTOUT_4 and CTOUT_5 outputs. Two pushbuttons allow that a falling edge on CTIN_2 input, start the timer and a low value on CTIN_6, stop it. The counter operates as a unified 32 bit timer (UNIFY = 1) counting up and down (BIDIR = 1). ADC0 input is used to read the voltage on R26 potentiometer. So, the firmware can convert it in PWM change. As for LPC1114, the LPC4350 core and SCT runs in 48 MHz. Register MATCH 0 defines half-period. The difference between MATCH 2 and MATCH 1 registers is equivalent to pulse width (1 µs). In other words: PULSE_WIDTH = MATCH 2 - MATCH 1                       (2) Despite this difference be constant, now the MATCH 2 and MATCH 1 contents must change at the same time. Figures 4 and 5 show the waveforms for duty-cycles 15 % and 85 %. For example, the duty-cycle can be determined through the expression: DC = 1 – (MATCH 1 + 0.5*PULSE_WIDTH )/ MATCH 0        (3) Figure 4. SCT Two Pulses Gate Drive solution - DC 15%. Note: In companion source code, the PULSE_WIDTH is referred as PULSE_LENGTH. Figure 5. SCT Two Pulses Gate Drive solution – DC 85%. In order to achieve this behavior, one simple Finite State Machine with two states has been defined (Table 1): STATE Meaning 0 CTOUT_4 pulse generation 1 CTOUT_5 pulse generation Table 1. Definition of states. Figure 6 illustrates the relationship between the counter, states and interrupts. The PWM updating scheme takes advantage of following SCT property (as stated on User Manual): “A MATCH register is loaded from the corresponding MATCHREL register when BIDIR is 1 and the counter reaches 0”. In this application, the ADC0 interrupts MCU in a 24 Hz rate, triggered by TIMER0 MR0 (EM0 rising edge). The code on this ISR determines the new MATCH 1, saves it on global variable match1 and enables the SCT interrupt associated with event “counter reach limit” - in fact, event for MATCH 0. Here note, as stated in expression (3), that DC depends only on MATCH1, since MATCH 0 is constant. The ISR code for MATCH 0 event, updates MATCHREL 1 and MATCHREL 2 registers based on variable match1. Also disables the associated interrupt for low overhead. When counter reaches 0, the MATCH 1, 2 registers will be reloaded from the MATCHREL 1, 2 values automatically. This procedure should avoid jitter and other dangerous edges on outputs. Note that MATCH registers are never handled by software when counter is running. The new desired values are indirectly loaded on MATCHREL registers. The first values for MATCH registers are intentionally unreachable (> MATCH 0). This ensures that only ADC readings brought useful values to them. The on board potentiometer generates a voltage from 0 V to 3.3 V, which translates to 0 – 1023 range by the 10 bit AD converter. The MIN_MATCH1 and MAX_MATCH1 predefined values equates to 36 and 1116 (equivalent to duty-cycle 5 % and 95 % DC). Therefore, the software relates ADC0 voltage to with match1 variable approximately through the expression: match1 = [(MAX_MATCH1 - MIN_MATCH1)*ADC0] / 1024 +            (4)                                                  MIN_MATCH1 Note: In the companion source code, the division by 1024 is performed with a 10 bit right shift.           Figure 6. PWM updating scheme - DC 50%. Table 2 lists the eight states comprising the state machine for the current application. The companion state transition diagram is showed on Figure 7. Here, note other SCT important property, as stated on User’s Manual: “If more than one event associated with the same counter occurs in a given clock cycle, only the state change specified for the highest-numbered event among them takes place”. This applies to events 6 and 7. In normal operation, the event 6 happens periodically in State 1; but when a pushbutton press causes a low level on CTIN_6, the event 7 is fired on State 1 and counter is stopped. The state is driven to 0, with the outputs cleared (until one falling edge on CTIN_2 initiates the counting). EVENT ID Happens in state Conditions Actions 0 0 Falling edge on CTIN_2 Start counter 1 0 Counter reach MATCH 1 when counting up Set CTOUT_4 (pulse rise) 2 0 Counter reach MATCH 2 when counting up Clear CTOUT_4 (pulse fall) 3 0 Counter reach MATCH 0 Limit counter (defines the half period) Int. to update MATCHREL 1/ 2 Change to STATE 1 4 1 Counter reach MATCH 2 when counting down Set CTOUT_5 (pulse rise) 5 1 Counter reach MATCH 1 when counting down Clear CTOUT_5 (pulse fall) 6 1 Counter reach MATCH 3 (0) MATCH 1/ 2 automatic reloading Change to STATE 0 7 1 Counter reach MATCH 3 (0) AND Low value on CTIN_6 Stop counter MATCH 1/ 2 automatic reloading Change to STATE 0 Table 2. Definition of states. Figure 7. State transition diagram. Conclusion The PWM generation carried out by two short pulses shifted in time is a good alternative when isolation and duty-cycles far from 50% are required - specially driving gate charge devices like Mosfet/IGBT. The main advantage over opto-isolated implementations is not necessary create an auxiliary power supply.  Regarding to the architecture, the designer can use microcontrollers equipped with UP/DOWN timers (bidirectional), but is required some external glue logic in order to generate those short pulses. In comparison with the LPC1114 presented solution, the SCT version consumes just one timer/counter. As shown, the SCT peripheral is very independent, resulting in low (or no) MCU intervention after an initial configuration. This simple application used only two inputs, two outputs, two states and eight events. For more complex designs, the SCT provides up to 8 inputs, 16 outputs, 16 events and 32 states. I’ve future plans to make other power electronics applications based on SCT, including a small dot matrix printer controller. Code Red company   provides a tool to draw state diagrams and automatically generate code for the SCT engine, called Red State [2] (not used in this application). Finally, I would like to thank David Donley from NXP, who assisted me by answering my technical enquiries about the State Configurable Timer and suggesting improvements on code. References     [1]    http://www.youtube.com/DirceuRodriguesJr     [2]    http://www.code-red-tech.com/lpcxpresso
View full article
This content was originally contributed to lpcware.com by Steve Sabram This example project implements acoustic range, finite infinite response (FIR) filters using the LPC4350 demo board and the ARM CMSIS DSP library. A sound resource of a science fiction “zap gun” plays out the headphone jack of the demo board. This sound sample is great for demonstration since it has many low-, mid-, and high-frequency components along the acoustical band. You play the sound resource by touching the capacitive touch buttons on the demo board as explained by the menu shown on the demo board’s LCD. It is best to listen to the sound with a headphone or ear buds. Each of the four buttons plays the same sound resource differently: 1)  Raw – The unprocessed sound plays according to its format (sample rate of 44.1 kHz, 16-bit sample and mono sound). 2)  Low Pass – filtered through a low pass, Butterworth filter with a cutoff of 5 kHz, similar to the bandwidth of a common analog telephone. When played, notice that high pitch components are removed similar       to the sound heard over a telephone. 3)  High Pass – filtered through a high pass, Butterworth filter with a low frequency cutoff of 8 kHz. Notice that the sound is lower in volume since only the upper harmonic components are played. 4)  Backward Mask – The sound resource sample plays in reverse order. The “Zap!” is now a “Zoup!” The digital filters were designed with a favorite public domain tool, WinFilter (http://www.winfilter.20m.com/)       accompanying this example. With exposure of this free DSP design tool via NXP, I hope its author expands its features.
View full article
The following document contains a list of documents, questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in LPC or MCUXpresso you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table  FAQ: MCUXpresso Software and Tools  How to create a new LPC project using LPCOpen and MCUXpresso IDE  Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  Using the MCUXpresso Pins Tool   MCUXpresso Config Tools is now available!   LPC55xx Multicore Applications with MCUXpresso IDE  LPC information LPC5460x MCU Family Overview  USB with NXP Microcontrollers LWIP memory requirements  LPC800 Four-Part Webinar Series!  The LPC804 Programmable Logic Unit (PLU)   LPC84x Technical Training - Now Available Guides and Examples Flashing and Installing the new firmware and drivers for LPC11U35 debug probes  Enabling debug output  USB FLASH download, programming, and security tool (DFUSec)  DMA Ping-Pong application  Getting start with LPCXpresso54608 &amp; emWin Graphics;  Capacitive Touch example using the LPC845 Breakout Board  OLED Display Application Example using LPC845 Breakout Board and SPI  Mixed-Signal Logic Analyzer &amp; Oscilloscope (Lab Tool) Solution  LPC FAQ How to calculate the value of crystal load capacitors? Can I send a message with X/Y/Z bits in the ID?  What is the difference between error active and error passive? What is the sample point for?  How can I verify the configured CAN bitrate, using an oscilloscope? 
View full article
This content was originally contributed to lpcware.com by Jack Ganssle In this project I looked at the relative performance of the LPC4350's M4 vs. M0 cores, emulating ARM's big.LITTLE approach. In the last few years the industry has increasingly embraced the notion of using multiple processors, often in the form of multicore. Though symmetric multiprocessing – the use of two or more identical cores – has received a lot of media attention, many embedded systems are making use of heterogeneous cores. A recent example is ARM’s big.LITTLE approach, which is specifically targeted to smart phones. A big Cortex-A15 processor does the heavy lifting, but when computational demands are slight it goes to sleep and a more power-frugal A7 runs identical code. NXP’s LPC43xx also has two ARM cores: a capable Cortex-M4 and a smaller M0. Since power constraints are hardly novel to phones, my question was: “if we mirror the big.LITTLE philosophy, what is the difference in performance between the M4 and the M0?”
View full article