No .wsd file generated by KSDK Project Generator for FRDMK82F board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No .wsd file generated by KSDK Project Generator for FRDMK82F board

2,468件の閲覧回数
shivamgautam
Contributor I

I was trying to generate project for my frdmk82f board using the KSDK Project Generator (Basic). I've selected the SDK location, Selected my board and then clicked Generate. It Generates the folder but under kds folder there is no myProject.wsd file generated which I can import to Kinetis Design Studio. Please Help.

ラベル(1)
4 返答(返信)

2,140件の閲覧回数
enriqueolivieri
Contributor I

I have the same problem. I use KSDK Project Generator 2.2 and doesn't generate the .wsd

0 件の賞賛
返信

2,140件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi,
Actually .wsd file is not needed to import KDS project.

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

Hope this helps

Jorge Alcala

2,140件の閲覧回数
enriqueolivieri
Contributor I

jorge_a_vazquez escribió:

Hi,
Actually .wsd file is not needed to import KDS project.

 

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

 

Hope this helps

Jorge Alcala

Thank You for your help

0 件の賞賛
返信

2,140件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Shivam,

yes, you are absolutely right.

I can confirm the same behavior on my side.

For KDS the .wsd file was not generated.

Thank you for pointing out this bug!

I already reported to Project Generator team. PGKSDK-343

I will keep you informed.

Best Regards,

Iva

0 件の賞賛
返信