No .wsd file generated by KSDK Project Generator for FRDMK82F board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No .wsd file generated by KSDK Project Generator for FRDMK82F board

1,729 次查看
shivamgautam
Contributor I

I was trying to generate project for my frdmk82f board using the KSDK Project Generator (Basic). I've selected the SDK location, Selected my board and then clicked Generate. It Generates the folder but under kds folder there is no myProject.wsd file generated which I can import to Kinetis Design Studio. Please Help.

标签 (1)
4 回复数

1,401 次查看
enriqueolivieri
Contributor I

I have the same problem. I use KSDK Project Generator 2.2 and doesn't generate the .wsd

0 项奖励
回复

1,401 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi,
Actually .wsd file is not needed to import KDS project.

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

Hope this helps

Jorge Alcala

1,401 次查看
enriqueolivieri
Contributor I

jorge_a_vazquez escribió:

Hi,
Actually .wsd file is not needed to import KDS project.

 

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

 

Hope this helps

Jorge Alcala

Thank You for your help

0 项奖励
回复

1,401 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Shivam,

yes, you are absolutely right.

I can confirm the same behavior on my side.

For KDS the .wsd file was not generated.

Thank you for pointing out this bug!

I already reported to Project Generator team. PGKSDK-343

I will keep you informed.

Best Regards,

Iva

0 项奖励
回复