Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
The document describes how to port yaffs2 file system for MQX. The detailed porting user guide can refer to the attached doc which use TWR-K70F120M as example. The reference code can be found in the attached source code package. Now, the yaffs2 for MQX can support NFC and non-NFC at the same time, the only difference is NAND driver. For NFC, you should use NFC driver and for non-NFC, you should use softnand driver. In yaffs2 porting package, include the files which should be modified in MQX release package. user_config.h should be placed at \config\platform name\ init_nandflash.c should be placed at \mqx\source\bsp\platform name\ \nandflash is the NAND driver, should be at \mqx\source\io\ \yaffs2 is the yaffs2 porting codes should be at the root directory of MQX release package softnand2K.c is the NAND driver for non-NFC(simulated by flexbus).
View full article
The following file contains example code for usage of ADC, UART, DAC, GPIO, I2C, interrupts, MCG and timers for the k53 platform. Regards.
View full article
General Purpose Input/Output module presented by Jose Maria Casillas, Freescale TIC. Module explanation and alternative pin´s functions. Short explanation on the Bit Manipulation Engine (BME). Hands-On: LED RGB. Push Button. Módulo GPIO (General Purpose I/O) presentado por Jose María Casillas, Freescale TIC. Explicar el modulo y las funciones alternativas de los pines. Breve descripción del Bit Manipulation Engine (BME). Hands-On: LED RGB. Push Button.
View full article
The Multipurpose Clock Generator module explained by Ali Piña, Freescale TIC. MCG Module Explanation Connection Diagram Operation Modes Hands On Toggle a LED in FEI (FLL engaged Internal) switch to PEE (PLL Engaged External). Watch changes. Switch from different operation modes. El Módulo de MCG (Multipurpose Clock Generator) presentado por Ali Piña, Freescale TIC. Explicación del Modulo MCG. Diagrama de conexiones Modos de operación. Hands-On Togglear un LED en modo FEI (FLL engaged Internal) y cambiar a PEE(PLL Engaged External). Observar cambios. Moverse entre varios modos de operación
View full article
      The MKW01Z device is highly-integrated, cost-effective, smart radio, sub-1 GHz wireless node solution composed of a transceiver supporting FSK, GFSK, MSK, or OOK modulations with a low-power ARM® Cortex M0+ CPU. The highly integrated RF transceiver operates over a wide frequency range including 315 MHz, 433 MHz, 470 MHz, 868 MHz, 915MHz, 928 MHz, and 955 MHz in the license-free Industrial, Scientific and Medical (ISM) frequency bands. This configuration allows users to minimize the use of external components.      The MPXY8600 is a sensor for use in applications that monitor tire pressure and temperature. It contains the pressure and temperature sensors, an X-axis and a Z-axis accelerometer, a microcontroller, an LF receiver and an RF transmitter all within a single package.        This setup offer customers to utilize Freescale MPXY8600/8700 as transmitter and MKW01 as receiver to form 315MHz, 433.92MHz TPMS transmitter and receiver  total solution.
View full article
To do: The development platform is Eclipse. The EVAL Board is the Kinetis Tower TWR K60. On the Tower, you find 2 pushbuttons and 4 LEDs. a) Generate a hexadecimal random number from 0x0 to 0xF as long as pushbutton1 is pressed. Display the result with the 4 LEDs for about 3 seconds. b) Replace the code for recognizing a pressed key by a macro "KEY1_PRESSED". c) Replace the access to the 4 LEDs by a macro "LEDx_TOGGLE" with x = 0...3". Use active wait loops instead of the timer in this Kinetis exercise. Result: TWR_K60_RANDOM.zip
View full article
Hi All, Embedded systems industry are tending to optimized their products to offers a better performance in power management, aiming for longer battery life, using low-power modes in the application without reducing functionality. With this in mind, it arises a requirement in these compact devices, power supply monitor. This document will include a brief description of some features available in different power modes of the Kinetis family and it will focus on how we can implement these features, using KSDK 2.0, to monitor power supply voltage and detect when this voltage has fallen at determined value. This document is based MCU K21 but the same principles can be applied to any Kinetis K and L family. It will use KDS 3.2 as IDE and TWR-K21F120M evaluation board as target.   Hope you can find it useful Best Regards Jorge Alcala
View full article
       上篇详细的介绍了加密锁定Kinetis的一种方法,本篇再接再厉,给大家再介绍一种加密方法(哎,这点家底都晒出来了)。当然实际上原理还是不变的,即还是通过修改0x400~0x40F地址段的内容来实现加密锁定,万变不离其宗,所谓殊途同归罢了,下面好戏登台:        既然实现security最终都是改写寄存器加载段flash地址的内容,那实际上修改flash内容的方式还是灵活多变的,方案一中提到的在中断向量表的最后添加flash配置信息只是其中一种,那还有哪些呢?还是不摆谱了,小心被拍砖,哈哈。不错,那就是通过在指定地址定义常量的方法,当然定义常量大家都会用到(有些应用譬如LCD显示的字模或者一些固定的查找表为节省RAM空间我们一般会选择定义const常量的方法将它们存放到flash空间中),但是指定地址的存放方式用的会少些(一般都是让编译器自动分配的),如果我们非要指定地址呢(哎,强迫症又开始了,呵呵),即将flash配置信息作为常量强制指定存放到0x400起始的地址,那岂不是跟方案一有了异曲同工之妙了,好吧,这样的话那就该“@”这位老兄上场了(咳咳,可不是给单片机发email啊,呵呵),相信很多人到此处就都明白了。下面我仍然以IAR环境下锁定K60为例,简单介绍下方案二的使用步骤: 1. 打开待加密工程中的main.c文件,在其中的main函数之前以添加如下图所示常量定义,即将FlashConfig数据组数据存放到“.flashConfig”段中,其中FlashConfig[11]即为0x40C地址: 2. 至于这个.flashConfig段属性是需要在与该工程匹配的IAR连接文件(.icf文件)中人为添加定义的,如下图所示,需要添加三个部分,然后保存: 3. 前两步完成之后,其实需要添加的部分就已经完成了,但是还有特别重要的两点需要注意,这里我加红注释一下,如下: (1)采用方案二的情况,需要确保vectors.c中中断向量表最后的16个字节没有被添加,即不能有4个CONIFG_x配置信息的,否则会出现编译错误,因为这就涉及到两者冲突的问题,也就是说在采用方案一的话就不能采用方案二,同理,采用方案二的话也不能采用方案一,总之两者不能同存; (2)还需要考虑编译器优化的问题,因为我们在.flashConfig段定义了常量,但是在代码程序里却没有使用它,这种情况下编译器会直接把这段常量优化掉,所以我们做的工作算是白做了,即使我们在IAR的优化等级中设置成low或者none都不行,因为人家编译器认死理儿,反正你也没有使用它,我就是怕它pass掉,这下子伤心了,呵呵。还好IAR给我们留了条后路,在options->Linker->Input选项卡中提供了Keep symbol功能,如下图,将FlashConfig添加进去即可强制编译不优化它,这样目的就达到了,呵呵,看来还是天无绝人之路啊有木有。 3. 编译通过,下载调试,程序下载之后同样会出现进入不到调试窗口的现象,这个是正常现象,因为这个时候芯片就已经被security了,这样就可以放心量产了,呵呵~       希望这两篇系列文章能对大家有所帮助,enjoy it~
View full article
The documentation points out that the Figure 32-1. Multipurpose Clock Generator (MCG) block diagram in KV5xP144M240RM.pdf is incorrect, the  /2 divider is NOT included in the feedback loop. It gives the formula to compute the VCO and MCGPLLCLK clock frequency and corresponding code.
View full article
The AOI and Crossbar modules are inregrated in DSC, Kinetics KV and i.mxrt families, user can use them to generate complicated trigger signal for the on-chip peripherals. The DOC discusses the AOI function, crossbar fuction based on KV58. It gives the example, the example demos how to implement AND operation of two signals via crossbar switch A and B and AOI modules. The two logic signals are connected to the pads of KV58, and routed to AOI inputs via Crossbar switch B, the AOI sub-module0 implements the AND operation of the two signals, and output the AND output signal Event0  to pad of KV58 via crossbar switch A. Connect input pads and output pad of KV58 to oscilloscope, from the waveform of the three signals on scope, we can see that the AND logic  is implemented.
View full article
UART Presentation (universal asynchronous receiver/transmitter) by Ali Piña, Freescale TIC. Module Explanation Connection Diagram Hands-On. Polling mode. Interrupt Mode. Presentación de UART  (universal asynchronous receiver/transmitter) by Ali Piña, Freescale TIC. a.       Explicación del modulo. b.      Diagrama de conexión. c.       Hands-On. Modo de Poleo Modo de Interrupción
View full article
This is an example for the Kinetis KE02Z devices, showing how to program the EEPROM with initial values when the flash is programmed.  The example works on the FRDM-KE02Z40M board, and was written with Kinetis Design Studio (KDS) v3.0.0.  The example also uses Processor Expert (PEx) to configure the UART and erase/program the EEPROM.  The EEPROM programming works with the P&E Micro Multilink Universal debugger, as well as the P&E Micro OpenSDA debugger app for the FRDM-KE02Z40M board. To program the EEPROM with initial values, the application declares constants for the EEPROM locations, and initializes these in the source code in eeprom.c. Compiler pragmas/attributes are used to force the linker to place these constants in EEPROM, using the m_eeprom memory section defined in the linker command file \Project_Settings\Linker_Files\ProcessorExpert.ld.  The P&E Micro flash programming algorithms initialize the EEPROM in 4Byte words. Therefore, any initialized EEPROM locations should be in aligned 4Byte words. This example initializes the first 4Bytes in the EEPROM as 0, 64, 128, 192. The example uses a terminal program to display EEPROM information.  It connects to the OpenSDA COM port on the FRDM-KE02Z40M board using UART1 from the KE02Z. The terminal settings are:   Baud Rate: 38,400   Data: 8bit   Parity: None   Stop: 1bit   Flow Control: None The example prints 5 bytes of EEPROM to the terminal after reset: the 4 initialized bytes, plus the following EEPROM byte which was not initialized. Then the example increments the first byte, and decrements the second byte, and writes the new values back to EEPROM.  The other 3 bytes are not changed. Then the application prints the new EEPROM values of all 5 bytes.  Everytime the MCU is reset, it will print the existing EEPROM data and then the changed data.  Below is the example output from the terminal after initially programming the KE02Z, and then doing a single reset: Terminal output:   KE02Z EEPROM example   EEPROM values after reset = 0 64 128 192 255   EEPROM values after updating = 1 63 128 192 255   KE02Z EEPROM example   EEPROM values after reset = 1 63 128 192 255   EEPROM values after updating = 2 62 128 192 255
View full article
系统框图如下图示: 硬件设计支持如下扩展功能: (1)      USB、SD卡(SDHC接口) (2)      SWD调试+串口Printf。 (3)      SPI外设接口,支持NRF24L01、W5100、WIFI等。 (4)      两路差分ADC输入、一路DAC输出。 (5)      50M有源晶振,供MCU以及以太网PHY工作。 (6)      32.768K RTC时钟晶振。 (7)      SPI Flash、EEPROM(IIC接口) (8)      CAN接口。以太网应用。 (9)      TSI电容触摸按键。 (10)  GPIO:按键输入以及LED输出指示。 (11)  PWM输出。 (12)  FlexBus总线扩展: 扩展应用一:4.3寸LCD。 扩展应用二:FPGA扩展高速ADC采集。(设计进行中) 基于K60+SSD1963驱动4.3寸屏并移植ucGUI的测试实例,移植后的视频效果见如下链接: http://v.youku.com/v_show/id_XNzAwMTE5OTA0.html?firsttime=15 Pixels/sec: 16397220。
View full article
Download Kinetis M bare-metal drivers and software examples installation file. Changes in 4.1.6 : Modified FreeRTOS kernel to disable all interrupts prior entry to critical section and enable all interrupts upon exiting from critical section. This kernel behavior is compatible with standard FreeRTOS port to the ARM Cortex-M0 core. All freertos_cfg header files updated to reflect kernel change. Updated PLL_Disable macro and Quad Timer driver. Added UART_SetBaudRate macro. Removed RCM_ClrResetFlags macro. Fixed issue of generating callback events after conversion for these ADC channels with interrupt disabled.
View full article
Some of our customers encountered clock stretching issue when using the I2C. Actually the first should been in mind is the clock stretching is usually done by the slave, not the master.  In the case for the Kinetis as master to connect with I2C device, the clock stretching should been done by the slave device. In this case the slave device should hold the clock signal low until it has data available. There isn’t anything that needs to be done to enable clock stretching on the master side. So how the code do with the clock stretching? The slave should toggling read_start high first and reading the data register to actually start the transfer. Be remember that the read from the data register is what actually triggers the transfer. Customer always missed this point.
View full article
  MCU Bootloader2.0.0 enables quick and easy programming of Kinetis MCUs through the entire product life cycle, including application development, final product manufacturing, and beyond. It supports many kinds of peripherals, include UART, I2C, SPI, USB, CAN and so on. Among these peripherals, UART is most common used. In reference manual, it only says that feature can be turned on or off by using #define statement in bootloader_config.h. In fact, you can use UART0 by default. But if you want to use other UART port, change TERM_PORT_NUM to other value is useless. If you traced this value, you’ll find it is not used at all, nor the TERMINAL_BAUD. Here we use FRDM-KV31F512 as the example. We want to download image by UART2. First, we should modify peripherals_pinmux.h. #define BL_ENABLE_PINMUX_UART2 (BL_CONFIG_SCUART)     //line 38   //! UART pinmux configurations #define UART2_RX_PORT_BASE PORTE #define UART2_RX_GPIO_BASE PTE #define UART2_RX_GPIO_PIN_NUM 17               // PIN 16 in the PTB group #define UART2_RX_FUNC_ALT_MODE kPORT_MuxAlt3   // ALT mode for UART0 RX #define UART2_RX_GPIO_ALT_MODE kPORT_MuxAsGpio // ALT mode for GPIO functionality #define UART2_RX_GPIO_IRQn PORTE_IRQn #define UART2_RX_GPIO_IRQHandler PORTE_IRQHandler #define UART2_TX_PORT_BASE PORTE #define UART2_TX_GPIO_PIN_NUM 16             // PIN 17 in the PTB group #define UART2_TX_FUNC_ALT_MODE kPORT_MuxAlt3 // ALT mode for UART0 TX   The original define is UART0, here we change it to UART2. It is strongly recommended to do so. Otherwise you’ll find that UART can’t work at all. Another comment here is PTE16 and PTE17 is conflict with SPI. You must disable SPI or change SPI function to other pins.   Next we must modify peripherals_KV31F512.h. const peripheral_descriptor_t g_peripherals[] = { #if BL_CONFIG_SCUART    // UART0    {.typeMask = kPeripheralType_UART,      .instance = 2, // change this value from 0 to 2      .pinmuxConfig = uart_pinmux_config,      .controlInterface = &g_scuartControlInterface,      .byteInterface = &g_scuartByteInterface,      .packetInterface = &g_framingPacketInterface },   Although there is a baud rate definition TERMINAL_BAUD, but it is never used too. MCU bootloader2.0.0 use auto baud rate detection. When power on, bootloader will go to autobaud detection mode. KinetisFlashTool sends ‘0x ’ every second. Bootloader check this byte and calculate baud rate.   After getting this value, bootloader will change to normal communication mode. Baud rate will not change until reset. If blhost is used, subsequent blhost invocations must specify the same baud rate as was used for the initial invocation unless the bootloader is reset. If the baud rate is not specified using the -p COMx, <baudrate> option, the UART baud rate will be set to 57600. Since Kinetis MCU UART module don’t have auto frequency detect function, the bootloader detects frequcny by software. It uses GPIO interrupt and timer to measure frequency. But in bootloader, there is only code for UART0, there isn’t code for other UART port. We must add the code. In hardware_init_KV31F512.c, modify the function get_uart_clock()   uint32_t get_uart_clock(uint32_t instance) {    switch (instance)    {        case 0:        case 1:            // UART0 and UART1 always use the system clock            return SystemCoreClock;        case 2:            return get_bus_clock();        default:            return 0;    } }   KV31 has 4 UART, include three UART modules and one low-power UART. They have different clock source. UART0 and UART1 use System clock while UART2 and LPUART0 use Bus clock. Thus, we finished the work. UART2 can work as the download port now.
View full article
Many customers reported that their ADC function works on FRDM-KL27Z board but meet issue on their own board. We need to pay attention to the difference between the ADC reference voltages of different packages (on board MKL27Z64VLH4 is 64LQFP package). This tip introduce the ADC Reference Options on KL17/KL27 32/36pin package Part number involved: 32-pins 36-pins MKL17Z32VFM4 MKL17Z32VDA4 MKL17Z64VFM4 MKL17Z64VDA4 MKL27Z32VFM4 MKL27Z32VDA4 MKL27Z64VFM4 MKL27Z64VDA4 PTE30/VREF_OUT- connected as the primary reference option on 36-pin and below packages VDDA/VSSA - connected as the VALT reference option   ADCx_SC2[REFSEL] selects the voltage reference source used for conversions.   About the primary reference option: When on-chip 1.2V VREF is enabled, PTE30 pin must be used as VREF_OUT and has to be configured as an analog input, such as ADC0_SE23 (PORTE_PCR30[MUX] = 000). Notice: this pin needs to connect a capacitor to ground.   PTE30 can also be used as an external reference voltage input as long as PTE30 is configured as analog input and VREF module is disabled. It means you can connect external reference voltage to PTE30 pin and use it as ADC reference voltage. (For example 3.3V) KL17P64M48SF2RM     Kinetis KL17: 48MHz Cortex-M0+ 32-64KB Flash (32-64pin) (REV 4.1) KL27P64M48SF2RM     Kinetis KL27: 48MHz Cortex-M0+ 32-64KB Flash (32-64pin) (REV 4.1)
View full article
Hi,All Our team have developed the K60's peripheral derives lib which is open source and open source firmware library. the The open source lib have these feature just as follow: 1\The setup code based on the CMSIS Standard; 2\The lib include most of peripherals of K60 such as ADC,DAC,DMA,CAN,FTM,LPTMR, ENET,FLASH,FLexBUS,GPIO,IIC,MCG,PDB,SPI,USB,TSI,UART,WDOG,SDHC,PIT,etc. 3\All of the peripheral initiate function are based on the a structure variable Struct format. 4\Add parts of Freescale USB Stack into the lib such as USB CDC and USB HID mouse. 5\We also develop relative example projects to demonstrate how to use the library for the peripheral. All of the project are created by the IAR for ARM Ver.6.4. The attach is the code. We divide the code into two parts. One part is driver lib, and another part is project. PS 1:All of the code comments are Chinese, please forgive. PS 2:All of drivers is on the \lib\LPLD\HW.      The K60 project need Unzip into the \porject\. PS 3:The code has many place that need update and improve. if you have any doubt and opinions,please contact us.support[AT]lpld.cn Best Regards Wang
View full article
I recently developed a Visual Studio .NET application that uses an OpenSDA virtual serial port to communicate with a FRDM-K64F. My serial protocol is a binary command-response protocol, which means that every time the .NET application sends a command packet to the serial port, it should always receive a response packet back. You can find more details about the protocol in the Freescale Intelligent Sensing Framework, but for the purposes of this document, all that matters is that every command should receive a response. My Visual Studio .NET application uses the SerialPort class, and worked beautifully...until I changed the OpenSDA firmware. Originally I used OpenSDA firmware from P&E; this time I had tried out Segger. In theory, this change should not have made a difference, however with the Segger firmware my .NET application never received response packets. I knew that the command packets were transmitting correctly from PC to board because they would turn a board LED on and off as expected. I tried using a binary terminal, RealTerm, to send commands to see if it would receive responses, and it did. So the problem had to be in my .NET application. After a lot of googling and some trial-and-error, I ultimately found that enabling the Data Terminal Ready (DTR) signal did the trick. Strangely, I didn't need to enable DTR in RealTerm. The moral of the story is that if you want to use Segger OpenSDA with a .NET SerialPort, then you must enable DTR. Fortunately this configuration also works with P&E and mbed OpenSDA.
View full article
在工业热电偶数据采集与处理方面,ADI,MAXIM的模拟芯片几乎占据了90%以上的市场,尽管他们的单片售价高的吓人。1片16位的AD芯片没有个2个美金是买不到的,24位的更不用多说。现在他们的竞争对手来了,飞思卡尔针对表计市场推出的基于M0+内核的KM1x,KM3x,片上集成24位的Σ-Δ模拟前端, 其中2路带有独立的可编程最高32倍PGA,无论是市场上应用最多的K型热电偶、还是专注于低温测量的T型热电偶,通过合理的配置都可以满足他们极宽范围的量程。确切的讲,KMxx和这两种产品根本不能算是一个数量级的PK对手,无论从资源上还是从价格上。但是尽管这样,就一定能打败竞争对手吗?首先得有的说服力的参考设计吧,不着急,已经开始设计了。 处理器:MKM33Z128CLH5 暂定功能: 1. K型热电偶+T型热电偶兼容采集处理,板上预留2种热电偶接口,带冷端温度补偿功能 2. 按键切换热电偶类型 3. 段码式LCD显示采集的实时温度,状态显示 4. 低功耗演示,面向手持式设备市场 5. 音乐变调蜂鸣器 主要针对竞争目标:Maxin的 MAX31855KASA (T型热电偶) 关于精度嘛,等参考设计完成了测试一下就知道了。 以上参考设计敬请等待,也欢迎多提宝贵建议。
View full article