Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
   CodeWarrior v10.6 and KDS are integrated development tools which are based on Eclipse, these two IDEs provide easy way to build project when using the GUI, but some engineers still want to build their projects from command line to do automated builds. This document provides examples on how to do it! Build project in CodeWarrior from command line: For a CW v10.6 created project, CW provides the “Make” tool and can also generate the needed “MakeFile” to build this project out of eclipse GUI. The below are the steps: Create and new project “k22_makefile” in CW v10.6, you will see there are two build configurations: RAM & FLASH Launch “cmd prompt” in Windows and go to “eclipse” folder of CW installation Now, you can generate the makefile for configuration FLASH by executing the below command ecd.exe –generateMakefiles –project “C:\workspace_cmd\k22_makefile” –config FLASH Now, checking the “FLASH” subfolder in project location, you will see “makefile” is generated. 4.To use “make” tool convenient, we can define an environment variable pointing to {CW}\gnu\bin where “make” is located. See command as below: 5. Go to the configuration folder “FLASH” where the project’s makefiles are located and run the follow commands to build the project. %MCU_BIN%\make.exe PS: to get more information of make and ecd, please just run the below command: Ecd.exe –help Make.exe –help Build project in KDS from command line: Compare with CodeWarrior, it is much easier to build an application in command mode. KDS provides a command “eclipse.exe” with which you can build a project with only two steps. In this example, I have created an application with name “cmd_ke02”, and the workspace path is “C:\wks_kdscmd”. To build the application in cmd, please first launch command mode in Windows system and then go to {KDS}\eclipse. Then, you need import the application into current workspace in the below command: eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\wks_kdscmd" -import "C:\wks_kdscmd\cmd_ke02" then, build the project with the below command: eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\wks_kdscmd" -build "cmd_ke02" For more details of building project from command line in KDS, please refer: http://mcuoneclipse.com/2014/09/12/building-projects-with-eclipse-from-the-command-line/
記事全体を表示
1. 飞思卡尔常用调试工具 2. 使用OpenSDA平台作为J-Link调试Kinetis 3. 使用OpenSDA平台作为USBDM调试Kinetis 4. 使用MTB模块快速跟踪定位Cortex-M0+指令执行状态(Use MTB in Cortex-M0+ to trace instructions) 5. KL25被加密,芯片锁死问题? 6. 对比几款流行的Kinetis调试器速度 7. 修复Jlink固件损坏的方法 8. Jlink调试Kinetis L系列的使用方法 9. CMSIS-DAP调试器在IAR v7.1中问题(Probe not Found)修复 10. FRDM_KL26 虚拟串口安装失败的解决方法 11. 使用J-Link TCP-IP Server通过以太网远程下载程序到Kinetis 12.Kinetis LOCK的原因及解决方案​
記事全体を表示
Kinetis E series MCUs target to applications where require high performance on EMC/ESD. With 5V power supply and robust IO design, Kinetis E series MCUs can help customer for a robust design. Here take a Microwave Oven demo as example, shares how to make a robust design with Kinetis E Series MCU, from hardware, software perspective.
記事全体を表示
Hi All, attached bootloader is a short program that allows possibility to update existing firmware in Kinetis-M microcontroller device. It consist of Master PC application and a tiny slave application that runs on target device. It uses UART communication.
記事全体を表示
Description Thing.... Internet Enabled..... with command line and GUI over a TCP connection Parts Fantasma Toys Hand Runner: http://www.newegg.com/Product/Product.aspx?Item=9SIA0190BB9057 FRDM-K64 : http://mbed.org/platforms/FRDM-K64F/ RN-XV: https://www.sparkfun.com/products/10822 FRDM-AUTO: https://community.freescale.com/docs/DOC-99621 GUI Code:  https://github.com/ehughes/InternetofThing MBED Code: http://mbed.org/users/emh203/code/InternetOfThing/wiki/internet_of_thing Action Shots
記事全体を表示
           This is a demo of NFC device to read and write the contactless card. Kinets K60 tower board and NXP PN512 board are used for this test enviroment. These connected pins from K60 tower board to PN512 RF board are listed as below:   SPI1:     SPI1_SIN : PTE1/SDHC0_D0     SPI1_SCK : PTE2/SDHC0_DCLK     SPI1_SOUT : PTE3/SDHC0_CMD     SPI1_PCS0 : PTE4/SDHC0_D3     Reset:     PTB9   External interrupt:     PTA26         Because the SPI1 port is used as the host interface of pn512, it is necessary to enable the SPI1 driver in the user configuration file of MQX.           To open the project file in the /build folder with CW10.5.    And the PSP and BSP libraries had to be built before test image is built, as they are needed in this test project.   The following diagram shows the serial numbers and block data of reading from the test card of Mifare one.
記事全体を表示
Example of integrating CMSIS3.20 into MQX4.0.x on the TWR-K60D100M (no floating point unit) using CW10.4 using the MQX4.0.2\mqx\examples\hello2 project. In the attached ZIP file (hello2twrk60d100m_CMSIS_NoFPU.zip) is a MSWord document detailing the steps used.  That document name is TWR-K60D100M_CMSIS_CW10.4_MQX4.0.x.docx. Regards, David
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-332687
記事全体を表示
by: Carlos Musich, Luis Garabito Microcontrollers Application Engineers with Freescale. This application note is intended to demonstrate http client implementation using Freescale MQX RTOS capabilities. The hardware used to illustrate this is the TWR-K60N512-KIT. The remote controlling and monitoring have become a need rather than an option in the embedded world. This application note takes advantage of two social media interfaces for these purposes. One is used to enter commands to the MCU; http://twitter.com/. The other one is used to pull out data from the MCU; https://www.supertweet.net/. It is important to focus in the fact that with these methods the MCU is reachable through Internet without the need of a public IP address or without mounting a HTTP server in the MCU. The application source code described in this document can be found in the AN4417SW.zip file. For a full description of Freescale MQX RTOS, please visit https://www.freescale.com. This application defines two tasks in MQX. The first task is main. It is meant to configure GPIO, the RTCS and create the second task. The name of this second task is httpclient. The purpose of this task is to carry out the communication with the Twitter server and read the commands to be executed. To retrieve the input commands, the httpclient task reads them from the last tweet published by a specific Twitter account. The command then is parsed and executed according to the implementation. The main task enters into an infinite loop where the httpclient is restarted in each loop to allow a cycle behavior for reading commands. The time for each loop is controlled by a sample rate value that can be configured by the user via a command. Get the full application note...
記事全体を表示
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-335320
記事全体を表示
1. Freedom开发板: 飞思卡尔Freedom开发平台是一套低成本的用于性能评估和软件开发的工具,自带板载调试器,用户可以直接通过自己的PC机快速搭建开发环境并进行测试和评估芯片简单的外设资源。一般来说,同一个系列功能互相兼容的芯片会推出一款Freedom开发板来评估,具体分类如下: Freedom开发板 可以覆盖的芯片型号 开发板代码包 FRDM-KL02Z Kinetis KL02 MCUs KL02_SC FRDM-KL03Z Kinetis KL03 MCUs Kinetis SDK for KL03 FRDM-KL05Z Kinetis KL04 and Kinetis KL05 MCUs KL05_SC FRDM-KL25Z Kinetis KL14, Kinetis KL15, Kinetis KL24 and Kinetis KL25 MCUs KL25_SC FRDM-KL26Z Kinetis KL16 and Kinetis KL26 MCUs KL26_SC FRDM-KL43Z Kinetis KL17, Kinetis KL27, Kinetis KL33 and Kinetis KL43 MCUs FRDM-KL43_SC FRDM-KL46Z Kinetis KL36 and Kinetis KL46 MCUs KL46_SC FRDM-KE02Z Kinetis KE02_20M MCUs KEXX_DRIVERS_V1.2.1_DEVD FRDM-KE02Z40M Kinetis KE02_40M MCUs KEXX_DRIVERS_V1.2.1_DEVD FRDM-KE04Z Kinetis KE04 MCUs KEXX_DRIVERS_V1.2.1_DEVD FRDM-KE06Z Kinetis KE06 MCUs KEXX_DRIVERS_V1.2.1_DEVD 2. TWR开发板: 飞思卡尔塔式系统开发板为可扩展性比较强的评估板,板载资源比较丰富且通过构建塔式系统可以灵活的添加和裁剪外设资源,用户可以通过与相应外设塔式板结合使用进行更高级和复杂的功能测试或验证。 Tower开发板 可以覆盖的芯片型号 Header 3 TWR-KL25Z48M Kinetis KL14, Kinetis KL15, Kinetis KL24 and Kinetis KL25 MCUs KL25_SC TWR-KL43Z48M Kinetis KL17, Kinetis KL27, Kinetis KL33 and Kinetis KL43 MCUs TWR-KL43Z48_SC TWR-KL46Z48M Kinetis KL16, Kinetis KL26, Kinetis KL36 and Kinetis KL46 MCUs KL46_SC TWR-KM34Z50M Kinetis KM3x MCUs KMSWDRV TWR-KV10Z32 Kinetis KV1x TWR-KV10Z32_SC 3. 第三方开发板 (1) MAPS四色板套件 (2) YL-KL26Z 开发板
記事全体を表示
Reference Solution being developed with Kinetis V (also can be done with a Kinetis K device) of a Class-D audio amplifier. 16-bit ADC sampling the audio input FlexTimer doing the PWM's for the Class-D amplifier DC/DC switched power supply with input of 12V and output of 130V to 180V (generates the power you need for making some good noise - 1kW) being controlled by the Kinetis MCU also. Capabiltiy of Audio processing/filtering using the Cortex-M4 DSP capabilities. Solution originally designed for cost-effective Automotive aftermarket sound systems. But can be adapted for implementing other audio amplifier applications also in the consumer space! Can you thing of cool applications/markets that this solution can be also quickly adapted? Soon, plan to make the reference solution design files available in the community. Stay tunned. Cheers! PK
記事全体を表示
KL17 reference manual V4.1 and V5.1 with updated Figure 13-2. Kinetis Bootloader Start-up Flowchart at page 179 There with modification to add "is direct boot valid" check. Please check below picture for the detailed info: The "is direct boot valid" check function is not supported for KL17 product, the correct flow chart should be below: The "is direct boot valid" check function is reserved for further parts(such as KL82), which has one bit in BCA filed to control running code in QSPI Flash or internal Flash: Thank you for the attention.
記事全体を表示
for M68HC08, HCS08, ColdFire and Kinetis MCUs by: Pavel Lajsner, Pavel Krenek, Petr Gargulak Freescale Czech System Center Roznov p.R., Czech Republic The developer's serial bootloader offers to user easiest possible way how to update existing firmware on most of Freescale microcontrollers in-circuit. In-circuit programming is not intended to replace any of debuging and developing tool but it serves only as simple option of embedded system reprograming via serial asynchronous port or USB. The developer’s serial bootloader supported microcotrollers includes 8-bit families HC08, HCS08 and 32-bit families ColdFire, Kinetis. New Kinetis families include support for K series and L series. This application note is for embedded-software developers interested in alternative reprogramming tools. Because of its ability to modify MCU memory in-circuit, the serial bootloader is a utility that may be useful in developing applications. The developer’s serial bootloader is a complementary utility for either demo purposes or applications originally developed using MMDS and requiring minor modifications to be done in-circuit. The serial bootloader offers a zero-cost solution to applications already equipped with a serial interface and SCI pins available on a connector. This document also describes other programming techniques: FLASH reprogramming using ROM routines Simple software SCI Software for USB (HC08JW, HCS08JM and MCF51JM MCUs) Use of the internal clock generator PLL clock programming EEPROM programming (AS/AZ HC08 families) CRC protection of serial protocol option NOTE: QUICK LINKS The Master applications user guides: Section 10, Master applications user guides. The description of Kinetis version of protocol including the changes in user application: Section 7, FC Protocol, Version 5, Kinetis. The quick start guide how to modify the user Kinetis application to be ready for AN2295 bootloader: Section 7.8, Quick guide: How to prepare the user Kinetis application for AN2295 bootloader.
記事全体を表示
Hello. I am trying to use a PIT interrupt. I had never used Kinetis so there are certain things which with I am not familiarized yet. once i have created de PE code, cleaned and then I build the proyect, the following error pops up 'undefined reference to int_disp'. What it is about? Where should I write my ISR fuction? Does the ISR pit function has to have an specific name so as to be recognised by PIT.c?
記事全体を表示
The following file contains codewarrior code that was migrated from the IAR example code in the sample code package at the freescale webpage. It contains the following examples: adc_demo freedom_greem_led freedom_red_led lcd_rtc_lowpower PIT_basic sLCD_freedom uart_low_power_wu_dut Regards
記事全体を表示
KBOOT learning diary Overview      FSL’s already released the KBOOT v1.1.0 in Dec, 2014 and the v1.2.0 will be released in Jun, 2015. KBOOT is an innovation bootloader solution instead of former and it just seems like a platform for quick and easy programming the Kinetis MCUs. KBOOT will make the developers to save the effort for design the bootloader, even it support the developers to customize the bootloader.        KBOOT provides two ways for implementing, ROM bootloader and Flash bootloader, ROM bootloader is only applicable to the Kinetis MCUs which already integrate the ROM and the KBOOT application reside in it. So the ROM bootloader is available during the entire product life cycle.  The opposite side, the Kinetis MCUs without ROM can be programmed through the Flash bootloader. For the Flash bootloader, it runs into RAM and receive the application image, after it program the image into the Flash completely, then it Flash bootloader will go to die, in another word, it will no longer be available again. Table 1 shows supported Kinetis MCUs. Table 1 Support Kinetis Devices        KBOOT’s supported to program the target through the UART, SPI, I2C, USB HID communication and it will also support the MSD Device and MSD HOST mode, Ethernet, etc in future. And developers can use blhost application or GUI tool as the host tool to communicate with the bootloader, then program the application code in flash via the bootloader. Implementing        In these user guides as follow: Getting Started with the Kinetis ROM Bootloader, Getting Started with the Kinetis Flashloader, Kinetis blhost User's Guide, Kinetis Updater User's Guide, you can find a completely procedure to program the application code via bootloader. Exception However I’ve encountered an issue when I tried to use the blhost application to communicate the FRDM-KL03Z (Fig1), it still couldn’t establish a connection, as Fig 2 shows. Fig 1 Fig 2 Workaround       The issue will disappear after choose a lower baud rate when blhost application communicate with the FRDM-KL03Z board after I validated. And the whole procedure to program application code as follow.       1. Establishes the connection        2. Erases the entire flash array       3. Programs the application code       4. Application code runs
記事全体を表示
This is a Processor Expert project created by CodeWarrior for MCUs v10.6 which implements the charge-discharge time of a RC circuit for measuring capacitance. The charge-discharge sequence is performed by TPM0 operating in PWM mode, while the time is measured by TPM1 operating in Input Capture mode. A 100K ohm series resistor is being used, and the result is expressed on nF. It is also using the LCDHTA component from Erich Styger for showing the measurements on a 16x2 LCD, connected to the FRDM-KL05Z through a proto shield. The project is attached, and the pictures shows the measurements of three different capacitors: 10nF, 47nF and 1uF.
記事全体を表示
I have included the files needed to mass erase the flash of the MCU and re-program another binary.   The procedure is shown in the folder " FRDM-KW31_FAT_added_2019" Summarizing you... 1) update the debugger with bootloader mode (press reset and plug in usb cable) drag and drop .sda file on MSD bootloader. 2) unplug and re-plug USB. program the flashloader_loader_mkv31f512.bin by dragging and dropping the binary on to the virtual mass storage device FRDM-KV31 which appear when you plug the USB cable from the FRDM-KV31 to the PC.  3) Open a CMD prompt window and navigate to the folder the files were unzipped to. 4) Determine the COM port by using the device manager 5) from the CMD prompt run the batch file      Erase_KMS_program_bubble.bat COMX
記事全体を表示