question about KEA128 clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

question about KEA128 clock

跳至解决方案
2,031 次查看
vegetarian1
Contributor III

I have a question about KEA128. According to Reference manual, FLL frequency must be in the range 31.25 kHz to 39.0625 kHz in some modes, and the minimal frequency of flash is 1M. Would flash work properly via FLL in low frequency?

标记 (1)
1 解答
1,925 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport
0 项奖励
回复
2 回复数
1,925 次查看
vegetarian1
Contributor III

I'm a novice about KEA128. I think the reason is  FLL locks the frequency to 1280 times the internal or external reference
frequency. Thanks for your attention.

1,926 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

yes

ICSFLLCLK.png

Figure 5-1. Clocking diagram.png

0 项奖励
回复