question about KEA128 clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about KEA128 clock

Jump to solution
2,121 Views
vegetarian1
Contributor III

I have a question about KEA128. According to Reference manual, FLL frequency must be in the range 31.25 kHz to 39.0625 kHz in some modes, and the minimal frequency of flash is 1M. Would flash work properly via FLL in low frequency?

1 Solution
2,015 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
2,015 Views
vegetarian1
Contributor III

I'm a novice about KEA128. I think the reason is  FLL locks the frequency to 1280 times the internal or external reference
frequency. Thanks for your attention.

2,015 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

yes

ICSFLLCLK.png

Figure 5-1. Clocking diagram.png

0 Kudos
Reply