question about KEA128 clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question about KEA128 clock

ソリューションへジャンプ
1,990件の閲覧回数
vegetarian1
Contributor III

I have a question about KEA128. According to Reference manual, FLL frequency must be in the range 31.25 kHz to 39.0625 kHz in some modes, and the minimal frequency of flash is 1M. Would flash work properly via FLL in low frequency?

タグ(1)
1 解決策
1,884件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
1,884件の閲覧回数
vegetarian1
Contributor III

I'm a novice about KEA128. I think the reason is  FLL locks the frequency to 1280 times the internal or external reference
frequency. Thanks for your attention.

1,885件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

yes

ICSFLLCLK.png

Figure 5-1. Clocking diagram.png

0 件の賞賛
返信