MKV31F128VLH10 and SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV31F128VLH10 and SDK

Jump to solution
1,916 Views
andreasruetten
Contributor III

I have updatetd the last sdk for the kinetis ...

After this i can't choose the MCU anymore.

The only MCU i can choose is MKV31F512 !!

 

 

Unbenannt.jpg

2.jpg

 

So what do i wrong ??

MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]

 

SDK 2.9.0

 

0 Kudos
Reply
1 Solution
1,888 Views
andreasruetten
Contributor III

Hi Sebastion,

i solved the prom to my self ...

View solution in original post

0 Kudos
Reply
2 Replies
1,889 Views
andreasruetten
Contributor III

Hi Sebastion,

i solved the prom to my self ...

0 Kudos
Reply
1,899 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Andreas, I hope you're doing well!

 

Could you please let me know if you are still experiencing this issue? If you try using another workspace, are you able to open other SDKs?

 

Best regards,

Sebastián

0 Kudos
Reply