MKV31F128VLH10 and SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKV31F128VLH10 and SDK

ソリューションへジャンプ
2,818件の閲覧回数
andreasruetten
Contributor III

I have updatetd the last sdk for the kinetis ...

After this i can't choose the MCU anymore.

The only MCU i can choose is MKV31F512 !!

 

 

Unbenannt.jpg

2.jpg

 

So what do i wrong ??

MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]

 

SDK 2.9.0

 

0 件の賞賛
返信
1 解決策
2,790件の閲覧回数
andreasruetten
Contributor III

Hi Sebastion,

i solved the prom to my self ...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,791件の閲覧回数
andreasruetten
Contributor III

Hi Sebastion,

i solved the prom to my self ...

0 件の賞賛
返信
2,801件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Andreas, I hope you're doing well!

 

Could you please let me know if you are still experiencing this issue? If you try using another workspace, are you able to open other SDKs?

 

Best regards,

Sebastián

0 件の賞賛
返信