KV11 support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV11 support

Jump to solution
2,938 Views
davidsherman
Senior Contributor I

We are interested in using the KV11, but it appears in KDS 3.2 that it only supports KV10.  While the two are similar and we could alter things to support KV11, are there plans to add KV11 to make a basic project without Processor Expert or KSDK?

Labels (1)
0 Kudos
Reply
1 Solution
2,402 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

Besides Alice, User can use kds3.2+ksdk1.3 processor expert also.

The KSDK 1.3 mainline release contain the support of the KV11. See the following link:

 

Software Development Kit for Kinetis MCUs|NXP 

 

and navigate to the Kinetis SDK 1.3 Mainline download link:

pastedImage_3.png

To work with KV11+processor expert, we need:

1. install KDS3.2

2. install KSDK1.3 mainline.

3. Do update from KDS IDE menu "help", "check for update".

 

then you will see KV11 and processor expert available. see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,403 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

Besides Alice, User can use kds3.2+ksdk1.3 processor expert also.

The KSDK 1.3 mainline release contain the support of the KV11. See the following link:

 

Software Development Kit for Kinetis MCUs|NXP 

 

and navigate to the Kinetis SDK 1.3 Mainline download link:

pastedImage_3.png

To work with KV11+processor expert, we need:

1. install KDS3.2

2. install KSDK1.3 mainline.

3. Do update from KDS IDE menu "help", "check for update".

 

then you will see KV11 and processor expert available. see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,402 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

You can download the KSDK2.0 for MKV11   "SDK_2.0_MKV11Z128xxx7",

the detail steps for download please refer to :How to: install KSDK 2.0 

If you don't want to use the KDSDK drivers , you can select "Empty " when create proect :

pastedImage_2.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------