KV11 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,088件の閲覧回数
davidsherman
Senior Contributor I

We are interested in using the KV11, but it appears in KDS 3.2 that it only supports KV10.  While the two are similar and we could alter things to support KV11, are there plans to add KV11 to make a basic project without Processor Expert or KSDK?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,552件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

Besides Alice, User can use kds3.2+ksdk1.3 processor expert also.

The KSDK 1.3 mainline release contain the support of the KV11. See the following link:

 

Software Development Kit for Kinetis MCUs|NXP 

 

and navigate to the Kinetis SDK 1.3 Mainline download link:

pastedImage_3.png

To work with KV11+processor expert, we need:

1. install KDS3.2

2. install KSDK1.3 mainline.

3. Do update from KDS IDE menu "help", "check for update".

 

then you will see KV11 and processor expert available. see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,553件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

Besides Alice, User can use kds3.2+ksdk1.3 processor expert also.

The KSDK 1.3 mainline release contain the support of the KV11. See the following link:

 

Software Development Kit for Kinetis MCUs|NXP 

 

and navigate to the Kinetis SDK 1.3 Mainline download link:

pastedImage_3.png

To work with KV11+processor expert, we need:

1. install KDS3.2

2. install KSDK1.3 mainline.

3. Do update from KDS IDE menu "help", "check for update".

 

then you will see KV11 and processor expert available. see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,552件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

You can download the KSDK2.0 for MKV11   "SDK_2.0_MKV11Z128xxx7",

the detail steps for download please refer to :How to: install KSDK 2.0 

If you don't want to use the KDSDK drivers , you can select "Empty " when create proect :

pastedImage_2.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------