Command Line Builds in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Command Line Builds in KDS

ソリューションへジャンプ
2,829件の閲覧回数
ScottW
Contributor II

In CodeWarrior, I could do command line builds of my projects using ecd.exe.  We used this for build automation.  Is there equivalent functionality in KDS? 

ラベル(1)
1 解決策
2,024件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
2,025件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

2,024件の閲覧回数
ScottW
Contributor II

Thanks!  That works great.

0 件の賞賛
返信