Command Line Builds in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Command Line Builds in KDS

Jump to solution
2,868 Views
ScottW
Contributor II

In CodeWarrior, I could do command line builds of my projects using ecd.exe.  We used this for build automation.  Is there equivalent functionality in KDS? 

Labels (1)
1 Solution
2,063 Views
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

View solution in original post

2 Replies
2,064 Views
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

2,063 Views
ScottW
Contributor II

Thanks!  That works great.

0 Kudos
Reply