KDS for noobies?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS for noobies?

509 Views
jverive
Contributor III

I've been using Raspberry Pi and Arduino, both of which had learning curves, but nothing like what I'm experiencing with the K22f and KDS/KSDK. Is there a place for noobies to go to learn how to do the basics, like blink an LED and capture the state of on-board switches? All I really want to do at this time is write a C/C++ program that includes the necessary headers, then compile the program, build it for the board, and upload/download it to the board. Is that too much to ask?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

357 Views
DavidS
NXP Employee
NXP Employee

Hi Jeff,

Start with

Kinetis SDK K22 User's Guide.pdf

and

Kinetis SDK Demo Applications User's Guide.pdf

Located in: C:\Freescale\KSDK_1.0.0\doc

Regards,

David

0 Kudos
Reply