Command Line Builds in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Command Line Builds in KDS

跳至解决方案
2,869 次查看
ScottW
Contributor II

In CodeWarrior, I could do command line builds of my projects using ecd.exe.  We used this for build automation.  Is there equivalent functionality in KDS? 

标签 (1)
1 解答
2,064 次查看
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

在原帖中查看解决方案

2 回复数
2,065 次查看
BlackNight
NXP Employee
NXP Employee

Yes, there is the normal Eclipse Kepler command line version of the IDE available which can do this.

See Building Projects with Eclipse from the Command Line | MCU on Eclipse

I hope this helps,

Erich

2,064 次查看
ScottW
Contributor II

Thanks!  That works great.

0 项奖励
回复