Kinetis Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Design Studio Knowledge Base

Labels

Discussions

Sort by:
Taking code for a simple LCD function that is used in Code Warrior and modifying it for use in KDS on the FRDM-KL46Z board.
View full article
This is an update to Kinetis Design Studio V3.0.0 which updates it to version V3.1.0. You need KDS V3.0.0 installed in order to install this update. This update includes as well a Processor Expert for Kinetis V3.0.2 update. It is an online update through the Eclipse update mechanism.   Note: the updates are available for offline installation as well from the download section on www.nxp.com/kds   This update fixes a know issue with the dependency to the GNU ARM Eclipse plugins described in Unable to Debug after KDS Update .   Online Update To install the update from the Eclipse update site, the preferred method is to use the menu Help > Check for Updates As this lists many other updates which might cause conflicts, make sure you only select the Kinetis Design Studio 3.1.0 update: Install the update, then in a second update you can install the other KDS updates. Here again, do not select other 3rd party updates as this might cause conflicts: Then go through the installation process.   An alternative method is to use Help > Install New Software and use the following Eclipse Update site: http://freescale.com/lgfiles/updates/Eclipse/KDS (Note: this is an Eclipse update site, not usable for a web browser)     Then select "Kinetis Design Studio 3.1.0" update from the list (shown for Windows host below): Next it will inform about the actions taken. A Somnium portion of the IDE will be removed and replaced: Press 'Next' and go through the update process.   Offline Update The update is available as zip archive which can be downloaded once and then used for an offline installation, pointing to the zip archive as update site.   Go to Kinetis Design Studio Integrated Development |NXP  and click 'Download' in the Download tab:   Select the KDS 3.0.0 for the host you are using: Select the "Kinetis Design Studio 3.1.0" update (screenshot shown for Mac OS X) and download it: In Kinetis Design Studio V3.0, use the menu Help > Install New Software and point to the downloaded file to install it.   For details additional, see the attached release notes.
View full article
Hello community!   Attached is a document that introduces the usage of Component Development Environment (CDE) by creating a software component that will use the Kinetis Software Development Kit (KSDK) drivers to control a 16x2 LCD.   The code provided on the below document will be used as starting point for the creation of the component:   Driving 16x2 LCD using KSDK drivers: https://community.freescale.com/docs/DOC-329190     Contents: 1. Glossary   2. Overview and concepts   2.1 Processor Expert Software   2.1.1 Embedded Components   3. Creating a new embedded component   3.1 Adding properties   3.2 Adding a method   3.3 Adding inherited components   4. Testing component.   Appendix A - References       I hope you can benefit from this post, if you have questions please let me know.   Best Regards! Carlos Mendoza
View full article
Accelerometer in KDS Description:   This is a small project made in KDS using the accelerometer on a FRDM-MK64FN1M0VLL12 board. The blue LED is on when the board is flat or upside down The red LED is on when the board is on its side The green LED is on when the board is on its nose or tail   Sections of code taken from http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/
View full article
This list includes all the documents in the NXP community Kinetis Design Studio space. You can download the latest version of KDS on NXP web : Kinetis Design Studio Integrated Development |NXP .   Installation and Update New Kinetis Design Studio v3.2.0 available Kinetis Design Studio Update V3.1.0 available New Kinetis Design Studio V3.0.0 available Kinetis Design Studio V2.0.0 available on the Web! Kinetis Design Studio V1.1.1 Released! Kinetis Design Studio V1.1.0: Release Notes and News Kinetis Design Studio V1.0.1 Beta Release Notes KDS Install Guide KSDK 1.3.0 Documents Plugin for KDS 3.0.0 Extended Device Support: Updated P&E Debug Plugin V1.1.4 for KDS V1.1.1 Kinetis Design Studio V1.0.1 Beta Release Notes Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio   How to Use   Generate aligned HEX and S-record data output with GNU in KDS 3.2  How to support multiple targets in CodeWarrior(Classic, Eclipse)/KDS  Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio  Using KBOOT v2 on KDS in Debug Mode Debugging Bootloader and Application using Kinetis Design Studio V3.2.0 Changing MCU for SDK2.0 project in KDS How to start customized KSDK V1.2 project based on KSDK demo code Tutorials using the Kinetis SDK V1.0.0 with Kinetis Design Studio  How to Create a C++ Project Using MQX RTOS for KSDK1.2 Converting a non-Processor Expert Project into a Processor Expert Project Creating KDS project based upon the KL46 from CW project How to Add Existing Files to KDS Relocating Code and Data Using the KDS GCC Linker File for Kinetis Increasing Eclipse Heap Space to Improve Performance Semihosting for Kinetis Design Studio Getting started with CDE in Kinetis Design Studio Getting started with SVN and Kinetis Design Studio Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V3.0.0) Importing MCU V10.6 projects (sample, using PE and MQX) under KDS V1.1.1  Quickstart Guide for KDS v1.0.1 beta Using ESFC bit - Flash programming routines in Cotex M0+ kinetis MCU Start working with NXP Touch Software library How to Start CAN Module Development on KDS v3.2.0 + Processor Expert   Compiler and Linker Changing the ARM GNU Tool Chain in Kinetis Design Studio Extended Inline Assembly with Kinetis Design Studio How to build BeeKit exported CodeWarrior 10.6 projects using KDS How to add uninitialized data section to a GCC build Merging applications using Kinetis Design Studio   Debugger Interface and firmware GDB Debugging with Kinetis Design Studio KDS Debug Configurations (OpenOCD, P&E, Segger) Summary of FRDM-K64F open source debug interface Summary of FRDM-K22F debug interface Using FRDM-K64F with P&E and Segger OpenSDAv2 Firmware FRDM-K22F: Debugging with P&E OpenSDAv2.1 Firmware FRDM-K22F: Debugging with Segger J-Link OpenSDAv2.1 Firmware OpenOCD support for K22FN512 & K24FN256 in KDS How to setup SEGGER J-Link lite debugger connection in Kinetis Design Studio 1.1.1 Register Detail Debugging with KDS   KDS Application KEA128 CAN Bootloader  Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+ Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4 Using the FRDM-KL25 Board as a USB Keyboard in KDS Using the FRDM-KL25 Board as a USB Mouse in KDS KDS - Simple Air Mouse on a FRDM KL25Z Hello World bare metal project for FRDM-KL25 using KDS Using the Accelerometer on the FRDM-KL25 Board in KDS Using the FRDM-KL46 Board as a USB Mouse in KDS Using the FRDM-KL46 Board as a USB Keyboard in KDS Using the LCD screen on a FRDM-KL46 Board as a timer using KDS Using the LCD screen on a FRDM-KL46 Board to display accelerometer data using KDS Using the LCD screen on a FRDM-KL46 Board to display temperature using KDS Using the LCD screen on a FRDM-KL46 Board to light intensity using KDS Baremetal code examples using FRDM-K64F Using the FRDM-MK64 Board to write to an SD Card in KDS Using the FRDM-MK64 Board to write to Accelerometer data to an SD Card in KDS SD Card Bootloader :how to using SD card to update existing firmware on CodeWarriror or KDS Using the Accelerometer on the FRDM-MK64 Board in KDS Blinking an LED on a FRDM-MK64 Board in KDS Reaction measuring game on a FRDM-KL46 board using KDS Tutorials: WS2812B LED Stripes with the FRDM-K64F Board Toggling the FRDM-K64F RGB LED using interrupts in Kinetis Design Studio (KDS) How to use printf() to print string to Console and UART in KDS2.0 Disabling Watchdog for 'Bare' Projects   Bug and Workaround Defect fix for KSDK1.2/KSDK1.3 MK02FN128 -- “xxx.elf uses VFP register arguments” kds_quick_start has ommision error. Uninstalling KDS: "Error opening installation log file."   KDS FAQ KDS Frequently Asked Questions (FAQ)
View full article
Accelerometer in KDS   Description:   This is a small project made in KDS using the accelerometer on a FRDM-KL25Z128M4 board. The program outputs the 3D position of the board to a terminal, such as Tera Term at 9600 baud. PWMs are also used, their intensity is dependent on the offset from the zero position. The red LED intensity increases with X offset. The blue LED intensity increases with Y offset. Simply press any key to begin data output.   Sections of code taken from http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/   Issues:   There seem to be 'dead zones' while the board is tilted towards a corner. The terminal will not output anything while in a 'dead zone'.   There will be a constant flicker of the LED even when the board is flat. This is due to the accelerometer occasionally outputting 1 even when the board is static.
View full article
Greetings, I have created a multi-part tutorial how to use the WS2812B (aka Adafruit NeoPixel) LED stripes and boards with the FRDM-K64F board:   Tutorial: Adafruit WS2812B NeoPixels with the Freescale FRDM-K64F Board – Part 1: Hardware Tutorial: Adafruit WS2812B NeoPixels with the Freescale FRDM-K64F Board – Part 2: Software Tools Tutorial: Adafruit WS2812B NeoPixels with the Freescale FRDM-K64F Board – Part 3: Concepts Tutorial: Adafruit WS2812B NeoPixels with the Freescale FRDM-K64F Board – Part 4: Timer Tutorial: Adafruit WS2812B NeoPixels with the Freescale FRDM-K64F Board – Part 5: DMA The tutorials go though the hardware setup, Kinetis Design Studio, debugging the first project, using the Kinetis SDK, how to set up the Flex Timer Module (FTM) and how to use the Kinetis eDMA to generate the timing and bitstream to drive the WS2812B LED stripes.   I hope you find this useful, and you learn from this for your next design.   Happy Kinetising 🙂
View full article
For the Windows version of SDK, I was not able to use the OpenSDA with CMSIS-DAP running on the FRDM-KL25Z.. The Quick Start guide Figure 12 shows the a blank field for "Other options". You must enter "-f kinetis.cfg" here or you will not be able to debug. See below.
View full article
LCD Timer in KDS   Description:   A project made in KDS using the FRDM-MKL46Z256VLL4 board's LCD screen as a timer. The LCD will display minutes and seconds from 00:00 to 99:59, before resetting to 00:00.   Sections of code taken from an example project found at: https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/FRDM-KL46Z/FRDM-KL46Z_Demo
View full article
This document is a step by step to install KDS.
View full article
  Hello Freedom community users Bheema has posted on the Element14 community a very clear tutorial (accessible following the link below) to create from scratch a basic project example for the FRDM-K64 with Kinetis Design Studio (KDS). Freescale Freedom development platform: [FRDM-K... | element14 I strongly recommend you to start following those steps to properly setup the tool and the OpenSDAv2 interface embedded in the new Freedom and TWR boards. Happy Programming Greg
View full article
Accelerometer in KDS   Description:   A project made in KDS using the FRDM-MKL46Z256VLL4 board's LCD screen to display accelerometer data. The LCD will initially display the accelerometer data for the X axis. Pressing SW3 will toggle between displaying other axis. A timer has also been included from my previous project. Pressing the SW1 at any time will reset the timer back to 0.   Sections of code taken from an example project found at: https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/FRDM-KL46Z/FRDM-KL46Z_Demo
View full article
Since last year, I have received several same cases from customers when using KSDK1.2/KSDK1.3 and KDS3.0 with MK02FN128. When create a new MK02FN128 KSDK project with  SDK Project Generator (http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/development-platforms-with-mbed/software-development-kit-for-kinetis-mcus:KINETIS-SDK?fpsp=1&tab=Design_Tools_Tab ) or KDS3.0 project wizard, even the new created project has build errors:   When we use KSDK,  ksdk_platform_lib_xxxx must be built for the specific SoC being used in the new created KSDK platform. For K02F12810, this library project file is under: C:\Freescale\KSDK_1.3.0\lib\ksdk_platform_lib\kds\K02F12810   Open ksdk_platform_lib_K02F122810 with KDS3.0, there is wrong setup in ksdk_platform_lib_K02F12810 properties setting: the default target processor is cortex-m0plus!   Because K02 is cortex m4 core, obviously we need modify ksdk_platform_lib_K02F12810 target setting to cortex-m4 instead:   After above revise, rebuild the library project.  Then rebuild user project. The errors are gone.   If user needs to use K02F12810 ksdk_hal_lib_K02F12810 or ksdk_startup_lib_K02F122810 library, they need revise ARM family core to cortex-m4 accordingly. These two libraries project files are under: C:\Freescale\KSDK_1.3.0\lib\ksdk_hal_lib\kds\K02F12810 C:\Freescale\KSDK_1.3.0\lib\ksdk_startup_lib\kds\K02F12810   I have tested all the KSDS1.3 library projects. This defect is only in K02F12810 . NXP doesn’t have K02F FRDM board so far, User can download K02F128 project to FRDM-K22F board without problem. I suggest user use K02F128 project+FRDM-K22F board to start a project. For more information on this related, see application note: http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5040.pdf “Using the FRDM-K22F to Evaluate K02 and K22FN Devices Hardware and Software Considerations”
View full article
NOTE: with the release of KDS V1.1.0 this quickstart is depreciated!   Note that this quickstart guide is an update/newer version than the one installed by the installer.
View full article
This is an ISF2.1 Project that goes with the blog post titled "Creating a Data Logger embedded application using ISF 2.1".
View full article
Recently I received two cases from Kinetis users. They both meet problem when porting Kinetis Interrupt project from CodeWarrior 10.x to KDS. There is a document KDS_Porting_Guide.pdf under KDS install folder which covers this topic. However I know many customers still have difficulty even they follow the document steps. This scenario is normal; because users’ projects are various, we can’t expect one porting document solve all kinds of problem of individuals. For me, honestly, I seldom use this porting guide to port my project. I prefer porting my project all by hand. Thus I can know my project changes from up to bottom. Thus even if I meet problem later, I can still position it easily and quickly. For the reason of time, in this article, I will focus on how to port Kinetis Interrupt from CodeWarrior to KDS by hand. Some NVIC register definition name and file structure are different in CodeWarrior and KDS. One big difference is that KDS uses core file from ARM limited directly. I summarized the difference as below table. It’s good to know the basic difference before we start the porting.       CodeWarrior KDS NVIC Register Definition :   Where MCU header file. Eg: MK60N512VMD100.h ARM Core file. Eg: core_cm4, core_cm0plus.h Written by NXP(former Freescale) ARM Limited Sample of usage NVICISERx = 0x01 NVIC->ISER[x] = 0x01 Packaged in NVIC_EnableIRQ(n) Vector Table Definition: Where Kinetis_sysinit.c Startup_MK60D10.S Language Using C Assembly Interrupt handler name Defined by user Defined by KDS. Eg, PORTA_IRQHandler Allow user modify. For more, see attached document.
View full article
Introduction   OpenOCD is the PC host application that is used by OpenSDAv2 (CMSIS-DAP application) for debugging. The standard installation of KDS does not include support for debugging the K22FN512 & K24FN256 device families via OpenOCD. This document will guide a KDS user through updating OpenOCD, bundled in KDS, to provide support for the K22FN512 & K24FN256 device families. In addition, we will show the user how to re-configure a KDS project to use OpenOCD to debug with CMSIS-DAP on a FRDM-K22F development board.   Requirements   The following CMSIS-DAP versions are required for this version of OpenOCD:   Development Board CMSIS-DAP Version FRDM-K22F 0203 TWR-K22F120M 0203 TWR-K24F120M ff03   Updating OpenOCD   First the user must locate their installation of KDS. On Windows machines, the default installation directory is “C:\Freescale\KDS_1.1.1”. For Linux users, the default installation folder is “opt/Freescale/KDS_1.1.1”. Inside this installation, you should see the same directories and files as seen in the figure below. Note: before continuing you must stop any debugging sessions and shutdown KDS.   Figure 1: Default KDS_1.1.1 installation directory.   In Figure 1, you can see the folder named “openocd”. This contains all the files necessary for OpenOCD to run in KDS. Before we install the updated version of OpenOCD we must rename the “openocd” folder. This way we have the old version of OpenOCD, should you feel the need to return.   Figure 2: Renamed "openocd" folder.   Once the “openocd” folder is renamed, as in Figure 2, we then need to download the “kds-openocd-update-09-04-14.zip” file attached to this document. Save this file into the KDS installation directory, as in Figure 3.   Figure 3: KDS OpenOCD update in KDS installation.   Once downloaded, extract the “openocd” folder for your operating system into the KDS installation directory. Figure 4 shows where the updated “openocd” folder is located for Windows users.   Figure 4: Location of updated OpenOCD folder for Windows.   Once the new “openocd” folder is copied to your KDS installation the update process is complete. OpenOCD in KDS now supports the K22F family of devices. It is now possible for FRDM-K22F users to debug their KDS projects with CMSIS-DAP via OpenOCD. Figure 5 shows the KDS installation folder after successfully updating OpenOCD.   Figure 5: Updated KDS installation.   Preparing projects for debugging with OpenOCD   Now a quick walkthrough on how to configure KDS projects to debug using OpenOCD. We will assume that the user already has a project in their workspace.[1] The first step is to highlight the desired project, and then select “Debug Configurations…” from the Debug drop down.   Figure 6: Open "Debug Configurations..."   Once the “Debug Configurations” menu pops up on your screen, select “GDB OpenOCD Debugging”, then click on the “New Launch configuration” button in the upper left of the window. Figure 7 shows where these items are located.   Figure 7: Create a new GDB OpenOCD Debugging configuration.   The new debug configuration should automatically pull in information from the selected project. If an .elf file exists for the project, then the “C/C++ Application” and “Project” fields will be populated as in Figure 8.   Figure 8: These fields should be generated automatically if the project has already been built.   If the “C/C++ Application” field is not populated, you can search your project for an .elf file using the “Search Project…” button below the “C/C++ Application” field. If no .elf exists, then it is necessary for the user to build the project to generate the .elf file.   Once the “Main” tab has been completed, it is time to move onto the “Debugger” tab. In the “Debugger” tab, it is necessary for the user to define the configuration file in the “Config options” field. For debugging in KDS, OpenOCD will need a configuration file, and the default configuration file is “kinetis.cfg”. Enter “-f kinetis.cfg” into the “Config options” field. Figure 9 shows the correct input for the “Config options” field. After populating the field, the user can now press the “Debug” button to begin debugging.   Figure 9: User must enter “Config options”.   If this is the first time debugging in the current workspace, a dialog box will appear prompting you to open the “Debug” perspective. You should check the “Remember my decision” box, and press the “Yes” button. This will allow KDS to switch to the “Debug” perspective, for you whenever you begin to debug an application. See Figure 10 for more detail.   Figure 10: Select to automatically change perspective when debugging.   Figure 11, below, shows a successful debug connection to the target device using OpenOCD. The application has run to “main” and is waiting for the user to interact with the debug session.   Figure 11: Once debugger has connected and run to main.   Summary   After completing the steps in the sections above, a KDS user should be able to debug applications using OpenOCD and CMSIS-DAP with K22FN512 & K24FN256 device families. For more information on KSDK and KDS please consult the documentation located in C:\Freescale\KSDK_1.0.0\doc and C:\Freescale\KDS_1.1.1\doc\pdf, respectively.   [1] For directions on importing an existing KSDK demo to KDS please consult the device family specific user’s guides in “C:\Freescale\KSDK_1.0.0\doc”, and on creating new KDS projects consult the “kds_user_guide” in “C:\Freescale\KDS_1.1.1\doc\pdf”. Original Attachment has been moved to: kds-openocd-update-09-04-14.zip
View full article
If you are migrating from CodeWarrior to KDS, then you might notice that CodeWarrior had a 'Add Files...' menu: KDS is using an unmodified Eclipse version, and because the above menu was a CodeWarrior specific extension, this menu is not present in Eclipse. But there are many different other ways in Eclipse how to add existing files to a project in KDS: File Import Menu Drag and Drop Copy and Paste See How to Add Existing Files to Eclipse Projects | MCU on Eclipse   Happy Adding 🙂
View full article
In KDS and Codewarrior for MCU GCC build, linker will initialize RAM after reset, the enter main function. However in some application,  User doesn’t want linker initialize data section. A typical case is when in a bootloader+application combined project, the two program need share the same RAM memory - user application writes data to a shared RAM then invoke bootloader by software reset,  bootloader can read the exact data out. The data in shared RAM are not being overwritten by bootloader linker initialization.This article will introduce two methods about how to add uninitialized data section to GCC build.   Method 1. Use NOLOAD keyword in linker file: NOLOAD : The section should be marked as not loadable, so that it will not be loaded into memory when the program is run. For example in below section .buffram and .bss2 are addressed as “NOLOAD” and doesn’t need to be loaded when the program starts to run. For detail, see article on MCU on Eclipse: http://mcuoneclipse.com/2014/04/19/gnu-linker-can-you-not-initialize-my-variable/   Method 2. Use  pointer in C code for uninitialized RAM. This method doesn’t use NOLOAD. Here are the steps to utilize it: Step1: don’t define uninitialized RAM in linker file. Step2: in C file, use point to access the uninitialized address.   For detail, see attached document with demo listed.
View full article
More and more customers now use the ARM MBED develop Internet of Things(IoT) and embedded devices, also includes the kinetis chips. While this development tool only supports writing and compile code , not supports debug project. The good news is now we can export the project to KDS, we can debug it on KDS IDE. Below is the steps how to do it .
View full article