Mtrdevkspnk144 development of motor control system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mtrdevkspnk144 development of motor control system

Jump to solution
3,189 Views
47772614
Contributor II

I use mtrdevkspnk144 platform to develop motor control system. I want to control motor speed through freemaster variable. In the PMSM_appfreemaster_TSA. H or freemaster_TSA. H file, which variable stores the target speed of the motor transmitted by freemaster?

1 Solution
3,072 Views
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

View solution in original post

4 Replies
3,073 Views
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

3,072 Views
47772614
Contributor II

Thinks for your help!

0 Kudos
Reply
3,072 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear customer, 

this question is not related so much to FreeMASTER as it is a general tool and framework for runtime visualization and control of embedded applications. I will try to redirect the question to author of the Mtrdevkspnk144 application.

3,072 Views
47772614
Contributor II

Thinks for your help!

0 Kudos
Reply