Mtrdevkspnk144 development of motor control system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mtrdevkspnk144 development of motor control system

ソリューションへジャンプ
3,180件の閲覧回数
47772614
Contributor II

I use mtrdevkspnk144 platform to develop motor control system. I want to control motor speed through freemaster variable. In the PMSM_appfreemaster_TSA. H or freemaster_TSA. H file, which variable stores the target speed of the motor transmitted by freemaster?

1 解決策
3,063件の閲覧回数
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

元の投稿で解決策を見る

4 返答(返信)
3,064件の閲覧回数
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

3,063件の閲覧回数
47772614
Contributor II

Thinks for your help!

0 件の賞賛
返信
3,063件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear customer, 

this question is not related so much to FreeMASTER as it is a general tool and framework for runtime visualization and control of embedded applications. I will try to redirect the question to author of the Mtrdevkspnk144 application.

3,063件の閲覧回数
47772614
Contributor II

Thinks for your help!

0 件の賞賛
返信