Mtrdevkspnk144 development of motor control system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Mtrdevkspnk144 development of motor control system

跳至解决方案
3,176 次查看
47772614
Contributor II

I use mtrdevkspnk144 platform to develop motor control system. I want to control motor speed through freemaster variable. In the PMSM_appfreemaster_TSA. H or freemaster_TSA. H file, which variable stores the target speed of the motor transmitted by freemaster?

1 解答
3,059 次查看
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

在原帖中查看解决方案

4 回复数
3,060 次查看
marekmusak
NXP Employee
NXP Employee

Dear customer, 

Rotor speed can be controlled through FreeMASTER variable "Speed Required".

3,059 次查看
47772614
Contributor II

Thinks for your help!

0 项奖励
回复
3,059 次查看
MichalH
NXP Apps Support
NXP Apps Support

Dear customer, 

this question is not related so much to FreeMASTER as it is a general tool and framework for runtime visualization and control of embedded applications. I will try to redirect the question to author of the Mtrdevkspnk144 application.

3,059 次查看
47772614
Contributor II

Thinks for your help!

0 项奖励
回复