MPC5604B JTAG uncensoring through USB Multilink in FreeMASTER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604B JTAG uncensoring through USB Multilink in FreeMASTER

2,272 次查看
ginzhou
Contributor I

Hi

  I have a problem to connect MPC5604B through USB Multilink in FreeMASTER. I cannot find the option to enter JTAG password in FreeMASTER. So i tried to uncensor the device in PROGPPCNEXUS first, but it's not useful, although it's connected, but the value of variables is not correct, meaningless. XCP is disabled, so i cannot connect through CAN bus either. How can i connect a censored device in FreeMASTER?

Thank you.

标记 (3)
0 项奖励
回复
1 回复

2,148 次查看
iulian_stan
NXP Employee
NXP Employee

Hi ginzhou‌,

Frankly speaking, we (FreeMASTER developers) never worked with censored devices. From your explanation I understand that they are password protected which implies a different connection flow or passing an additional property in the standard flow - this is not supported by the connection plugin.

Sorry for the delayed reply,

Iulian

0 项奖励
回复