FRDM Training Hub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM Training Hub

FRDM Training Hub


Restricted Beta Program

  • Comprehensive software and tools for seamless prototyping and rapid development
  • Scale your project with modular, quick-start FRDM and expansion boards
  • Leverage our application code hub or GoPoint to access 180+ code snippets and demos

  • Leverage FRDM Training Hub to learn from the experts
  • Not sure where to start ?

ディスカッション

ソート順:
MCXW71 is a three-core platform that integrates a Cortex-M33 application core (CM33), a dedicated Cortex-M3 radio core, and an isolated EdgeLock Secure Enclave. The radio core, also called as Narrow Band Unit (NBU) features a Bluetooth Low Energy (LE) unit with a dedicated flash. The memories integrated in the NBU consist of Bluetooth LE controller stack and radio drivers. On MCXW71, only boot ROM has access to the NBU flash. The ROM bootloader provides an in-system programming (ISP) utility that operates over a serial connection on the microcontroller units (MCUs) This hands-on describes how to update the code in NBU and the User firmware using the ISP. Lab guide: FRDM-MCXW71_NBU_and_User_Firmware_Update_Using_ISP
記事全体を表示
Introduction   This hands-on video explains how to take a trained AI model and deploy it for NPU-accelerated inference using eIQ Neutron on the FRDM i.MX 95 PRO development board. YOLOv8n is used as the example model. The video covers the complete workflow, including host setup, model export, calibration, INT8 quantization, Neutron compilation, board deployment, benchmarking, and troubleshooting. By the End of This Training, You Will Be Able To Understand the main components of the eIQ Neutron-S hardware and software stack. Download and export a YOLOv8n model to TFLite. Quantize the model to INT8 for Neutron NPU execution. Compile the quantized model for the i.MX 95 target. Review compiler statistics and determine which operations are delegated to the NPU. Deploy the model, delegate, driver, and firmware to the board. Run CPU and NPU benchmarks. Compare inference latency and calculate the NPU speed-up.   Hardware and Prerequisites   Before starting the training, verify that you have the required development board, host system, network connection, model, calibration data, and software tools. Development Board   FRDM i.MX 95 PRO development board. NXP BSP LF6.18.20 2.0.0. eIQ Neutron runtime compatible with Neutron SDK 3.2.1 or later. TensorFlow Lite 2.19.0 benchmark application. Ethernet or USB-CDC connectivity. SSH and SCP access to the board. Root access on the target system. Linux Host Computer   Ubuntu 20.04 or Ubuntu 22.04 is recommended. Python 3.8 or later. Python virtual environment support. SSH and SCP command-line tools. Sufficient storage for the SDK, models, calibration images, and generated artifacts.     Watch the Complete Training Video   Watch the video from beginning to end and execute the commands in the presented order. Each stage generates an artifact required by the next stage.     Command Cheat Sheet   The following commands are organized in execution order. Replace placeholders such as <board-ip> with the values for your environment. 1. Download and Configure the Neutron SDK   # Extract the SDK archive unzip eiq-neutron-sdk-linux-3.2.1.zip # Enter the SDK directory cd eiq-neutron-sdk-linux-3.2.1 # Add the SDK tools to PATH for the current terminal export PATH="$PWD/bin:$PATH" # Optional: make the PATH configuration persistent echo 'export PATH="/path/to/eiq-neutron-sdk-linux-3.2.1/bin:$PATH"' >> ~/.bashrc # Reload the shell configuration source ~/.bashrc # Verify the SDK tools tflite-profiler --help tflite-quantizer --help neutron-compiler --help   2. Create the Python Environment   # Create a Python virtual environment python3 -m venv .venv # Activate the virtual environment source .venv/bin/activate # Upgrade pip python3 -m pip install --upgrade pip # Install the required packages pip install generate-parameter-library-py \ ultralytics \ hf \ ai-edge-litert \ litert_torch \ numpy \ opencv-python   3. Download the YOLOv8n Model   # Download the trained YOLOv8n weights hf download Ultralytics/YOLOv8 yolov8n.pt --local-dir . # Verify the downloaded model ls -lh yolov8n.pt   4. Export YOLOv8n to TFLite   # Export the PyTorch model to TFLite yolo export model=yolov8n.pt format=tflite # Locate the generated TFLite model find . -name "*.tflite" -type f # Update the following commands if your exported # model uses a different file name or directory.   5. Download the COCO Calibration Dataset   # Create a directory for the calibration dataset mkdir -p coco cd coco # Download the COCO training images wget --no-check-certificate \ http://images.cocodataset.org/zips/train2017.zip # Extract the images unzip train2017.zip # Return to the project directory cd .. # Verify the image directory find ./coco/train2017 -type f -name "*.jpg" | head   6. Create the Calibration Conversion Script   Save the following script as jpg2bin.py . It converts the JPEG calibration images into raw binary tensors expected by the profiler. #!/usr/bin/env python3 import argparse import glob import os import random import cv2 import numpy as np def letterbox(image, new_shape=640, color=(114, 114, 114)): height, width = image.shape[:2] ratio = min(new_shape / height, new_shape / width) resized_height = int(round(height * ratio)) resized_width = int(round(width * ratio)) resized = cv2.resize( image, (resized_width, resized_height), interpolation=cv2.INTER_LINEAR, ) canvas = np.full( (new_shape, new_shape, 3), color, dtype=np.uint8, ) top = (new_shape - resized_height) // 2 left = (new_shape - resized_width) // 2 canvas[ top:top + resized_height, left:left + resized_width, ] = resized return canvas def main(): parser = argparse.ArgumentParser( description="Convert JPEG images to YOLOv8n calibration tensors." ) parser.add_argument( "--images", default="./coco/train2017", help="Directory containing the calibration JPEG images.", ) parser.add_argument( "--out", default="./calib_yolov8n", help="Output directory for the binary tensors.", ) parser.add_argument( "--num", type=int, default=1000, help="Maximum number of calibration images.", ) parser.add_argument( "--size", type=int, default=640, help="Model input width and height.", ) parser.add_argument( "--shuffle", action="store_true", help="Shuffle the image list before selecting images.", ) args = parser.parse_args() os.makedirs(args.out, exist_ok=True) files = sorted( glob.glob(os.path.join(args.images, "*.jpg")) ) if args.shuffle: random.seed(0) random.shuffle(files) files = files[:args.num] if not files: raise RuntimeError( f"No JPEG images were found in {args.images}" ) for index, file_path in enumerate(files): image = cv2.imread(file_path) if image is None: print(f"Skipping unreadable image: {file_path}") continue # Convert BGR to RGB. image = cv2.cvtColor(image, cv2.COLOR_BGR2RGB) # Letterbox resize to 640 x 640. image = letterbox(image, args.size) # Convert to float32 and normalize to [0, 1]. tensor = image.astype(np.float32) / 255.0 # Add batch dimension. # Final layout: 1 x 640 x 640 x 3, NHWC. tensor = np.expand_dims(tensor, axis=0) output_path = os.path.join( args.out, f"calib_{index:05d}.bin", ) tensor.tofile(output_path) print( f"Calibration tensors written to: {args.out}" ) if __name__ == "__main__": main() # Make the script executable chmod +x jpg2bin.py # Generate up to 1000 calibration tensors python3 jpg2bin.py \ --images ./coco/train2017 \ --out ./calib_yolov8n \ --num 1000 \ --size 640 \ --shuffle # Count the generated binary files find ./calib_yolov8n -type f -name "*.bin" | wc -l # Check the size of a generated tensor ls -lh ./calib_yolov8n | head   7. Inspect the TFLite Input and Output Tensors   python3 - <<'PY' from ai_edge_litert.interpreter import Interpreter model_path = "yolov8n.tflite" interpreter = Interpreter(model_path=model_path) interpreter.allocate_tensors() print("Input details:") for tensor in interpreter.get_input_details(): print(tensor) print("\nOutput details:") for tensor in interpreter.get_output_details(): print(tensor) PY Record the exact input tensor name reported by the model. Replace serving_default_args_0 in the profiling command if your model uses a different name.   8. Profile the Floating-Point TFLite Model   # Replace serving_default_args_0 if the model # reports a different input tensor name. tflite-profiler \ --input yolov8n.tflite \ --dataset serving_default_args_0,calib_yolov8n \ --output yolov8n_profile.csv # Verify that the profiling CSV was generated ls -lh yolov8n_profile.csv # Preview the beginning of the profile head yolov8n_profile.csv   9. Quantize the Model to INT8   # Generate the INT8 TFLite model tflite-quantizer \ --input yolov8n.tflite \ --profile yolov8n_profile.csv \ --output yolov8n_quant.tflite # Compare the model file sizes ls -lh yolov8n.tflite yolov8n_quant.tflite   10. Verify the Quantized Model   python3 - <<'PY' from ai_edge_litert.interpreter import Interpreter model_path = "yolov8n_quant.tflite" interpreter = Interpreter(model_path=model_path) interpreter.allocate_tensors() print("Quantized input details:") for tensor in interpreter.get_input_details(): print("Name:", tensor["name"]) print("Shape:", tensor["shape"]) print("Data type:", tensor["dtype"]) print("Quantization:", tensor["quantization"]) print() print("Quantized output details:") for tensor in interpreter.get_output_details(): print("Name:", tensor["name"]) print("Shape:", tensor["shape"]) print("Data type:", tensor["dtype"]) print("Quantization:", tensor["quantization"]) print() PY   11. Compile the Model for the Neutron NPU   # Compile the INT8 model for the i.MX 95 Neutron NPU neutron-compiler \ --input yolov8n_quant.tflite \ --output yolov8n_neutron.tflite \ --target imx95 # Verify the generated model ls -lh yolov8n_neutron.tflite Generate Compiler Statistics # Generate compiler and delegation statistics neutron-compiler \ --input yolov8n_quant.tflite \ --output yolov8n_neutron_stats.tflite \ --target imx95 \ --dump-statistics # Review the compiler output and record: # 1. Number of delegated nodes # 2. Number of CPU fallback nodes # 3. Unsupported operators # 4. Generated NeutronGraph partitions Create a Profiling Build # Compile a profiling-enabled model neutron-compiler \ --input yolov8n_quant.tflite \ --output yolov8n_neutron_prof.tflite \ --target imx95 \ --use-profiling # Verify all generated models ls -lh yolov8n_quant.tflite \ yolov8n_neutron.tflite \ yolov8n_neutron_prof.tflite   12. Configure the Board IP Address   # Replace the example address with the board IP address export BOARD_IP="192.168.1.100" # Verify network connectivity ping -c 4 "$BOARD_IP" # Test the SSH connection ssh root@"$BOARD_IP"   13. Create the Deployment Directory   # Create the working directory remotely ssh root@"$BOARD_IP" \ "mkdir -p /root/neutron_demo"   14. Copy Runtime Artifacts to the Board   The driver, delegate, and firmware may already be included in the BSP. Copy them only when the required or matching versions are not already installed. # Copy the Neutron driver scp libNeutronDriver.so \ root@"$BOARD_IP":/lib/ # Copy the Neutron delegate scp libneutron_delegate.so \ root@"$BOARD_IP":/usr/lib/ # Copy the Neutron firmware scp NeutronFirmware.elf \ root@"$BOARD_IP":/lib/firmware/ # Copy the plain INT8 model for the CPU baseline scp yolov8n_quant.tflite \ root@"$BOARD_IP":/root/neutron_demo/ # Copy the Neutron-compiled model scp yolov8n_neutron.tflite \ root@"$BOARD_IP":/root/neutron_demo/ # Optional: copy the profiling-enabled model scp yolov8n_neutron_prof.tflite \ root@"$BOARD_IP":/root/neutron_demo/   15. Verify the Files on the Board   # Connect to the board ssh root@"$BOARD_IP" # Enter the deployment directory cd /root/neutron_demo # Verify the models ls -lh /root/neutron_demo/ # Check the driver ls -lh /lib/libNeutronDriver.so # Check the delegate ls -lh /usr/lib/libneutron_delegate.so # Check the firmware ls -lh /lib/firmware/NeutronFirmware.elf # Refresh the shared-library cache ldconfig # Verify that the delegate is visible to the loader ldconfig -p | grep -i neutron   16. Check the BSP and Runtime Environment   # Display the Linux distribution and BSP information cat /etc/os-release # Display the kernel version uname -a # Search for Neutron-related kernel messages dmesg | grep -i neutron # Search for firmware-related messages dmesg | grep -i firmware # Locate the TensorFlow Lite benchmark application find /usr/bin -name "benchmark_model*" -type f 2>/dev/null   17. Run the CPU Baseline   cd /root/neutron_demo /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model \ --graph=yolov8n_quant.tflite \ --num_threads=4 \ --num_runs=50 Record the average inference latency, minimum latency, maximum latency, initialization time, and memory information reported by the benchmark.   18. Run the NPU Benchmark   cd /root/neutron_demo /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model \ --graph=yolov8n_neutron.tflite \ --external_delegate_path=/usr/lib/libneutron_delegate.so \ --num_runs=50 Confirm that the benchmark output reports that the external delegate was loaded and that one or more model partitions were delegated.   19. Save Benchmark Results   # Save the CPU benchmark output /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model \ --graph=yolov8n_quant.tflite \ --num_threads=4 \ --num_runs=50 \ 2>&1 | tee cpu_benchmark.txt # Save the NPU benchmark output /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model \ --graph=yolov8n_neutron.tflite \ --external_delegate_path=/usr/lib/libneutron_delegate.so \ --num_runs=50 \ 2>&1 | tee npu_benchmark.txt # Review the saved results cat cpu_benchmark.txt cat npu_benchmark.txt   20. Calculate the NPU Speed-Up   Use the average latency reported by each benchmark: Speed-up = CPU average latency / NPU average latency Example: CPU average latency = 100 ms NPU average latency = 10 ms Speed-up = 100 / 10 Speed-up = 10x     Required Deployment Artifacts   Artifact Example File Purpose Neutron driver libNeutronDriver.so Communicates with the Neutron firmware and passes model buffers, weights, kernels, and input or output data. Neutron delegate libneutron_delegate.so Connects TensorFlow Lite to the Neutron runtime and delegates supported NeutronGraph operations to the NPU. Neutron firmware NeutronFirmware.elf Runs on the dedicated RISC-V core and executes the generated Neutron microcode. Quantized TFLite model yolov8n_quant.tflite Provides the CPU baseline and serves as the input to the Neutron compiler. Neutron-compiled model yolov8n_neutron.tflite Contains NeutronGraph operations generated for NPU execution.   Troubleshooting   Use the following table to identify common host, model, compilation, deployment, and runtime problems. Area Problem Possible Cause Recommended Solution Host setup SDK commands are not found. The SDK bin directory is not included in PATH . Run export PATH="$PWD/bin:$PATH" from the SDK directory. Add the absolute SDK path to ~/.bashrc if the configuration must persist. Python environment A required Python module cannot be imported. The virtual environment is not active or the package was installed in a different environment. Run source .venv/bin/activate . Verify the active interpreter with which python3 , and reinstall the missing dependency with pip install PACKAGE_NAME . Model export The expected yolov8n.tflite file cannot be found. The exporter created a subdirectory or used a different filename. Run find . -name "*.tflite" -type f . Update the following commands to use the actual exported model path. Calibration No calibration binary files are generated. The image directory is incorrect or does not contain JPEG files. Verify the directory with find ./coco/train2017 -name "*.jpg" | head . Pass the correct directory through the --images argument. Calibration The calibration tensor has the wrong shape or size. The resize, batch dimension, layout, or data type is incorrect. Confirm an NHWC tensor with shape 1 x 640 x 640 x 3 , RGB channel order, float32 data, and values normalized to [0, 1] . Calibration The quantized model produces inaccurate predictions. The calibration preprocessing differs from inference preprocessing. Verify letterbox resizing, padding color, RGB conversion, normalization, tensor layout, input size, and data type. Use representative images that match the intended application. Profiler The profiler reports an invalid or unknown input tensor. The tensor name in --dataset does not match the model input name. Inspect the model input details with the TFLite interpreter. Replace serving_default_args_0 with the exact name reported by the model. Profiler The profiler cannot read the calibration files. The dataset path is incorrect, the folder is empty, or the binary format does not match the input tensor. Verify the folder path, count the files, and confirm the expected number of bytes for each tensor. Quantization The quantized model still uses floating-point tensors. The model was not fully quantized or the generated profile is incomplete. Re-run profiling with valid calibration data. Inspect the input, output, and intermediate tensor data types before compiling the model. Compilation neutron-compiler fails. The input model is invalid, not INT8, or contains unsupported quantization parameters. Confirm that the input is the quantized TFLite model. Inspect its tensor types and quantization parameters, then run the compiler again with statistics enabled.   Conclusion   Congratulations! You have completed the end-to-end workflow for deploying and running an AI model on the eIQ Neutron-S NPU integrated into the FRDM i.MX 95 PRO. Throughout this training, you learned how to prepare the Linux host environment, export YOLOv8n to TFLite, build a representative calibration dataset, quantize the model to INT8, and compile it for the i.MX 95 target. You also learned how to transfer the required runtime artifacts to the board and compare CPU and NPU inference performance. This workflow is not limited to YOLOv8n. You can use the same process as a starting point for deploying your own computer vision models. However, each model must be evaluated individually because input formats, preprocessing requirements, quantization behavior, and operator support may differ. Recommended Next Steps   Validate the accuracy of the INT8 model against the original floating-point model. Review the compiler statistics to identify unsupported operations and CPU fallback sections. Measure end-to-end application performance, including preprocessing, inference, and post-processing. Test the workflow with your own model and a calibration dataset that represents your real application. Use a profiling-enabled build to identify the most expensive layers and potential performance bottlenecks.
記事全体を表示
  Introduction   This hands-on walks you through everything that happens before you ever write a line of application code: unboxing your FRDM i.MX 95 Pro board, getting acquainted with its layout and ports, powering it on, and confirming a healthy first boot from the on-board eMMC. By the time you are done, you will be comfortable using both the i.MX System Manager console and the Linux command line to confirm exactly what hardware you have in front of you. By the end you will be able to: Verify that the contents of your FRDM i.MX 95 Pro box are complete Get acquainted with the board, its peripherals, and ports Set up and boot the board for the first time Get familiar with the i.MX System Manager (SM) console and the Linux CLI Verify the board's hardware and resources using Linux commands Hardware & Prerequisites You need very little to get started: FRDM-IMX95-PRO board (the box) — in addition to the board itself, the box includes USB-C cables for power and debugging, mounting standoffs, the IW612 wireless module, and a documentation card linking to the product page and a getting-started tutorial. Power supply — a USB-C to USB-C cable is included in the box. For basic bring-up, any standard USB-C phone charger is sufficient. If your setup adds higher-power accessories (e.g., a display), use a 100 W-capable USB-C power adapter instead. PC host — a computer with a terminal / serial console program to connect to the board's debug port. That's it — no display or camera is required for this hands-on. Watch the Module Video Watch the full hands-on walkthrough below, then follow along on your own board.   Steps to Run the Hands-On Step 1: Explore the Board with Linux Commands Once the board has booted, open a terminal on the debug console and run the following commands to confirm the Linux environment and the hardware resources available to you. # 1) Linux version uname -a # 2) Storage devices lsblk # 3) Verify CPU numbers and architecture. lscpu # 4) SoC Id and Family cat /sys/devices/soc0/soc_id cat /sys/devices/soc0/family # 5) RAM memory available cat /proc/meminfo | head -20 # 6) network peripherals and addresses ip addr # 7) List Video Encoders and Decoders v4l2-ctl --list-devices # 8) GPU specs and capabilities vulkaninfo --summary # 9) Print available GPIOs gpioinfo Step 2: Explore the i.MX System Manager Console Next, switch to the i.MX System Manager (SM) console to inspect the board at the system level — Logical Machines, boot times, power rails, and clocks. # 1) System manager version, Board, Revision, Silicon etc info # 2) Logical Machines information lm info # 3) Boot time of each Logical machine btime # 4) Power status of each peripheral power.r # 5) Clocks status clock.r Troubleshooting Symptom What to check Power LED is on but there is no output on the console Check the Boot Mode switches (set them to eMMC) Power-cycle the board (turn it off and back on) after changing the Boot Mode switches Verify the serial console baud rate is set to 115200 Confirm the Debug port is connected to the host PC Open all the COM ports exposed by the board when the Debug port is connected to the host PC Conclusion In this hands-on, you: Verified the contents of your FRDM i.MX 95 Pro box Got acquainted with the board, its peripherals, and ports Set up and booted the board for the first time from eMMC Used the i.MX System Manager console and the Linux CLI to inspect the board Confirmed the board's hardware and resources via Linux commands If you have not already, watch the module video above for the full walkthrough, and check out the rest of the FRDM Training Hub for the next hands-on in the series.
記事全体を表示
  Introduction This hands-on walks you through bringing a display to life on the FRDM-IMX95-PRO board. You will flash a BSP image to an SD card, attach a Waveshare 7" DSI LCD, select the correct device tree in U-Boot, and then exercise the panel with brightness control, screen rotation, capacitive touch, and a live camera video pipeline. By the end you will have a fully working touch display and the core skills to configure DSI panels on i.MX 95. By the end of this hands-on you will be able to: Flash a BSP image to a microSD card using UUU in Serial Download mode. Connect the Waveshare 7" DSI display (FPC, power, and I2C) correctly. Select the matching device tree for the panel from the U-Boot prompt. Adjust and script the display backlight brightness. Rotate the screen through Weston's configuration. Verify capacitive touch with evtest . Stream live camera video to the panel with GStreamer. Hardware & Prerequisites FRDM-IMX95-PRO board. MicroSD card — 16 GB or larger. Waveshare 7" DSI LCD — 1024×600 IPS, 5-point capacitive touch. 22-pin FPC cable. Host PC with UUU installed. Watch the Module Video Watch the full hands-on walkthrough first to see each step performed on real hardware, then follow along on your own board using the steps below. Steps to Run the Hands-On 1. Enter Serial Download Mode Put the board into Serial Download Protocol (SDP) mode so the host can push the image, then connect it to your PC: Set boot switch SW1 = 1000 (Serial Download Protocol mode). Connect J7 USB-C to the host PC. Connect J22 USB-C to view debug output on the serial console. 2. Flash the BSP Image with UUU Run the following command on your host computer to flash the BSP boot image and full image to the SD card: # --- UUU --- # Run the following command on your host computer uuu.exe –b sd_all imx-boot-imx95-19x19-lpddr5-frdm-pro-sd.bin-flash_a55 imx-image-full-imx95evk.wic.zst 3. Switch to SD Boot Once flashing completes, reconfigure the board to boot from the SD card: Power off the board. Set boot switches SW3 and SW4 = 0011 (SD card boot). Turn on the board. 4. Connect the Display — FPC Cable Attach the 22-pin FPC cable between the board and the Waveshare panel, paying close attention to cable orientation on each end: Connect the 22-pin FPC to the board's MIPI-DSI connector — the stiffener side faces the board connector. Connect the other end to the Waveshare panel (15-pin side) — the conductive side faces the panel. 5. Connect the Display — Power & I2C The panel needs both power and an I2C connection for the display output to come up: Connect I2C via the J6 4-pin header. Connect 5V power to J17 (or any 5V connector). I2C must be connected for display output to work. 6. Change the Device Tree in U-Boot Watch the serial console during boot and press any key at the U-Boot countdown to reach the prompt: Hit any key to stop autoboot: 3 => (U-Boot prompt) At the U-Boot prompt, select the device tree for the Waveshare panel and boot: # --- U-Boot: select the device tree for the display --- fatls mmc 1 setenv fdtfile imx95-19x19-frdm-pro-waveshare-7inch-c-panel.dtb saveenv boot 7. Set & Check Backlight Brightness Once Linux is running on the board, the panel backlight is exposed through sysfs. The commands below set a brightness value and read the current and maximum allowed values. Valid range is 0 (off) up to max_brightness . Run these as root: # --- Linux on board --- # Run the following command on the board # Path to the backlight /sys/class/backlight/3-0045/ # Set brightness echo 128 > /sys/class/backlight/3-0045/brightness # Read the current value cat /sys/class/backlight/3-0045/brightness # Read the maximum allowed value cat /sys/class/backlight/3-0045/max_brightness 8. Fun Example — Breathing Backlight For a quick visual test, this small script ramps the backlight up and down continuously, giving a "breathing" effect. Save it as breathe.sh , make it executable, and run it as root. Press Ctrl+C to stop. # --- Linux --- # Breathing back light # Create and open the file vi breathe.sh # Write the following lines into the bash script BL=/sys/class/backlight/3-0045 MAX=$(cat "$BL/max_brightness") while true; do for ((i=0; i<=MAX; i++)); do echo "$i" > "$BL/brightness"; sleep 0.01; done for ((i=MAX; i>=0; i--)); do echo "$i" > "$BL/brightness"; sleep 0.01; done done # Change the permissions of the bash script chmod +x breathe.sh # Run the bash script ./breathe.sh 9. Rotate the Screen (Weston) Display orientation is controlled in Weston's configuration file. Edit weston.ini , add an [output] section with the desired transform, then restart the service: # --- Linux --- # On board # File path /etc/xdg/weston/weston.ini # Open the file vi /etc/xdg/weston/weston.ini # Add the following [output] name=DPI-1 transform=rotate-90 # Valid formats # normal - 0 degrees (default) # rotate-90 - 90 degrees clockwise # rotate-180 - upside down # rotate-270 - 270 degrees clockwise # Reboot or restart the service systemctl restart Weston # Check the status of the service systemctl status weston You can confirm the panel resolution and active modes with modetest : # --- Linux --- # Check the panel resolution modetest -c # list connectors & modes # full DRM/KMS overview modetest # Look for the DSI/DPI connector and confirm # 1024x600 is listed as an active mode 10. Test Capacitive Touch (evtest) Run evtest with no arguments to list the available input devices, then select the touch screen's event number to start capturing touch events: # --- Linux --- # Touch screen evtest # Run the evtest command evtest # It will list the available devices Available devices: /dev/input/event0: scmi_dev.11 /dev/input/event1: Goodix Capacitive TouchScreen Select the device event number [0-1]: 1 # Then it will run the evtest of the touch screen 11. Display Camera Video (GStreamer) Stream live camera video to the panel to verify both the camera and the display path in one go: # --- Linux --- # Gstreamer pipe line for webcam # Run the following command gst-launch-1.0 v4l2src device=/dev/video52 ! video/x-raw,width=640,height=480 ! Glimagesink # Pipeline breakdown # v4l2src device=/dev/video52 - capture from V4L2 node # video/x-raw,width=640,height=480 - raw 640x480 video # glimagesink - render on display via OpenGL Troubleshooting Symptom What to check No display output Check FPC orientation — the stiffener side must face the board connector. Ensure the I2C bus (J6) is connected; it is required for display output. fatls mmc 1 fails Verify the SD card is inserted. Confirm SW3 and SW4 = 0011 (SD boot mode). "No such file or directory" at the backlight path Confirm the node name with ls /sys/class/backlight/ . Touch not working after screen rotation Add a calibration_matrix for the touch device in weston.ini , or configure the touch coordinate transform via libinput. Conclusion In this hands-on you brought up a Waveshare 7" DSI display on the FRDM-IMX95-PRO board from a fresh SD card flash all the way to a working touch panel with live camera video. Key takeaways: Flashed a BSP image to the SD card with UUU and switched the board to SD boot. Connected the DSI panel correctly (FPC orientation, 5V power, and the required I2C link). Selected the matching device tree in U-Boot so the panel enumerates at 1024×600. Controlled backlight brightness, rotated the display in Weston, validated touch with evtest , and verified the camera path with GStreamer. Be sure to watch the module video above to see each step in action, and explore the rest of the FRDM-IMX95-PRO Training Hub for more hands-on modules.
記事全体を表示
  FRDM i.MX 95 Pro · Hands-On Series GoPoint — Running Pre-Built Demos September 2026  |  FRDM i.MX 95 Pro Hands-On Series   Introduction Discover what your FRDM i.MX 95 Pro can do — right out of the box. This hands-on walks you through the full range of pre-built demo categories available through GoPoint on the FRDM i.MX 95 Pro board. From neural processing and machine learning to GPU-accelerated graphics, each demo showcases the real-world capabilities of NXP's i.MX 95 application processor — no custom code required. The hands-on covers the following topics: Launching GoPoint on the Weston desktop Exploring the available demo categories (NPU, ML, GPU) Running NPU demos with the Ara240 module Running ML and GPU demos By the end of this hands-on, you will be able to: Navigate the GoPoint interface on Weston Identify the available demo categories (NPU, ML, and GPU) Launch and run pre-built demos on your FRDM i.MX 95 Pro board Understand the hardware requirements for each demo type   Hardware & Prerequisites Before starting, make sure you have the following items ready: Required Hardware FRDM-IMX95-PRO board (booted from eMMC) HDMI display Mouse Keyboard USB camera Ara240 module (required for NPU demos) Optional Hardware EXPI-OS08A20 camera module — covered in the separate EXPI-OS08A20 Camera + ISP Pipeline hands-on Note: The board must be booted from eMMC with the pre-loaded BSP image before launching GoPoint. Ensure your display is connected via HDMI before powering on.   Watch the Hands-On Video A complete video walkthrough accompanies this hands-on. It demonstrates every step shown below — from opening GoPoint on Weston to running NPU, ML, and GPU demos live on the board. Watch it alongside the written steps for the best learning experience.   Steps to Run the Hands-On Follow the steps below to explore GoPoint and run the pre-built demos on your board. Step 1 — Launch GoPoint on Weston After the board boots into the Weston desktop environment, locate the GoPoint application icon on the desktop or in the application launcher. Click it to open the GoPoint demo browser. GoPoint provides a graphical interface that organises all available demos by category, making it easy to browse and launch them without any command-line interaction. Step 2 — Explore the Demo Categories Once GoPoint is open, you will see the main demo category tiles. The three primary categories available on the FRDM i.MX 95 Pro are: NPU Demos — Neural Processing Unit demos that leverage the Ara240 module for hardware-accelerated AI inference ML Demos — Machine learning demos running on the i.MX 95 application processor GPU Demos — Graphics Processing Unit demos showcasing GPU-accelerated rendering and compute Browse each category to see the individual demos available. Each demo tile shows its name, a brief description, and any special hardware it requires. Step 3 — Run NPU Demos (Ara240 Required) NPU demos require the Ara240 module to be attached to the board. Select any NPU demo from the GoPoint interface and click Run. GoPoint will automatically load the required AI model and launch the demo. The Ara240 module handles the neural network inference, delivering real-time results on-screen. Note: If AI/ML models are not yet present on the board, run the fetch_models command first (see the Troubleshooting section below). Step 4 — Run ML Demos ML demos run directly on the i.MX 95 application processor and do not require the Ara240 module. Select an ML demo from the GoPoint interface and click Run. These demos cover a range of machine learning use cases including image classification, object detection, and more. Step 5 — Run GPU Demos GPU demos showcase the graphics and compute capabilities of the i.MX 95's integrated GPU. Select a GPU demo from the GoPoint interface and click Run. These demos include GPU-accelerated graphics rendering and visual effects that highlight the board's multimedia performance.   Troubleshooting If you encounter issues while running GoPoint demos, use the table below to identify the symptom and the recommended action. Symptom What to Check Missing AI/ML models — demo fails to start or reports missing model files Fetch the required models using the commands below. Use --list to see available models and --repo-id to fetch a specific one: # List available models fetch_models --list # Fetch a specific model by repository ID fetch_models --repo-id Cannot download software requirements — network or SSL errors during model download The board's system clock may be incorrect, causing certificate validation to fail. Set the correct date and time, then retry: # Set the system date (replace with current date/time) date -s "MM/DD/YYYY HH:MM:SS" Board freeze — the board becomes unresponsive during a demo Reboot the board: reboot Corrupt download — a demo crashes immediately or shows unexpected errors after model download Remove the Python virtual environment ( venv ) for the affected demo and re-run it so GoPoint recreates a clean environment. The venv directory is located inside the demo's working folder. # Remove the venv of the corresponding demo, then relaunch it from GoPoint   Conclusion In this hands-on you explored the GoPoint application on the FRDM i.MX 95 Pro board and ran pre-built demos across three hardware-accelerated categories: Launched and navigated the GoPoint interface on the Weston desktop Ran NPU demos using the Ara240 neural processing module Ran ML demos on the i.MX 95 application processor Ran GPU demos showcasing the board's graphics capabilities Learned how to fetch AI/ML models and resolve common setup issues For a full visual walkthrough, watch the video in the Watch the Hands-On Video section above. To continue your learning journey, visit the FRDM i.MX 95 Pro Training Hub for the complete series of hands-on modules covering camera pipelines, connectivity, security, and more.
記事全体を表示
FRDM i.MX 95 Pro Hands-On: ARA240 DNPU AI Accelerator FRDM i.MX 95 Pro Hands-On Training Series  |  September 2026   Introduction This hands-on walks you through the ARA240 DNPU AI Accelerator integrated with the FRDM i.MX 95 Pro development board. The ARA240 is an M.2-form-factor neural processing unit that connects over PCIe and dramatically expands the board's AI inference capability — from classic computer-vision pipelines to large language models (LLMs) and vision-language models (VLMs) — all powered by NXP's eIQ software stack.   Item Details Host Board FRDM i.MX 95 Pro AI Accelerator ARA240 DNPU (up to 2 modules) BSP L6.18.20-2.0.0 (precompiled, available on the NXP website) Interface PCIe via M.2 Key-M slots J24 / J25   By the end of this hands-on you will be able to: Verify that the ARA240 DNPU is correctly detected by the system. List, download, and run AI models (CNN, LLM, VLM) on the accelerator. Measure DNPU performance metrics using the provided shell utilities. Configure and start the eIQ AAF Connector service to expose a REST API for AI inference. Send chat-completion requests to a locally running LLM through the connector's web interface. Troubleshoot the most common setup issues.   Hardware & Prerequisites Gather the following before starting: Hardware FRDM-IMX95-PRO development board ARA240 DNPU module (one or two, depending on your use case) Keyboard (for direct board interaction) Host machine with a web browser (to access the connector API UI) Internet connection (required for model downloads) M.2 Connector Reference Connector Purpose J24 M.2 Key-M slot — ARA240 Module #1 J25 M.2 Key-M slot — ARA240 Module #2 J9 Fan power supply for the module in J24 J10 Fan power supply for the module in J25 Software BSP L6.18.20-2.0.0 — precompiled image available on the NXP website.   Watch the Hands-On Video The video below walks through the complete ARA240 DNPU setup and demo flow on the FRDM i.MX 95 Pro, covering device detection, model download, inference testing, NPU metrics, and the eIQ AAF Connector in action. Watch it alongside the step-by-step instructions in the next section.   Steps to Run the Hands-On All commands below are run directly on the FRDM i.MX 95 Pro board (via serial console or SSH). The eIQ utilities are pre-installed in the BSP image. Step 1 — Verify Device Detection After powering on the board with the ARA240 module seated in J24 (and/or J25), confirm the accelerator is recognized by the system: # Device Detection & Status chip_info.sh The script prints the detected DNPU chip information. If nothing is returned, check the M.2 seating and fan-power connectors (J9/J10). Step 2 — List Available Models Use the fetch_models utility to see which AI models are available for download: # List available models fetch_models --list The output shows model IDs for CNN, LLM, and VLM workloads that are compatible with the ARA240. Step 3 — Download a Model Download a model by its repository ID. The example below fetches a 7-billion-parameter instruction-tuned LLM: # Download a specific model (example: Qwen2.5 7B) fetch_models --repo-id nxp/Qwen2.5-7B-Instruct-Ara240 Models are stored under /usr/share/ in subdirectories named cnn , llm , or vlm depending on the model type. Step 4 — Run Inference Performance Tests Once a model is downloaded, benchmark its inference performance on the DNPU: # Running Inference Tests run_model_perf.sh Step 5 — Measure DNPU Metrics Capture real-time NPU utilization and performance counters: # Measuring DNPU Metrics ara2_metrics.sh Step 6 — Configure and Start the eIQ AAF Connector The eIQ AAF Connector exposes a REST API (OpenAI-compatible) so any HTTP client or web application can send inference requests to the ARA240. Follow these steps: # Check whether the connector service is already running systemctl status eiq-aaf-connector.service # Start the connector service (systemd-managed) systemctl start eiq-aaf-connector.service # Stop the connector service when done systemctl stop eiq-aaf-connector.service # Edit the connector configuration (model path, port, etc.) vi /usr/share/eiq/aaf-connector/server_config.json # Alternatively, start the connector manually (foreground) /usr/share/eiq/aaf-connector/venv/bin/connector --host 0.0.0.0 --port 8000 Once the connector is running, open the interactive API documentation in a browser on your host machine (replace <board-ip> with the board's actual IP address): # Open the connector Web API interface in a browser http://<board-ip>:8000/docs Step 7 — Send a Chat Completion Request With the connector running and a downloaded LLM, you can send an OpenAI-compatible chat completion request directly from the API docs page or via any HTTP client: # Example chat completion payload (POST to /v1/chat/completions) { "model": "Qwen2.5-7B-Instruct", "messages": [ { "role": "system", "content": "You are a helpful assistant" }, { "role": "user", "content": "hello, how are you?" } ] }   Troubleshooting Symptom What to Check chip_info.sh returns nothing / DNPU not detected Verify the ARA240 module is firmly seated in J24 or J25. Confirm the fan-power cable is connected to J9 (for J24) or J10 (for J25). Reboot the board after reseating. fetch_models --list fails or model download hangs Check internet connectivity: ping 8.8.8.8 If DNS resolution fails, set it manually: echo nameserver 8.8.8.8 > /etc/resolv.conf Model not found after download Verify the model landed in the correct directory: ls /usr/share/<cnn|llm|vlm>/ Certificate or TLS errors during model download The board's system clock may be wrong. Set the correct date and time: date --set="18 SEP 2026 13:00:00" Then retry the download. Connector service fails to start Check journalctl -u eiq-aaf-connector.service for error details. Ensure server_config.json points to a valid downloaded model path.   Conclusion In this hands-on you: Connected the ARA240 DNPU AI Accelerator to the FRDM i.MX 95 Pro via PCIe (M.2 Key-M). Verified device detection and explored available AI models using the eIQ command-line utilities. Downloaded and benchmarked a large language model on the DNPU. Measured real-time NPU performance metrics with ara2_metrics.sh . Configured and launched the eIQ AAF Connector to expose an OpenAI-compatible REST API. Sent a live chat-completion request to a locally running LLM — entirely on the edge. For a full visual walkthrough, watch the demo video above. Explore the rest of the FRDM i.MX 95 Pro Hands-On Training Hub for additional modules covering cameras, connectivity, multimedia, and more.
記事全体を表示
Unlike MCXW 71 MCU, MCXW 72 supports an Open NBU. This means that NBU firmware source code is exposed to user. On MCXW 71 MCU, NBU firmware is NXP proprietary; it is not user customizable.
記事全体を表示
This document is intended to guide you in the installation of the necessary tools and repository for start running Zephyr examples and development. Zephyr is a lightweight, open-source real-time operating system (RTOS) designed specifically for microcontrollers (MCUs) and other resource-constrained embedded devices. Unlike general-purpose operating systems, Zephyr is built to run on systems with limited memory, low power consumption, and strict real-time requirements. It provides the core software foundation that allows an MCU to run multiple tasks reliably, respond to events on time, and interact with hardware in a structured way.
記事全体を表示
This document is intended to guide you in the installation of the necessary tools and repository for start running matter examples and development. Matter (previously known as Project CHIP) is a single, unified, application-layer connectivity standard designed to enable developers to connect and build reliable, secure IoT ecosystems and increase compatibility among Smart Home and Building devices. Backed by major brands and developed through collaboration within the Connectivity Standards Alliance (previously known as the Zigbee Alliance), Matter is an open-source royalty-free connectivity standard built with market-proven technologies using Internet Protocol (IP) and compatible with Thread and Wi-Fi network transports. Building solutions and leading standards efforts, NXP provides scalable, flexible and secure platforms for the variety of use cases Matter addresses – from end nodes to gateways – so device manufacturers can focus on their product innovation. NXP’s Matter solutions go beyond just the connectivity with comprehensive capabilities for the compute and security requirements for IoT devices.
記事全体を表示
This project implements a configurable secure encrypted Ethernet communication node with the transmission of a large data image.
記事全体を表示
Goal of this lab is to show the SDK example implementing the Bluetooth LE Ranging profile, how to flash it and run it, as well as looking into the code to extract meaningful information for applications that use ranging Guide
記事全体を表示
This document is intended to guide you in the installation of the tools and let you know the material required for the FRDM-MCXW72 Channel Sounding Hands On 
記事全体を表示
In this lab we make some experience with the FRDM-MCXW72 board using the SDK project to implement a simple LED blinking. Once we will get familiar with the example project, we will integrate simple modifications
記事全体を表示
In this lab we will first import the MCUXpresso SDK for the MCX W72 Freedom board into MCUXpresso IDE and then we will build, flash and debug the hello world project to make sure the environment is set for the following Labs  
記事全体を表示
This hands-on describes how to run the Low Power Reference Design demo on FRDM-MCXW72. Two low-power reference design applications are provided in the reference_design folder: Low power peripheral application, demonstrating the low power feature on an advertiser peripheral Bluetooth LE device. Low power central application, demonstrating the low power feature on a scanner central Bluetooth LE device. These applications aim at providing: A reference design application for low power/timing optimization on a Bluetooth Low Energy application. These can be used in first intent for porting a new application on low power. A way for measuring the power consumption, wake-up time, and active time in various power modes. The default low-power mode used in different modes are shown as follows: Default power mode App core Radio core Advertise mode Power Down mode Deep sleep mode Connected mode Deep Sleep mode Deep Sleep mode Scanning mode Deep Sleep mode WFI or Deep Sleep mode For complete documentation please visit: reference_design — MCUXpresso SDK Documentation
記事全体を表示
Goal of this lab is to show the SDK example implementing the wireless UART profile and we will move forward in making some meaningful modifications to the example itself with the goal to show where in the code the end user should enter the relevant application software for the application. Run Wireless UART IoT Toolbox Demo
記事全体を表示
The MCX W72 family features a 96 MHz Arm® Cortex®-M33 core coupled with a multiprotocol radio subsystem also called Narrow Band Unit (NBU) supporting Matter, Thread, Zigbee and Bluetooth LE. The independent radio subsystem, with a dedicated core and memory, offloads the main CPU, preserving it for the primary application and allowing firmware updates to support future wireless standards. On MCXW72, only boot ROM has access to the NBU flash. The ROM bootloader provides an in-system programming (ISP) utility that operates over a serial connection on the microcontroller units (MCUs) The objective in this hands-on, is to learn how to recognize when the NBU firmware does not match with the SDK version.
記事全体を表示
The MCX W72 family features a 96 MHz Arm® Cortex®-M33 core coupled with a multiprotocol radio subsystem also called Narrow Band Unit (NBU) supporting Matter, Thread, Zigbee and Bluetooth LE. The independent radio subsystem, with a dedicated core and memory, offloads the main CPU, preserving it for the primary application and allowing firmware updates to support future wireless standards.   The ROM bootloader provides an in-system programming (ISP) utility that operates over a serial connection on the microcontroller units (MCUs)  This hands-on describes how to update the code in NBU and the User firmware using the ISP.  
記事全体を表示
Introduction This document is intended to guide you in the installation of the tools and let you know the material required for the FRDM-MCXW72 Hands On.  Required Materials The material and the software requirements will depend on the hand on, but the next is what it is required in most of them. Hardware Requirements FRDM-MCXW72 Board Personal Computer Type C USB Cable Software Requirements IDE: Visual Studio Code 1.107.1 or later SDK: v25.12.00 MCUXpresso extension for VS Code version v25.12.48 BLHost Tool or LinkFlash tool (Linkflash is included with LinkServer installation) Windows OS (It was used Windows 11 for this hands-on) NXP IoT Toolbox (For an Android or iOS device) Serial Terminal program, like PuTTY or Tera Term Environment Setup Note: In order to make downloads in NXP website, it is necessary to have an account. Register and log-in for moving forward. MCUXpresso for Visual Studio Code                                                                                                                                                                         MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. The extension enables NXP developers to use one of the most popular embedded editor tools and provides an easy and fast way to create, build and debug applications based on MCUXpresso SDK or Zephyr projects.   Install it following the next steps: Download Visual Studio Code from Microsoft Store or visual studio code web page Download Visual Studio Code - Mac, Linux, Windows Access to vscode for MCUX wiki and download MCUXpresso Installer  Dependency Installation · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub Run MCUXpresso Installer and for MCXW72 Hands On install at least MCUXpresso SDK Developer Matter Developer Arm GNU Toolchain Standalone Toolchain Add ons Linkserver PEmicro Installing the FRDM-MCXW72 SDK V25.12.00   Each MCU has its own SDK that includes driver, examples, middleware, docs and other components. To get and build the demo, let’s install the SDK into VS Code. Install the NXP’s GitHub SDK: Once MCUXpresso for Visual Studio Code is installed, open VS Code. Go to MCUXpresso for VS Code extension that is on the tools column at the left.    Look for INSTALLED REPOSITORIES option and press ‘+’ (Detail steps are described in wiki page. Working with MCUXpresso SDK · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub).                                               Search for the remote option of the Import Repository window. Select the MCUXpresso SDK in the repository option to download the GitHub SDK, then in the Revision tab you can select either the “main” revision (which corresponds to the latest version available) or to select an specific version (we’ll be using version v25.12.00 for these series of labs), optionally you can change the repository name and location.     Finally click on the “Import” button. Blhost Installation The blhost application is used on a host computer to issue commands to an NXP platform running an implementation of the MCU bootloader. The blhost application with the MCU bootloader, allows a user to program a firmware application onto the MCU device without a programming tool. Please go an download the tool in the next path and make sure to placed in a known location. BLHost Download page.
記事全体を表示
Objectives In this lab, you will learn: How to use the MCUXpresso Installer to obtain NXP Software (FreeMASTER) How to use Application Code Hub to import an example into the VS Code workspace How to build, clean, debug, and run the example. How to connect the Serial Monitor for UART console How FreeMASTER can be used as a real-time debug monitor and data visualization tool Hardware Requirements Personal Computer FRDM-MCXA153 Board Heart Rate 4 CLICK Module (MIKROE 5547) USB type-C cable   Software Requirements MCUXpresso for VS Code FreeMASTER v3.2 or latest FRDM-MCXA153 SDK Application Code Hub The Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by NXP in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. Find more information at www.nxp.com/ach.   Installing Prerequisites - Launch MCUXpresso for VS Code - Launch the MCUXpresso Installer from the QUICKSTART PANEL   - Install MCUXpresso SDK Developer, LinkServer, and FreeMASTER   Heart Rate Monitor Lab The NXP Application Code Hub provides a complete example of how to use the MCXA-153 microcontroller in a Heart Rate and SPO2 monitor application. This lab will walk through the steps to import, build, program and debug the example. The final section of the lab shows how to use FreeMASTER as a data-visualization tool for the acquired sensor data on the FRDM-MCXA153 development board. 1. Go to the Quick Start Panel 2. Select Application Code Hub 3. Filter Visible Examples (MCX + Sensors) - Go to the filter section next to the Search bar and select two filters. - Select MCX in the Device Families Section and Sensor in the Categories section of the filters   4. Search for Keywords in Examples - Search for the keyword 'heart rate'. - Select the demo "frdm mcxa153 freemaster heart rate". 5. Read Overview of Heart Rate Demo The Application Code Hub provides a consistent Readme Overview for every project. The FreeMASTER Heart Rate demo overview is previewed after clicking on the application card. Scroll through the readme to become familiar with the available contents like required hardware, software and setup instructions. 6. Select Destination for Project The wizard automatically provides a prompt to browse to a desired destination folder. Create the destination C:\NXP_ACH to store the project here. Or you can specify a custom location. 7. Import Project into Workspace Select Import Project(s) after entering the desired location. If a valid project is not available, the wizard only displays Import Repository, to allow a code repo, without a project, to be added to workspace. 8. Select Detected Project(s) The import wizard will scan the example repo and list valid projects that were discovered. This allows the user to select only the projects they want created. Select the mcuxpresso project listed at the top of the VS Code window. 9. Associate a Toolchain The last selection is to identify the Compiler toolchain to be used for the project. GCC will be used for this project. Select Arm GNU Toolchain 12.3.Rel1 (Or latest version available from MCUXpresso Installer prework) The scan may locate Compilers associated with MCUXPresso IDE. Verify the path and version between listed compilers. At this time the wizard will complete the project import. A Successful Conversion notification is displayed at the bottom of the screen. It is important to recognize that the selected Heart Rate example is a working project within the MCUXpresso IDE (Eclipse based). The VS Code extension has the ability to convert an existing MCUXpresso IDE projects for development in VS Code. 10. Navigating a Project in VS Code The MCUXpresso for VS Code extension includes a PROJECTS section to help users access useful project information. Users can review and modify project information with the following steps. Review Project Details Project details are shown in the Dropdown menu of the Projects Section in the MCUXpresso Extension Navigation Pane. • Settings: Workspace settings specific to the project • MCU: Targeted device. • Build Configurations: Select build configuration from available list (i.e. Debug or Release). • Debug Configurations: • Repository Information • Project Files 11. Working with Source Files There are two ways to view and modify the project's files: • Click on the Explorer Icon at the top of the VS Code left navigation pane.  • Expand the Project Files section from the PROJECTS view 12. Build the application The MCXA153 FreeMASTER Heart Rate project needs to build the application image. After the code builds without any errors, the application can be run on the FRDM board. The following steps require that you return to the MCUXpresso perspective by clicking the MCUXpresso for VS Code X icon in the Activity bar Build the project by clicking the Build Selected icon. After a successful build, the Terminal console displays the memory usage (or compiler errors if any). 13. Connect Serial Monitor to the board To use the Serial Monitor integrated into VS Code: - Connect the USB-C cable to J15 to power the FRDM board. The onboard debugger provides a USBUART bridge to interface with the Serial monitor. - Click on the SERIAL MONITOR found as a tab in the Terminal window at the Bottom of VS Code Window. NOTE: The default COM settings are valid for NXP eval boards: "115200, None..." - Click Start Monitoring to connect the monitor to the FRDM board’s auto-detected COM port. VS Code in light theme 14. Flash/Debug the Application This section uses the on-board debugger to connect to the MCU, and program the flash. LinkServer from NXP manages the GDB server for communicating with the NXP MCULink on-board debug probe. It includes support for flash programming. - Click the play icon to Debug the application: The application is flashed to the FRDM board and VS Code switches to the Debug perspective. Return to the SERIAL MONITOR tab under the Terminals. It switches to the OUTPUT terminal when a Debug session is started.  VS Code in light theme - The execution will be paused on a breakpoint. Click Continue/Play icon to continue execution. The application will advance to the start of main().   - Click Continue/Play icon a 2nd time for the Heart Rate application to launch inside main(). 15. View Heart Rate Values in Serial Terminal The Heart Rate application using the serial port to display information. The following should be displayed in the SERIAL MONITOR tab after main() starts. Place a finger on the sensor near the Heart silkscreened on Heart Rate 4 click board. The following should be displayed in the SERIAL MONITOR tab after a finger is placed on the sensor: A heart rate value will be calculated and displayed after 16. FreeMASTER Data Visualization FreeMASTER is a standalone application provided by NXP to help developers visualize, monitor and manipulate data available from their projects. The Heart Rate example includes a /freemaster folder that helps users get started using the tool. The settings in the Application Code Hub were established for an MCUXpresso IDE based project. There are a few changes that need to be made after the project is converted to a VS Code project. The following steps will properly configure FreeMASTER to work with the Heart Rate example project: Launch FreeMASTER Application There are two options for launching FreeMASTER. • Click on the heart_rate.pmpx using File Explorer. The FreeMASTER application should be associated with .pmpx file extensions. This will also automatically load the included project settings.   • Launch FreeMASTER by searching Windows Applications. • This will not load project settings. You will be required to Open Project using the FreeMaster menu as shown. Open the .pmpx project file. • Verify Project Options FreeMASTER has a few key settings to verify once a project is opened. A user should verify they are correctly set for the type of Debug Probe and location of the project output files. - Click Project -> Options from the menu bar. - Verify that the correct method is set for communicating with the board. The on-board Debug Probe for the FRDM-MCXA153 is by default shipped with NXP CMSIS-DAP firmware. Select FreeMASTER CMSIS-DAP Communication Plug-in found under the Comm tab, for Plug-in module:   - Verify that the correct Default symbol file is targeted for the VS Code project. The symbol file in VS Code projects is output under an /armgcc folder. Select the /armgcc folder within VS Code project MAP Files tab. The window will autodetect the Binary ELF File, and display this under File format:   - Visualize Data From Heart Rate Project The NXP software team has included a default visualization for the Heart Rate project. The demonstration showcases the different styles for project data to be shown. The following visualization settings are preset for the Heart Rate project: Welcome HTML Page: The HTML Pages (Under Options) points to welcome.html file. This provides structured web view for displaying elements. Beyond scope of this lab, but .html file can be reviewed to see how target values/charts are referenced in html. Oscilloscope Visual: View plots the values of a project variable. The plot axis are configured for scale and color. Heart Rate, SPO2 and ECG are configured. Variable Watch Table: After variables are configured to be tracked, they can be added to this table view.   Make sure that the debug probe is not in an active debug session in the IDE or VS Code. Click GO icon on the menu bar to initiate the project data visualization! The following points are highlighted for the FreeMASTER output. 1. Clicking on the elements listed under the Project Tree changes the view to the specific Oscilloscope Visual. 2. View the captured values for the variables in a Table view. 3. Visualization of data organized based on the layout defined in the Welcome.html.  
記事全体を表示