CodeWarrior special Edition for linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior special Edition for linux

跳至解决方案
1,896 次查看
bataliero
Contributor III

Hi,

I would like to get CodeWarrior Special Edition ( Kinetis ) for Linux but cannot find any links on freescale.com . I have found Linux version by its will expire after 30 days. I am going to use it with Kinetis MCUs. Could you provide links or information?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,586 次查看
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,587 次查看
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

0 项奖励
回复