CodeWarrior special Edition for linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior special Edition for linux

ソリューションへジャンプ
1,890件の閲覧回数
bataliero
Contributor III

Hi,

I would like to get CodeWarrior Special Edition ( Kinetis ) for Linux but cannot find any links on freescale.com . I have found Linux version by its will expire after 30 days. I am going to use it with Kinetis MCUs. Could you provide links or information?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,580件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,581件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

0 件の賞賛
返信