Kinetis design studio Trace and Profile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis design studio Trace and Profile

ソリューションへジャンプ
2,624件の閲覧回数
bataliero
Contributor III

Hi,

where is "Trace and Profile" tab in Kinetis Design Studio? In CodeWarrior it is places in Debug Configuration. That features are not supported in KDS?

 

I am using K60 - TWR_k60n512.

 

page13:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4506.pdf

http://blogs.freescale.com/wp-content/uploads/2011/09/figure-1-the-codewarrior-ide-trace-feature-dis...

ラベル(1)
0 件の賞賛
返信
1 解決策
1,730件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The CodeWarrior Trace and Profiling are not part of Kinetis Design Studio.

Trace and Profiling are supported by commercial IDE's for Kinetis, see IDEs for Kinetis MCUs|Freescale

If you want to do trace/profiling (on a different level, with source instrumentation), then this might be useful for you:

Poor Man’s Trace: Free-of-Charge Function Entry/Exit Trace with GNU Tools | MCU on Eclipse

Code Coverage for Embedded Target with Eclipse, gcc and gcov | MCU on Eclipse

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,731件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The CodeWarrior Trace and Profiling are not part of Kinetis Design Studio.

Trace and Profiling are supported by commercial IDE's for Kinetis, see IDEs for Kinetis MCUs|Freescale

If you want to do trace/profiling (on a different level, with source instrumentation), then this might be useful for you:

Poor Man’s Trace: Free-of-Charge Function Entry/Exit Trace with GNU Tools | MCU on Eclipse

Code Coverage for Embedded Target with Eclipse, gcc and gcov | MCU on Eclipse

Erich

0 件の賞賛
返信