CodeWarrior special Edition for linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior special Edition for linux

Jump to solution
1,886 Views
bataliero
Contributor III

Hi,

I would like to get CodeWarrior Special Edition ( Kinetis ) for Linux but cannot find any links on freescale.com . I have found Linux version by its will expire after 30 days. I am going to use it with Kinetis MCUs. Could you provide links or information?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,576 Views
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,577 Views
BlackNight
NXP Employee
NXP Employee

If it expires after 30 days, it will be in special edition mode. No need to re-install anything. You might rename the license.dat file to get rid of the 'expiration' message.

As for downloading the Linux version: it is available as v10.2 on www.freescale.com/cwmcu10.

Erich

0 Kudos
Reply