Freemaster 2.0.2 problem with transformed variables

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster 2.0.2 problem with transformed variables

ソリューションへジャンプ
2,611件の閲覧回数
agostinofacotti
Contributor III

Hi all,

 

i've just installed Freemaster rev. 2.0.2 but now i can't write real-transformed variables: if I switch theirs "Show as" from "REAL" to "DEC" I'm able to write.

 

With the Freemaster 2.0.0 there is no problem.

Where is the problem in your opinion?

 

thanks,

agostino

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,284件の閲覧回数
agostinofacotti
Contributor III

This is a duplicate question of the discussion https://community.nxp.com/thread/435986 

See that for the answer!

Regards,

agostino

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,285件の閲覧回数
agostinofacotti
Contributor III

This is a duplicate question of the discussion https://community.nxp.com/thread/435986 

See that for the answer!

Regards,

agostino

0 件の賞賛
返信
2,284件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

so solve the problem,  can you please provide more information:

1. your project

2. how to reproduce your problem?

3. problem screenshot.

Thanks.
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,284件の閲覧回数
agostinofacotti
Contributor III

Hi Jennie Zhang,

I tried to reproduce the problem (reinstalled Freemaster 2.0.2, created a new sample elf file with a led blinking and created the relative Freemaster project) but there is no problem in this configuration.

If I'll face with the problem I'll send you the documentation requested, a couple of days I think.

Thanks in advance,

agostino

0 件の賞賛
返信