Freemaster 2.0.2 problem with transformed variables

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster 2.0.2 problem with transformed variables

Jump to solution
2,676 Views
agostinofacotti
Contributor III

Hi all,

 

i've just installed Freemaster rev. 2.0.2 but now i can't write real-transformed variables: if I switch theirs "Show as" from "REAL" to "DEC" I'm able to write.

 

With the Freemaster 2.0.0 there is no problem.

Where is the problem in your opinion?

 

thanks,

agostino

Labels (1)
0 Kudos
Reply
1 Solution
2,349 Views
agostinofacotti
Contributor III

This is a duplicate question of the discussion https://community.nxp.com/thread/435986 

See that for the answer!

Regards,

agostino

View solution in original post

0 Kudos
Reply
3 Replies
2,350 Views
agostinofacotti
Contributor III

This is a duplicate question of the discussion https://community.nxp.com/thread/435986 

See that for the answer!

Regards,

agostino

0 Kudos
Reply
2,349 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

so solve the problem,  can you please provide more information:

1. your project

2. how to reproduce your problem?

3. problem screenshot.

Thanks.
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,349 Views
agostinofacotti
Contributor III

Hi Jennie Zhang,

I tried to reproduce the problem (reinstalled Freemaster 2.0.2, created a new sample elf file with a led blinking and created the relative Freemaster project) but there is no problem in this configuration.

If I'll face with the problem I'll send you the documentation requested, a couple of days I think.

Thanks in advance,

agostino

0 Kudos
Reply