i.MX RT1176 program to SD/EMMC and debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1176 program to SD/EMMC and debugging

Jump to solution
1,506 Views
JayCao
Contributor III

Hello all,

I am working on a project using SD/EMMC to store Firmware instead of Flash memory.

I have some questions as below:


1. Is there any guide to do that on RT1176?

I followed the guide below but did not work on our EVKs.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1050-SDRAM-app-code-boot-from-SDcard-burn-with...


2. Do we need to load any bootloader first and then follow the guide in 1st question for it to work?

3. How to debugger the firmware ?

Hope to hear from you soon.

Best regard,

Tu

Tags (4)
0 Kudos
Reply
1 Solution
1,437 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1 Reply
1,438 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Please refer to our previous post for the solution: https://community.nxp.com/t5/i-MX-RT/LED-cannot-blinking-when-loading-firmware-via-SDcard/td-p/18345...

Wish you have a nice day!

0 Kudos
Reply