i.MX RT Crossover MCUs Knowledge Base

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT Crossover MCUs Knowledge Base

ディスカッション

ソート順:
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-342954
記事全体を表示
​ The table below contains notable updates to the current release of the Reference Manual. The information provided here is preliminary and subject to change without notice. ​​​​​​​​​​​​​​​​​​ Affected Modules Issue Summary Description Date System Boot Incorrect encoding for BOOT_CFG[9] - ECC Selection The encoding for the boot configuration bit for the ECC selection is incorrect. Device ECC should be 0 and Software ECC should be 1. Before:    After:    - ​
記事全体を表示
This application note describes how to develop an audio player with NXP i.MX RT600 crossover MCU family. Click here to access the full application note.
記事全体を表示
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-341316
記事全体を表示
The RT1170 supports the ability to trigger dual ADC’s in SyncMode or AsyncMode via the ADC External Trigger Control (ADC_ETC): In SyncMode, ADC1 and ADC2 are controlled by the same trigger source. In AsyncMode, ADC1 and ADC2 are controlled by separate trigger source. In AsyncMode (TRIGa_CTRL[SYNC_MODE]==0), the ADC conversion clock frequency maximum is 88 MHz, but in SyncMode (TRIGa_CTRL[SYNC_MODE]==1), the ADC conversion clock frequency must be constraint to a lower frequency due to switching noise inherent to its design architecture.  Reducing the conversion clock frequency reduces the switching noise that is observed. NXP is currently conducting further characterization in order to specify the maximum frequency of conversion in SyncMode across process, voltage, and temperature.  However, on typical samples at room temperature 60 MHz is the maximum frequency.
記事全体を表示
NXP Updated the Hardware Development Guide for the MIMXRT1160/1170 Processor (MIMXRT1170HDUG) The main difference is: Updated capacitance value of VDDA_1P8_IN in Table 1 and Table 2 From 0.1uF to 1uF     This will help improve the robustness of the circuit at low temperatures.
記事全体を表示
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-341985
記事全体を表示
When: TUESDAY, SEPTEMBER 14TH AT 11 AM EST Click here to register today.   Topic of discussion From consumer to industrial devices, a paradigm shift has already begun. Our everyday experiences with smartphones are driving the demand for higher performance, more connectivity, and an exceptional user experience as the cornerstones of the embedded products we use. But how can you make it easier to take your product to the next level? Join NXP and Crank Software to learn why the NXP I.MX RT1170 crossover MCU is the right embedded hardware to create and can help lower development risks and how developing engaging user experiences can easily become part of your development workflow. During this session, you’ll learn: About optimizing power and performance with i.MX RT [1170] Crossover MCUs Just how embedded GUI development can be a collaborative experience between development and design How Storyboard’s Rapid Design and Iteration technology embraces UI design changes during development What integrated capabilities can help leverage the hardware’s full potential How easy it is to develop GUI apps via a live demo of a Storyboard  
記事全体を表示
The table below contains notable updates to the current release of the Reference Manual. The information provided here is preliminary and subject to change without notice. ​​​​​​​​​​​​​​​​​​ Affected Modules Issue Summary Description Date QDC Incorrect Input Filter Register (FILT) configuration.  FILT_PRSC bitfield is not implemented in Design. 22 May 2025 ​ ​
記事全体を表示
This document describes how to program a bootable image into the recovery Flash device using i.MX RT600 MCUs. Click here to access the full application note.
記事全体を表示
Realize a panoramic video layer with OpenGL
記事全体を表示
When design a project, sometimes CCM_CLKO1 needs to output different clocks to meet customer needs. This customer does not need to buy a separate crystal, which can reduce costs。The document describe how to make CCM_CLKO1 output different clock on I.MXRT1050. According to  selection of the clock to be generated on CCM_CLKO1(CLKO1_SEL) and setting the divider of CCM_CLKO1(CLKO1_DIV) in I.MXRT1050reference manual. CCM_CLKO1 can output different clock. If CCM_CLKO1 output different clock via SYS PLL clock. We can get the different clock for the application. CLKO1_DIV 000 001 010 011 100 101 110 111 Freq(MHz) 264 132 88 66 52.8 44 37.714 33 For example we want to get 88Mhz output via SYS PLL clock. We can follow the steps as the below(led_blinky project in SDK 😞       1. PINMUX GPIO_SD_B0_04 as CCM_CLKO1 signal.       IOMUXC_SetPinConfig(       IOMUXC_GPIO_SD_B0_04_CCM_CLKO1,              0x10B0u; 2.Enable CCM_CLKO1 signal. CCM->CCOSR |= CCM_CCOSR_CLKO1_EN_MASK; 3.Set CLKO1_DIV to get 88MHZ the clock for the application. CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_DIV_MASK)) | CCM_CCOSR_CLKO1_DIV(2); CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_SEL_MASK)) | CCM_CCOSR_CLKO1_SEL(1); 4 We will get the clock as the below. Note: In principle, it is not recommended to output CLOCK in CCM_CLKO1, if necessary, Please connect an 8-10pf capacitor to GPIO_SD_B0_04, and connect a 22 ohm resistor in series to prevent interference.
記事全体を表示
Using a different Flash with the RT1050 In IAR/Keil environment , when you change to other flash(not default flash on EVK board), please refer to below AN to modify the code for it. https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf
記事全体を表示
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-340813
記事全体を表示
1. Backgroud Customers adopting multi-i.MXRT master-slave architectures (one master, multiple slaves) aim to meet functional requirements while simultaneously reducing costs and improving system efficiency through optimized hardware design. 2.  Multi-i.MXRT Architecture Design 2.1 Independent Flash Architecture (Master-Slave) In multi-i.MXRT systems, a typical design adopts a master-slave architecture where one i.MXRT acts as the master and others as slaves. Since the i.MXRT chip lacks on-chip non-volatile memory, each i.MXRT requires an independent boot device (e.g., NOR Flash connected via FlexSPI) to load programs and initiate startup.  Traditional Architecture: - Each i.MXRT has its own dedicated Flash memory, ensuring operational independence. Advantages: - Full System Independence: Each i.MXRT operates independently with its own firmware and boot configuration. Fault isolation: A failure in one Flash or i.MXRT does not affect others. - Simplified Firmware Management: Independent firmware updates for each i.MXRT without coordination. Easier OTA version control (each device has its own update path). Disadvantages: - Complex programming workflow (multiple Flash devices need individual firmware updates). - Higher hardware complexity, larger PCB footprint, and increased cost due to multiple Flash chips. 2.2 Shared Flash Architecture (Master-Slave with Flash Sharing) A single Flash device is connected to multiple i.MXRTs. The master i.MXRT controls the POR_B (Power-On Reset) signal of all slave i.MXRTs, enabling shared access to the same Flash. Boot Process: 1. The master i.MXRT boots first in Non-XIP mode. 2. The master sequentially releases the POR_B signals of slave i.MXRTs, allowing them to occupy the Flash and boot in Non-XIP mode one at a time. Advantages: - Reduced cost and simplified hardware design. - Smaller PCB footprint with only one Flash required. - Streamlined firmware programming (single Flash update) for mass production. Disadvantages: - If slave i.MXRTs require different firmware, the Flash must be partitioned into regions, leading to: - Complex OTA version management challenges. - Reduced system independence among slave devices. 3. Hardware Platform Setup Master Board: MIMXRT1010-EVK Slave Board: MIMXRT1010-EVK Rework: Remove U13 (Flash) from the slave board. Retain U13 on the master board and fly-wire it to U13 of the slave board (only CS, SCLK, IO0, IO1 are required for low-speed boot). Connect GPIO_11 signal of the master i.MXRT1010 to POR_B of the slave i.MXRT1010 (Pin3/4 of SW3).   4. Software Design Due to both master and slave i.MXRTs sharing a single application (differentiated via conditional branches), the app must be Non-XIP. Therefore, we designed a boot_loader project that copies and jumps to the boot_app, instead of using SPT or MCUBootUtility. 🔗 Key modules: /boards/evkmimxrt1010/demo_apps/boot_loader /boards/evkmimxrt1010/demo_apps/boot_app . ├── boards │ └── evkmimxrt1010 │ ├── demo_apps │ │ ├── boot_app │ │ ├── boot_loader │ │ ├── hello_world │ │ └── led_blinky │ └── xip │ ├── evkmimxrt1010_flexspi_nor_config.c │ └── evkmimxrt1010_flexspi_nor_config.h ├── CMSIS │ ├── Core │ ├── Driver │ ├── DSP │ ├── LICENSE.txt │ ├── NN │ └── RTOS2 ├── components │ ├── lists │ ├── serial_manager │ └── uart ├── devices │ └── MIMXRT1011 ├── LICENSE └── README.md Note: Please see the whole reference project from attchement.  4.1 boot_loader Design The boot_loader is a XiP project directly booted by the chip's BootROM. It can be based on the SDK's hello_world example ( flexspi_nor target). The FCB boot header should be modified as follows (1-bit SPI, 30MHz, Normal Read Mode): // boot_loader // xip/evkmimxrt1010_flexspi_nor_config.c const flexspi_nor_config_t qspiflash_config = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClkLoopbackInternally, .csHoldTime = 3u, .csSetupTime = 3u, .deviceType = kFlexSpiDeviceTypeSerialNOR, .sflashPadType = kSerialFlash_1Pad, .serialClkFreq = kFlexSpiSerialClk_30Hz, .sflashA1Size = 16u * 1024u * 1024u, .lookupTable = { // Read LUTs FLEXSPI_LUT_SEQ(CHIP_SELECT, FLEXSPI_1PAD, 0x03, RADDR_SDR, FLEXSPI_1PAD, 0x18), FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_1PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0), }, .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, }; The boot_app is a Non-XIP project (based on SDK’s debug target). Its binary is imported into the boot_loader project. With proper linking address and memory layout, the copy & jump logic can be implemented with standard code. The finalized boot_loader can then be downloaded to Flash using an IDE. 4.2 boot_app Design The boot_app is also derived from the SDK's hello_world . It supports receiving simple UART commands ( A , B , etc.) for various tests. Currently, six test commands are supported:  Commands Target Device i.MX RT Description 'A' Master Drive master i.MXRT's GPIO_11 high to pull POR_B high and release slave i.MXRT from reset. 'B' Master Drive master i.MXRT's GPIO_11 low to pull POR_B low and hold slave i.MXRT in reset.   Commands Target Device Description 'F' Salve Toggle GPIO_11 periodically with a timer to blink the D25 LED.   Commands Target Device Description 'C' Master or Slave  Initialize Flash-related pins for FlexSPI functionality. 'D' Master or Slave  Restore Flash-related pins to default GPIO state. 'E' Master or Slave  Erase, program, and read U13 Flash.   Notes: Commands A and E may cause conflicts when both master and slave i.MXRT attempt to drive the same Flash through FlexSPI pins. Before executing Command A (to release the slave), the master should first execute Command D, calling the following function to restore FlexSPI pins to GPIO mode. Otherwise, the slave may fail to boot normally (BootROM configures these pins as FlexSPI during boot). void bsp_deinit_flexspi_pins(void) { IOMUXC_SetPinMux(IOMUXC_GPIO_SD_06_GPIO2_IO06, 0U); IOMUXC_SetPinMux(IOMUXC_GPIO_SD_07_GPIO2_IO07, 0U); IOMUXC_SetPinMux(IOMUXC_GPIO_SD_09_GPIO2_IO09, 0U); IOMUXC_SetPinMux(IOMUXC_GPIO_SD_10_GPIO2_IO10, 0U); IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_06_GPIO2_IO06, 0x10A0U); IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_07_GPIO2_IO07, 0x10A0U); IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_09_GPIO2_IO09, 0x10A0U); IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_10_GPIO2_IO10, 0x10A0U); } Commands C and E are typically used together. If the slave has already executed them and remains active, the master must either: The Master execute Command B to reset the slave which resets FlexSPI pin configurations The Slave to execute Command D before running C/E. 5. On-Board Testing Power up both boards. Download the boot_loader (containing embedded boot_app ) to Flash. Quick Test: Sending Command A initially may not start the slave properly. However, after executing Command D followed by Command A, the slave boots successfully. Both master and slave boards can read/write the shared Flash normally, verifying the feasibility of this innovative shared flash boot method. Note: Please see readme.md from attchement for more details. 6. Conclusion The i.MXRT master-slave architectures (Independent Flash vs. Shared Flash) offer distinct trade-offs: - Independent Flash: Prioritizes system reliability and independent firmware management at the cost of higher hardware complexity and cost. - Shared Flash: Reduces costs and PCB footprint but introduces firmware dependency and OTA management challenges. The prototype successfully validated the Shared Flash approach, demonstrating its feasibility for cost-sensitive, mass-production scenarios. Customers can choose between these designs based on their specific priorities: high reliability with independence (Independent Flash) or cost-efficiency with streamlined workflows (Shared Flash).
記事全体を表示
RT600 ROM API example for w25q128fw support.
記事全体を表示
​​迁移重点​​: ​​检查GPIO配置​​:利用新时序建议优化设计。 ​​更新SDK至25.06+​​:确保芯片版本识别和ROM API兼容。 ​​验证SEMC设计​​:若使用CSX1/2/3,需按ERR052401调整时序。 ​​工具链升级​​:J-Link v8.38+和MCUXpresso脚本更新。   0. 本文目的    若您并未遇到RT1170 FSGPIO漂移老化问题,请忽略本文档。 若您遇到RT1170A的ERR052351(输出电压>1.98V时参数漂移)和ERR050643(上电瞬间误触发上拉脉冲)问题,并想通过迁移到新硅片RT1170B,请查看本文完成迁移。 ​ 1. 硅片变更 (Silicon Changes)​ ​ ​​GPIO修复​​: 解决了RT1170A的ERR052351(输出电压>1.98V时参数漂移)和ERR050643(上电瞬间误触发上拉脉冲)问题。 影响范围:GPIO_AD/GPIO_LPSR/GPIO_DISP_B2 bank。 ​​ROM更新​​: 清理ROM补丁(不影响开放API)。 ​​HAB API向量表地址​​:从 0x0021_1C0C (A版)改为 0x0021_1C14 (B版)。 ROM_FLEXSPI_NorFlash_ClearCache() 入口地址变更(详见第6节)。 ​​芯片ID变更​​: MISC_DIFPROG 寄存器的 CHIPID 复位值变化: A版: 0x001170A0 B版: 0x001170B0 (需通过bit[7:4]区分:A版= 1011 ,B版= 1100 )。 ​​2. 数据手册变更 (Data Sheet Changes)​ ​ ​​型号命名​​:所有型号后缀从 A 改为 B (例: MIMXRT117xxxxxB )。 ​​GPIO电气规范​​: ​​表37​​:GPIO_AD/LPSR/DISP_B2的驱动电流调整(如DSE=1时IOH从-10mA→-9mA)。 ​​表40​​: 新增 Vpead 参数。 上升/下降时间调整(如DSE=0/SRE=1时从6ns→7.5ns)。 ​​关键建议​​: 3.3V模式:≥25MHz用连续范围模式(Continuous Range),<25MHz用高范围模式(High Range)。 1.8V模式:推荐低范围模式(Low Range)。 ​​其他更新​​: 存储温度范围:-40℃ → ​​-55℃​​。 SDR50/SDR104时序:输入建立时间从2.5ns→2.0ns。 FlexSPI时序:TDVO最大值从4→1,TDHO最小值从2→0。 ​​3. 参考手册变更 (Reference Manual Changes)​ ​ ​​芯片ID识别​​: MISC_DIFPROG[7:4] 复位值从固定值改为​​芯片版本标识​​(A版= 1011 ,B版= 1100 )。 ​​4. 勘误变更 (Errata Changes)​   参考资料:i.MX RT1170A Errata,  i.MX RT1170B Errata​ ​​修复问题​​: 移除ERR052351(GPIO参数漂移)和ERR050643(上电脉冲问题)。 ​​新增问题​​: ​​ERR052401​​:SEMC_CSX1/2/3信号时序退化(SYNC模式最大延迟增加2.4ns)。 ​​规避方案​​: SYNC模式:优先使用SEMC_CSX0或SEMC_RDY作为片选。 Async模式:调整SEMC配置寄存器(SRAMCR1/NORCR1的CES位)。 ​​5. SDK代码变更 (SDK Code Changes)​ ​ ​​SDK 25.06​​(2025年6月底发布)支持B版。 ​​关键代码调整​​: ChipID 和  ROM_API bootloader入口地址  变更 /*! * @brief ROM API init. */ void ROM_API_Init(void) { if (ANADIG_MISC->MISC_DIFPROG == 0x001170a0U) // A版 { g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0020001cU); } else // B版 { g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0021001cU); } } FlexSPI缓存清除函数入口地址变更 :ROM_FLEXSPI_NorFlash_ClearCache /*! @brief Software reset for the FLEXSPI logic. */ void ROM_FLEXSPI_NorFlash_ClearCache(uint32_t instance) { uint32_t clearCacheFunctionAddress; if (ANADIG_MISC->MISC_DIFPROG == 0x001170a0U) { clearCacheFunctionAddress = 0x0020426bU; } else if (ANADIG_MISC->MISC_DIFPROG == 0x001170b0U) { clearCacheFunctionAddress = 0x0021a3b7U; } else { clearCacheFunctionAddress = 0x0021a3bfU; } HAB API vector table addresses变更 :从0x0021_1C0C(i.MX RT1170A) to 0x0021_1C14(i.MX RT1170B). SDK无影响,SBL github已经解决。 ​​6. 工具变更 (Tool Changes)​ ​ ​​J-Link​​:需升级至​​v8.38或更高版本​​。 ​​MCUXpresso​​:v24.12及更早版本需更新 RT1170_reset.scp 脚本中的芯片ID检测逻辑。 ​​7. 通用数据手册更新 (Appendix A)​ ​ ​​电压范围​​: NVCC_GPIO重命名为​​NVCC_AD​​(后续版本将恢复原名)。 NVCC_AD/DISP2/LPSR最大值从1.95V→​​1.98V​​。 ​​GPIO模式定义​​: 统一命名:​​连续范围模式​​(原Normal/Derated)、​​低范围模式​​(原Low)、​​高范围模式​​(原High)。 ​​时序优化​​: LPSPI主模式频率上限从30MHz→​​60MHz​​,建立时间从10ns→3ns。 ​​新增警告​​: GPIO_AD/LPSR/DISP_B2的NVCC不可悬空,否则可能漏电​​500μA/每Bank​​。 ​​8. 其他信息​ ​ ​​文档版权​​:示例代码遵循​​BSD-3-Clause许可证​​。 ​​参考文档​: AN14716 MCUXPresso SDK i.MX RT
記事全体を表示
This article uses i.MXRT1170 as an example, but the rules apply to the i.MX RT series. 1. Backgroud and Questions DataSheets (e.g, RT1170A , RT1170B) show the 'NON JEDEC'  Package as following, but the Product quality page (e.g MIMXRT1172AVM8A) is marked as WSL 3 (Moisture Sensitivity Level 3), which is one of the moisture sensitivity levels defined in JEDEC-STD-020. Is there a contradiction? Does the product comply with JEDEC-STD-020?  2. What is JEDEC-STD-020? JEDEC-STD-020 is a standard that defines the moisture sensitivity level (MSL) and preconditioning requirements for surface-mount devices (SMDs) during the reflow soldering process. Compliance with this standard means that the device's storage and handling before reflow soldering meet industry specifications, making it suitable for automated manufacturing environments. 3. WSL 3 and JEDEC-STD-020 Compliance  On NXP’s product quality page, some i.MX RT1170 variants are marked as WSL 3 (Moisture Sensitivity Level 3), which is one of the levels defined in JEDEC-STD-020. This means: The device can be exposed to ambient conditions for 168 hours before reflow soldering;  It must be stored in dry-pack packaging; It complies with JEDEC-STD-020 handling and processing requirements. This indicates that i.MX RT1170 series have been tested and qualified according to JEDEC-STD-020. Key parameters from NXP Product pages: MSL (Moisture Sensitivity Level): 3 Peak Package Body Temperature: 260°C Time at Peak: 40 seconds 4. “NON JEDEC” Packge in the Datasheet In the i.MX RT1170 datasheet, some package types are labeled as “NON JEDEC”, which typically means: The package dimensions or layout do not strictly follow JEDEC standard outlines; The device has not undergone the formal JEDEC-STD-020 certification process. For example, the IMXRT1170BCEC Rev.1 datasheet states: Package Information: Plastic Package 289-pin MAPBGA, 14 x 14 mm, 0.8 mm pitch Package Type: NON JEDEC [1] This indicates that the package is not a JEDEC-standard mechanical outline. However, it does not necessarily mean the device fails to meet the moisture sensitivity requirements defined in JEDEC-STD-020. 5. In summary 'NON JEDEC' refers only to mechanical form, not to reliability standards. The "NON JEDEC" marking on a datasheet refers to the ​​physical package outline​​, while the MSL 3 rating on the product quality page is a ​​reliability and handling specification​​ determined through JEDEC test methods. JEDEC-STD-020 is a moisture sensitivity level testing standard for non-hermetic surface-mount devices. i.MX RT explicitly states that its MSL rating is based on the JEDEC-STD-020 testing process. Whether a package conforms to a JEDEC standard (such as MO-220) has no direct bearing on whether it can be tested under JEDEC-STD-020. ‘NON JEDEC’是指物理封装中的机械形式,不是可靠性标准。 JEDEC-STD-020 是针对非气密性表面贴装器件的湿敏等级测试标准; NXP 明确表示i.MX RT产品 MSL 等级是依据 JEDEC-STD-020 测试流程; 封装是否为 JEDEC 标准(如 MO-220)与是否能进行 JEDEC-STD-020 测试无直接关系。 6. Reference NXP i.MX RT1170 Product Page: https://www.nxp.com/part/MIMXRT1172AVM8A  i.MX RT1170 Datasheet: https://www.nxp.com/docs/en/data-sheet/IMXRT1170CEC.pdf  JEDEC-STD-020 Standard: https://www.jedec.org/document_search/field_doc_type/151?search_api_views_fulltext=%E2%80%8BJ-STD-020&order=title&sort=asc       
記事全体を表示
There are two version of the i.MX RT1170 Evaluation Kit:  MIMXRT1170-EVK (no longer available for purchase) MIMXRT1170-EVKB   The key differences between the two versions of are laid out in the MIMXRT1170-EVKB Board Hardware User Guide:    One important change is the QuadSPI flash used on each board. This means that if you attempt to use SDK projects created for the RT1170-EVKB, it will not run properly on an older RT1170-EVK board due to using the mismatched QSPI configuration data. And new releases of MCUXpresso SDK only support the newer EVKB board.  However there is a simple fix to get those newer i.MX RT1170 EVKB MCUXpresso SDK projects to run on the older i.MX RT1170 EVK hardware. Simply download the MCUXpresso SDK 2.16.00 for the original RT1170-EVK board, unzip the archive file, and then copy the evkmimxrt1170_flexspi_nor_config.h and evkmimxrt1170_flexspi_nor_config.c files found in \SDK_2_16_000_MIMXRT1170-EVK\boards\evkmimxrt1170\xip into your EVKB project's xip folder. Then either delete/rename the EVKB version of the evkbmimxrt1170_flexspi_nor_config.c and evkbmimxrt1170_flexspi_nor_config.h files from the project to avoid compiler conflicts. This will update the QSPI configuration for that project to be compatible with the QSPI hardware on the original EVK. As an exmaple, here is the RT1170 Hello World project with that change - the EVKB files were renamed with a .orig extension so they would not be included in the compilation:    Note that due to the new hardware features found on the EVKB board there are some EVKB SDK projects that simply can't be supported on the original EVK board. But this work-around will provide support for many MCUXpresso SDK projects that don't require those new EVKB board features. 
記事全体を表示
Recovery Methods for RT595 and RT685 Development Boards When Programming Fails During the development and use of RT595 and RT685 development boards, developers often encounter a common issue reported by users: persistent errors during programming via a debugger, making it impossible to reprogram the board and effectively rendering it “bricked.” These issues can arise from various causes, such as incorrect FCB writing, interruptions during the download process, or other unknown anomalies. This article introduces two effective recovery methods: Using the SEC TOOL utility. Using an external J-Link programmer. Note: Both methods require setting the RT595 and RT685 boards to Serial ISP mode beforehand. NXP has released two RT685-based development boards (MIMXRT685-AUD-EVK and MIMXRT685-EVK) and one RT595 board. Since the RT595 board operates similarly to the RT685 boards, this article uses the MIMXRT685-AUD-EVK board for demonstration. Ensure the SDK version is correct during the process. 1. Preparation: Entering Serial ISP Mode Using the MIMXRT685-AUD-EVK board as an example, set switches SW5[1-3] to “ON OFF OFF” to enter Serial ISP mode. This corresponds to the following pin levels: PIO1_17: High PIO1_16: High PIO1_15: Low Refer to the RT600 User Manual for detailed mappings between ISP pins and boot modes.   2. Method 1: Recovery Using SEC TOOL  1. Preparation: Generate APP Image Import SDK Demo: Open MCUXpresso IDE and import the demo project mimxrt685audevk_lpc_gpio_led_output_cm33.   Modify Project Settings: Make two key configuration changes to ensure successful image generation. Generate Hex File: After configuration, build the project to generate a Hex file for use with SEC TOOL. 2. Using SEC TOOL Download SEC TOOL: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING Create Workspace: Launch SEC TOOL and create a new workspace for MIMXRT685S. Select Connection Method: RT500 and RT600 support USB, UART, SPI, and I2C. Choose one (e.g., UART via J5 or USB via J7). Only one protocol can be used at a time. If switching, power cycle the board. Configure Flash Type and Test: Select the default external NOR Flash for MIMXRT685-AUD-EVK, apply settings, and run a test. Build Image: Use the previously generated App image and click “Build Image.”    Program Image: Flash the image to the RT685 chip.   Switch Boot Mode: Power off the board and set Boot mode to FlexSPI Boot from PortB: PIO1_17: Low PIO1_16: High PIO1_15: Low SW5[1-3]: “ON OFF ON” Power on the board again. It should now operate normally and run the program successfully. 3. Method 2: Recovery Using J-Link Programmer 1. Preparation: Generate Flashable File Import the same demo project into MCUXpresso IDE and compile it without modifications to generate a Hex or S19 file. Download and install SEGGER J-Flash from SEGGER Official Website. 2. Hardware Setup Board Modifications: Connect pins 2 and 3 of JP2. Remove jumpers JP17, JP18, JP19 (ensure p3 is disconnected). Set SW5 to “ON OFF OFF”. Device Connection: Connect J-Link Plus to J19 on the board. Connect J6 to the PC to power the board. 3. Programming with J-Flash Create New Project: Open J-Flash and create a new project for MIMXRT685S. Note: RT685 supports only SWD, not JTAG. Flash Program: Load the Hex file and flash it to the board.   Switch Boot Mode: After flashing, power off the board and set Boot mode to FlexSPI Boot from PortB: PIO1_17: Low PIO1_16: High PIO1_15: Low SW5[1-3]: “ON OFF ON” Power on the board again. It should now function normally and run the program successfully.   Conclusion By following either of the two methods described above, developers can effectively recover RT595 and RT685 development boards from programming failures and restore normal operation. Choose the method that best suits your specific situation. 
記事全体を表示