i.MX RT Crossover MCUs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Crossover MCUs Knowledge Base

Discussions

Sort by:
These lab guides provide step-by-step instructions on how to take a quantized TensorFlow Lite model and use the Neutron Compiler Tool found in eIQ Neutron SDK to convert the model to run on the eIQ Neutron NPU found on i.MX RT700 devices.  The eIQ Neutron NPU for i.MX RT700 Lab Guide documents focus on using the Neutron Compiler tool found inside eIQ Neutron SDK  to convert a model and then import that converted model into an eIQ MCUXpresso SDK example. There are labs for VSCode, GCC, and MCUXpresso IDE.    The labs were designed to run on the i.MX RT700 EVK, but the same concepts can be applied to MCX N boards as well and are similar to the MCX N eIQ Neutron NPU labs. You can also explore the TFLM Getting Started Guide for information on how to use your own model and data for inference.  Also be sure to check out AN14700 - i.MX RT700 eIQ Neutron NPU Enablement and Performance which goes into more details on the eIQ Neutron N3-64 NPU found on i.MX RT700.    --- Updated October 2026 for MCUXpresso SDK 26.09
View full article
This article will describe how to use the HiFi modules found on certain NXP microcontrollers as an optional method for inferencing a model.  There are several ways of running a TFLite neural network model on NXP microcontrollers: Inference a model only using the main core of the device (CM33 or M7) MCX N i.MX RT1050 i.MX RT1060 i.MX RT1170 i.MX RT1180 i.MX RT595 i.MX RT685 i.MX RT700   Inference a model directly on the HiFi4 or HiFi1 core (on supported platforms) i.MX RT595 i.MX RT685 i.MX RT700   Use the Neutron NPU to accelerate inference of a model - with the CM33 controlling the NPU and acting as a fallback for any non-NPU supported layers i.MX RT700 MCX N   Use the Neutron NPU to accelerate inference of a model - with the HiFi4 controlling the NPU and acting as a fallback for any non-NPU supported layers i.MX RT700     This article will cover options #2 and #4 which make use of the HiFi DSP module. Running a model on the HiFi4 (option #2) will be much faster than running a model just on the CM33/M7 (option #1).   However using the NPU (options #3 and #4) will be significantly faster than only using the DSP due to the hardware optimizations that an NPU provides for neural network calculations. The exact performance gains will be model specific, and also depend on the layer(s) that may not have been converted to use the NPU as NeutronGraph nodes. The accuracy should remain the very similar regardless of method being used. Any type of TFLite neural network model can be ran on the HiFi1/HiFi4 as those DSP modules are just being used accelerate the neural network math that the model uses. Below are the inference times of a CIFAR10 model on i.MX RT700 with different hardware modules used to inference the model (using default MCUXpresso SDK projects).  CM33: 103.653ms HiFi1*: 19.007ms HiFi4: 12.312ms NPU w/ CM33 Fallback: 0.883ms NPU w/ HiFi4 Fallback: 0.883ms *HiFi1 max frequency is 250MHz. All others are run at 325MHz.     Software requirements: Go to the Cadence i.MX RT700 or Cadence i.MX RT685 pages to download the following software. Xtensa Xplorer IDE License Key HIFI DSP Configuration File (NEWLIB) If using a HiFi4 example then download the HiFi4 license and DSP configuration files. Likewise, if using a HiFi1, then will need the HiFi1 license and DSP configuration files. Also you will need to download the Windows or Linux version of these files depending on which host OS you are using on your PC. Finally add the following global system variables which should be set based on the location that Xtensa Explorer was installed (assuming RT700 with HiFi4): XCC_DIR=<install_dir>\XtDevTools\install\tools\RI-2023.11-win32\XtensaTools XTENSA_CORE= rt700_hifi4_RI23_11_nlib   MCUXpresso SDK HiFi ML Examples: There are several HiFi related examples in MCUXpresso SDK for i.MX RT700: tflm_cifar10 – Uses Neutron NPU to inference the CIFAR10 model and uses the CM33 as the fallback for any non-NPU operators. tflm_cifar10_hifi1 – Uses HiFi1 to inference the CIFAR10 model. Does not use the Neutron NPU tflm_cifar10_hifi4 – Uses HiFi4 to inference the CIFAR10 model. Does not use the Neutron NPU tflm_cifar10_hifi4_neutron – Uses Neutron NPU to inference the CIFAR10 model and uses the HiFi4 as the fallback for any non-NPU operators.   tflm_label_image – Uses Neutron NPU to inference the CIFAR10 model and uses the CM33 as the fallback for any non-NPU operators. tflm_label_image_hifi4 - Uses HiFi4 to inference the Mobilenet model. Does not use the Neutron NPU   When using the HiFi eIQ projects provided in MCUXpresso SDK, ensure that the SDK is: Located in a short filename path (ie C:\nxp\RT700), as an excessively long filename path can cause compile issues Directory path contains no spaces If using VS Code import as a Repository project instead of Free Standing. Ensure using at least MCUXPresso SDK 26.03 as there are several important fixes in the 26.03 release for HiFi4 projects   Extending Memory Area in HiFi4 Examples for Larger Models: Open:  Github SDK Layout: \mcuxsdk\examples\_boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4_neutron\linker\hifi4\gdbio\ldscripts\elf32xtensa.x Classic SDK Layout: \boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4_neutron\linker\hifi4\min-rt\ldscripts\elf32xtensa.x  And make modifications below to extend the memory used for models.  dsp_core_seg :  org = 0x20200000, len = 0x200000  dsp_core_ncache_seg :  org = 0x20400000, len = 0x180000        _memmap_mem_dsp_core_start = 0x20200000;  _memmap_mem_dsp_core_end   = 0x20580000;  _memmap_seg_dsp_core_start = 0x20200000;  _memmap_seg_dsp_core_max   = 0x20580000;         Ensure that the stack heap is at 0x2058_0000:    PROVIDE(__stack = 0x20580000);    _heap_sentry = 0x20580000;          Now larger models will compile successfully in Xtensa.    Then after copying in the compiled HiFi4 binary files into the MCUXpresso IDE project, modify dsp_config.h file to update the DSP_SRAM_ADDRESS:  Github SDK Layout: \mcuxsdk\examples\_boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4_neutron\dsp_config.h  Classic SDK Layout:  \boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4_neutron\cm33_core0\dsp_config.h (or source\dsp_config.h in MCUXpresso IDE)      Then clean and build the project.   HiFi Lab: See the attached lab document for more details on using the HiFi DSP modules to inference models.      
View full article
eIQ Neutron SDK is a new software package that includes the Neutron Compiler tool and eIQ Neutron libraries to run Neutron converted neural network models on devices that have an eIQ Neutron NPU like MCX N, i.MX RT700, or i.MX95 Previously the Neutron Compiler tool was part of eIQ Toolkit. However going forward, new versions of the Neutron Compiler tool will be released as part of the eIQ Neutron SDK. This change will allow for more frequent updates to provide better performance and additional operator support. The Neutron Compiler tool was previously named the Neutron Converter tool, but the name was changed in August 2026 with the release of eIQ Neutron SDK 3.2.1. The functionality is the same, just the name changed.  MCUXpresso SDK and Linux BSP use Neutron libraries as part of the eIQ examples included in those software releases. However to use the latest Neutron Compiler, an eIQ project will need to be updated to use the latest Neutron software libraries. This post walks through where to place the updated Neutron libraries and header files.    If the version of the Neutron Compiler tool that was used to convert a model does not match the Neutron libraries used by the eIQ project, then during inference you will see the following error(s) printed on the serial terminal and may get incorrect results: Microcode version mismatch Or Internal Neutron NPU driver error 281b in model prepare Or Incompatible Neutron NPU microcode and driver versions The version of the Neutron Compiler tool that was used to convert a model can be found by either viewing the converted model in Netron or by looking at the generated header file:     Here is a table showing where you can find the matching version of the Neutron Compiler tool for the default Neutron libraries found in different versions of MCUXpresso SDK: MCUXpresso SDK Default Neutron Library Version in MCUXpresso SDK Default Compatible Neutron Compiler/Converter Can Be Found In 24.12 1.2.0+0x6f710a6d eIQ Toolkit 1.17 25.03 1.2.0+0X1b86b19d eIQ Toolkit 1.17 25.06 2.0.2 eIQ Toolkit 1.17 25.09 2.1.3 eIQ Toolkit 1.17 25.12 2.2.2 eIQ Neutron SDK 2.2.2 26.03 3.0.0 eIQ Neutron SDK 3.0.0 26.06 3.1.1 eIQ Neutron SDK 3.1.1 26.09 3.2.2 eIQ Neutron SDK 3.2.2 Manually Update SDK Libraries To Use Latest Version   eIQ Neutron SDK 3.2.3   Since Neutron library v3.2.0, the version of the Neutron library being used in a project can be determined with: #include "NeutronDriver.h" NeutronSdkVersion version=neutronGetSdkVersion(); PRINTF("Neutron Library Version %d.%d.%d\r\n", version.major, version.minor, version.patch);       It is highly recommend to always use the latest Neutron Compiler tool and to update the libraries in your eIQ project to match the latest Neutron Compiler tool. The libraries can be updated by overwriting the original files. You may wish to make a backup first though as the default eIQ examples in that SDK will use models that were converted to match those original Neutron libraries. The Neutron file structure in eIQ Neutron SDK and MCUXpresso SDK are now the same so that the entire Neutron folder can be overwritten directly.    Updating Neutron Libraries in MCUXpresso SDK 25.12 and later: File Source Directory in eIQ Neutron SDK Target Directory in MCUXpresso SDK libNeutronDriver.a target\imxrt700\ rt700\cm33\ \middleware\eiq\neutron\rt700\cm33\ libNeutronFirmware.a target\imxrt700\ rt700\cm33\ \middleware\eiq\neutron\rt700\cm33\ NeutronDriver.h target\imxrt700\ driver\include\ \middleware\eiq\neutron\driver\include\ NeutronErrors.h target\imxrt700\ common\include\ \middleware\eiq\neutron\common\include\   Note: The target\imxrt700\driver\include\NeutronEnvConfig.h and the libraries in target\imxrt700\cmodel are used by the ExecuTorch inference engine and so are not needed for TFLM eIQ projects.  Note: If updating the HiFi4 Neutron libraries use the ones in the RJ-2025.5 folder Note: In MCUXpresso SDK 26.03 there are two sets of Neutron libraries in imported projects. It's the files in the /middleware/eiq folder that need to be updated.      Updating Neutron Libraries in MCUXpresso SDK 25.09 or before: File Source Directory in eIQ Neutron SDK Target Directory in MCUXpresso SDK libNeutronDriver.a target\imxrt700\ rt700\cm33\ \middleware\eiq\tensorflow-lite\third_party\neutron\rt700\ libNeutronFirmware.a target\imxrt700\ rt700\cm33\ \middleware\eiq\tensorflow-lite\third_party\neutron\rt700\ NeutronDriver.h target\imxrt700\ driver\include\ \middleware\eiq\tensorflow-lite\third_party\neutron\driver\include\ NeutronErrors.h target\imxrt700\ common\include\ \middleware\eiq\tensorflow-lite\third_party\neutron\common\include\   Updating Neutron Libraries for MCUXpresso SDK 2.16 or before: Replace the entire middleware\eiq directory from MCUXpresso SDK 26.03 into your project, and then the Neutron libraries can be updated per the instructions above. In these older MCUXpresso SDK releases there were additional eIQ changes beyond just the four files above, so the easiest method to update those older projects is just to replace the entire eIQ middleware directory.        Updating Neutron Libraries for i.MX devices: To update the neutron runtime on a target device, upload the files to their designated directories, as follows:   File Target Directory NeutronFirmware.elf /lib/firmware libNeutronDriver.so /lib/ libneutron_delegate.so /lib/  
View full article
OEM Key Import, Signed Message, and TLV Blob Generation Flow  Based on the i.MX RT1180 EdgeLock Enclave 
View full article
i.MX RT1170 MCUboot-Custom ECDSA Keys and Direct-XIP OTA Validation Abstract This article uses the MIMXRT1170-EVKB platform to demonstrate how to generate a custom ECDSA-P256 key pair for MCUboot, replace the default public key in the mcuboot_opensource project, and re-sign application images with the new private key. It then uses the Shell and XMODEM functions provided by ota_mcuboot_basic to transfer a candidate image to the Secondary Slot. MCUboot performs signature verification, image-state checks, and version selection, and uses Flash Remap to support Direct-XIP execution. The results show that an image signed with the old key cannot be verified by the new public key, while a higher-version LED image signed with the new private key can be written to the Secondary Slot and started directly through Flash Remap. Important: The addresses, slot sizes, and commands in this article apply to the RT1170 example project used in this validation. Before porting the procedure to another project, verify the linker script, Flash partitioning, and MCUboot configuration. 1. Why Replace the Default Signing Key? The MCUboot example key included in the NXP MCUXpresso SDK is intended for development and validation only. Because it is publicly available, it is not suitable for production releases. For production, the release owner should securely protect the private key and compile only the corresponding public key into the bootloader. After the public key is replaced, images signed with the old private key should fail signature verification, confirming that the new key has taken effect. Signature verification, version management, and image confirmation serve different purposes—ensuring a trusted source, selecting an upgrade image, and managing runtime state, respectively—and cannot replace one another. 2. Platform Configuration and Scope 3. Flash Layout  Each signed image contains a 0x400-byte MCUboot header that records boot metadata such as the image size and version. At power-on, MCUboot checks the images in both slots, parses the header and TLV area, verifies image integrity and the ECDSA signature, and evaluates image state and version. In the test configuration used here, images are generated with --confirm. Among images that satisfy the signature and state requirements, MCUboot selects the higher version that complies with the upgrade policy. This behavior applies only to this test configuration and does not represent every MCUboot state or upgrade policy. In DIRECT-XIP + FLASH REMAP mode, if the selected image is stored in the non-default mapped slot, MCUboot configures Flash Remap before jumping to the application. This maps the image's physical storage region to the logical execution address expected by the application, allowing in-place execution without copying or swapping images. 4. MCUboot Signature Verification Fundamentals Important: A hash detects content changes; a digital signature verifies image origin and integrity; the version number identifies and compares image releases; and the Confirm state determines whether a test image is retained permanently. 5. Generate an ECDSA-P256 Private Key in the scripts Directory imgtool.py is located in the middleware\mcuboot_opensource\scripts directory of the MCUXpresso SDK. Change to this directory before running the key-generation command. Replace <SDK_INSTALL_PATH> with the actual SDK installation path on your computer: <SDK_INSTALL_PATH>\middleware\mcuboot_opensource\scripts python imgtool.py keygen ^  -k my_priv.pem ^  -t ecdsa-p256 dir my_priv.pem keygen: Generates a new key. -k my_priv.pem: Specifies the output key file. -t ecdsa-p256: Selects the ECDSA-P256 algorithm. After the command completes successfully, the private key is generated as middleware\mcuboot_opensource\scripts\my_priv.pem. Security reminder: In a production project, never compile the private key into the bootloader, program it into the MCU, commit it to a regular Git repository, or distribute it with the SDK project. Store only the public key in the bootloader. 6. Export and Replace the MCUboot Public Key python imgtool.py getpub -k my_priv.pem python imgtool.py getpub -k my_priv.pem > my_pub.c The command outputs a C array that can be compiled by MCUboot. The key symbols are: const unsigned char ecdsa_pub_key[] = {     0x30, 0x59, ... }; const unsigned int ecdsa_pub_key_len = 91; The public-key source file replaced in this article is: evkbmimxrt1170_mcuboot_opensource_cm7\bootutil\nxp_port\keys\sign-ecdsa-p256-pub.c Back up the original public-key file, and do not include the backup copy in the project build. Replace the original public-key array with the output from getpub. Keep the ecdsa_pub_key and ecdsa_pub_key_len symbol names consistent with the project references. Clean and rebuild evkbmimxrt1170_mcuboot_opensource_cm7. Program the new bootloader at 0x30000000. 7. Negative Validation: Images Signed with the Old Key Are Rejected Replace only the signature-verification public key in MCUboot, rebuild and program the updated bootloader, and leave the existing application image in Flash without re-signing it with the new private key. Because the image is still signed with the old private key while MCUboot now verifies it with the new public key, the key pair does not match. The image therefore fails signature verification and is classified as invalid. In the project configuration used here, the bootloader then erases the invalid image. This negative test confirms that the new public key has been compiled into MCUboot correctly and is actively used during boot verification. If the image signed with the old key is classified as invalid, the new public key has been compiled correctly and is being used for MCUboot verification. Successfully parsing the image header and reading the version only proves that the image structure is recognizable; it does not mean signature verification passed. A digital signature generated with the old private key cannot be verified by a nonmatching new public key. The version number is used only for image identification and upgrade selection. It cannot replace signature verification; even an image with a correct or higher version will not boot if signature verification fails. 8. Sign the ota_mcuboot_basic Image with the New Private Key python imgtool.py sign ^  --key my_priv.pem ^  --align 4 ^  --version 1.4.0 ^  --slot-size 0x200000 ^  --header-size 0x400 ^  --pad-header ^  --pad ^  --confirm ^  evkbmimxrt1170_ota_mcuboot_basic_cm7.bin ^  ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin evkbmimxrt1170_ota_mcuboot_basic_cm7.bin is the raw application image generated by the Basic project. In this example, --confirm is added so that the image is generated with the Confirmed state. Note the following: Notes on --confirm and Production Deployment The README states that an initial image manually programmed together with the bootloader requires the additional --pad and --confirm options. Otherwise, the bootloader may reject the image because the trailer lacks the required state information. --pad pads the image to the size specified by --slot-size and creates the slot trailer required by MCUboot. --confirm presets the image_ok flag in the trailer to the confirmed state while the image is generated. MCUboot therefore treats the initial image as a confirmed valid image at boot. Production recommendation: This usage is intended mainly for the initial image manually programmed together with the bootloader. It is not recommended for production OTA images. Pre-confirming an update image with --confirm bypasses MCUboot's test boot → image confirmation → failure rollback flow. If the new image cannot boot, fails peripheral initialization, or encounters a critical application error, MCUboot cannot use the unconfirmed state to roll back automatically, which may leave the device unrecoverable. The MCUboot bootloader primarily reads the image_ok flag in the trailer and uses it for image-state evaluation, version selection, and rollback handling. It does not proactively write the confirmation flag on behalf of the application. The running application should explicitly confirm the image at an appropriate time. For example, after the candidate application completes its startup self-test, peripheral initialization, and critical functional checks, it can call boot_set_confirmed(). An application with Shell support, such as ota_mcuboot_basic, can also be confirmed manually with the image accept command. This preserves MCUboot's test-boot and failure-rollback capabilities and prevents a faulty image from being marked permanently valid too early.   python imgtool.py dumpinfo ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin Check the magic, hdr_size, img_size, version, and TLV information in the output. The TLV area should contain SHA256, KEYHASH, and ECDSASIG, which represent the image digest, public-key identifier, and ECDSA signature respectively. 9. Program the Signed ota_mcuboot_basic Image into the Primary Slot This article uses ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin, generated in the previous section, as the initial image in the Primary Slot. ota_mcuboot_basic provides the Shell and XMODEM image-receive functions. After it starts, the application can transfer subsequent candidate images to the Secondary Slot. Program the signed image containing the complete MCUboot header, application payload, and signature TLV—not the raw BIN generated directly by the application project. File to program: ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin Programming address: 0x30040000 Program the complete signed image at the Primary Slot start address, 0x30040000. Reset the device and inspect the MCUboot log to confirm that signature verification succeeds and the version is read correctly. Confirm that the device enters the ota_mcuboot_basic Shell and that image info reports the image state. 10. Generate a Candidate Signed Image for the Secondary Slot This article creates an LED application project and uses it as the candidate image for the Secondary Slot. The image is signed with the newly generated private key, my_priv.pem, and assigned a version later than the currently running image. In DIRECT-XIP + FLASH REMAP mode, both the LED and ota_mcuboot_basic projects are linked to the same logical addresses: the signed image begins logically at 0x30040000, and the application vector table is at 0x30040400. The signed LED image is physically written to the Secondary Slot at 0x30240000, with its vector table physically located at 0x30240400. When MCUboot selects this image, Flash Remap maps the Secondary Slot to the logical execution address expected by the application. Therefore, the Secondary Slot identifies the image's physical storage location, while the application still executes using the logical addresses associated with the Primary Slot. python imgtool.py sign ^  --key my_priv.pem ^  --align 4 ^  --version 1.5.0 ^  --slot-size 0x200000 ^  --header-size 0x400 ^  --pad-header ^  --pad ^  --confirm ^  evkbmimxrt1170_igpio_led_output_cm7_second_app.bin ^  ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin --key my_priv.pem: Uses the private key paired with the public key currently trusted by MCUboot. --version 1.5.0: Sets the candidate image version, which must be later than the currently running version 1.4.0. --slot-size 0x200000: Matches the slot size in the current Flash partition layout. --header-size 0x400 and --pad-header: Reserve and populate the 0x400-byte MCUboot header area at the beginning of the image. --pad: Pads the output to the full size specified by --slot-size and reserves the image trailer area. Whether the image is pre-confirmed is controlled by --confirm. --confirm: Generates the candidate image in the Confirmed state. python imgtool.py dumpinfo ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin Before transfer, verify that the output reports valid magic, hdr_size, img_size, version, and TLV information. In particular, confirm that the version is 1.5.0+0 and that the TLV area contains SHA256, KEYHASH, and ECDSASIG. After the checks pass, use the complete ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin file in the next section. The ota_mcuboot_basic application transfers it to the Secondary Slot through XMODEM. 11. Transfer the Signed Image to the Secondary Slot Using XMODEM Start the development board, enter the Basic Shell, and run the xmodem command. In the serial terminal, select File → Transfer → XMODEM, select ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin, and start the transfer. After the transfer completes, run image info and verify the version and image state in the Secondary Slot. 12. Inspect the Candidate Image and Validate Version Switching image info reboot After reboot, inspect the MCUboot log for the Primary and Secondary versions, confirmation states, and selected boot slot. In the test configuration used here, the candidate image is pre-confirmed with --confirm. It must pass signature verification, satisfy the Confirmed-state requirements, and have a later version that complies with the upgrade policy. A valid signature means only that the image source is trusted and the content is intact; it does not guarantee that the image will be selected. Once all conditions are met, MCUboot boots the candidate image. In Direct-XIP + Flash Remap mode, the image can execute in place from the Secondary Slot without being copied or swapped. 13. Summary Generate and securely store a project-specific ECDSA-P256 private key, and compile the corresponding public key into the MCUboot project. Confirm that key replacement is effective by verifying that images signed with the old key fail while images signed with the new private key pass. Use the signed ota_mcuboot_basic image as the initial Primary Slot image and the later-version signed LED image as the Secondary Slot update image. Transfer the complete signed image to the Secondary Slot through XMODEM and validate the MCUboot flow that starts the update image through Flash Remap. For production OTA, remove --confirm and have the application write image_ok by calling boot_set_confirmed() after successful self-tests, preserving MCUboot's automatic rollback capability.
View full article
Zephyr now supports the eIQ Neutron NPU on MCX N and i.MX RT700. This article will describe how to get Zephyr and use the eIQ Neutron NPU libraries and examples.  Some previous experience with eIQ Neutron NPU enablement is assumed, so ensure you're familiar with the eIQ Neutron SDK, converting models for eIQ Neutron NPU, and basic ML concepts by going through the MCX N or i.MX RT700  NPU bare-metal lab guides for VS Code before continuing on below.  Install Software Run the MCUXpresso Installer tool and install three key components: Zephyr Developer Arm GNU Toolchain Zephyr SDK LinkServer   Install LinkServer and add LinkServer to the PATH Install VS Code and MCUxpresso VS Code plugin   Download Zephyr Open VSCode Go to the MCUXpresso for VSCode plugin and click on Import Repository Go to the Remote tab and select the Zephyr repository. Choose it a directory name and location to download the repository to, and then click on Import.   It will take approximately 30 minutes to download the repository. Near the end of the download there will be several prompts in the terminal asking to accept licenses. Type “y” to accept and hit enter. There will be about 10 of these prompts at the end. Open the MCUXpresso Venv Terminal which has a Python virtual environment with all the paths preconfigured that were installed by MCUXpresso Installer.   In the terminal that pops up, type “1” to select the default environment. Then navigate to the directory you downloaded Zephyr into Run the following commands to get TensorFlow: west config manifest.project-filter -- +tflite-micro west update Go into the zephyr subdirectory folder cd zephyr Now need to explicitly download the Pull Request (PR) that enables eIQ Neutron. This eventually won’t be necessary when Zephyr 4.5 is released in October, but until then will need to type the following In the command prompt to get it:   git remote -v git remote add upstream https://github.com/zephyrproject-rtos/zephyr.git git remote -v   git stash git fetch upstream pull/108834/head:pr-108834 git checkout pr-108834   After this command you should see there’s now a folder at <zephyr_location>\ \zephyr\samples\boards\nxp\tflm_neutron with example source code.   Compile and Run a Zephyr eIQ Neutron NPU example Compile the project with west:  For MCX N: west build -p auto -b frdm_mcxn947/mcxn947/cpu0 samples/boards/nxp/tflm_neutron   For RT700: west build -p auto -b mimxrt700_evk/mimxrt798s/cm33_cpu0 samples/boards/nxp/tflm_neutron Open TeraTerm or other serial terminal program, and connect to the virtual COM port that board enumerated as when you plugged in the USB cable. Use 115200 baud, 1 stop bit, no parity. Flash the resulting code with west flash The serial terminal should show the following: Can debug with west debug      Run your own NPU accelerated ML model in Zephyr Make sure you've gone through the MCX N or i.MX RT700  hands-on labs so you're familiar with the enablement. The same steps for converting a model with the Neutron Compiler tool inside eIQ Neutron SDK, updating the eIQ Neutron libraries, modfiying the operator list, and adding a new model are relevant when using Zephyr, but the file locations will be Zephyr specific. Also note that the header file generated by the Neutron Compiler tool will need to be updated to match the header of the model.hpp file.  Also note that the README.rst file in the Zephyr Neutron example mentions using eIQ Toolkit but that information is outdated and been superseded by eIQ Neutron SDK.  eIQ Neutron example is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron Neutron libraries are at <zephyr_location>\modules\hal\nxp\zephyr\blobs\neutron\ Model data is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\models\mcxn\model.hpp Labels file is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\labels.h kTensorArenaSize variable is set in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 40) and is set to 60KB by default OpResolver is set in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 65) The model is selected in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 11)   Additional References: Blog post on west which Zephyr uses. Zephyr on FRDM-MCXN947 Zephyr on i.MX RT700 Zephyr TensorFlow
View full article
The i.MX RT700 microcontroller family includes an eIQ Neutron N3-64 NPU for accelerating neural network models. The i.MX RT700 EVK can be combined with a camera and LCD screen to showcase running TinyML vision models on a microcontroller. It's recommended to also go through the basic i.MX RT700 NPU Lab to learn more about eIQ enablement on RT700. The rest of this post will cover using vision models with camera+LCD on i.MX RT700.    i.MX RT700 Camera Hardware Setup: The following hardware is used: i.MX RT700 EVK RK055HDMIPI4MA0 LCD panel Camera Options: USB Camera with USB A to micro-B converter OV7670 parallel camera (with optional wide-angle lens) The USB camera should be attached to the i.MX RT700 EVK on USB OTG port J40. The parallel camera interface is available on J53 and uses FlexIO with eDMA to read in the camera data. AN14836 describes the details. Note that the links in that app note for the demo software do not work but the demo code is in the process of being posted on NXP’s Application Code Hub.  When inserting the parallel camera align it to the left most side, as shown in the image below:       Directions for attaching the LCD panel to the J52 connector on the underside of the i.MX RT700 EVK can be found on this Community post.  Note that there are multiple names used for the LCD panel and all these part numbers refer to the exact same panel: RK055HDMIPI4MA0 RK055MHD091 RK055MHD091-CTG RK055MHD091A0-CTG i.MX RT700 Vision ML Examples: There are two vision AI/ML examples for i.MX RT700 available today: Object Detection (part of AN14718) Hand Gesture Recognition Both of these examples use a USB camera.  i.MX RT700 Vision MPP Examples:  The Media Processing Pipeline (MPP) interference examples in i.MX RT700 MCUXpresso SDK 26.06 and later support both parallel and USB camera interfaces. These SDK examples are only available for command line GCC and VS Code MCUXpresso SDK layouts. They are not available for MCUXpresso IDE, IAR, or Keil.    A parallel camera is used by default in the RT700 MPP projects. A USB camera can be enabled by adding a USE_USB_CAMERA declaration in the project's CMakeLists.txt file by adding the following macro:   mcux_add_macro(     CC "-DUSE_USB_CAMERA"     CX "-DUSE_USB_CAMERA" ) However it's important to note that the camera_usb_final_fr_app_view project is setup to use USB camera by default, but it only works with a very specific HM2131 camera. All other MPP demos can work with most generic USB cameras.   
View full article
1. Abstract The GenAVB/TSN Stack FreeRTOS Evaluation User's Guide (version:8.0 Release) covers multiple hardware platforms, software configurations, and evaluation use cases. While comprehensive, the document can be challenging for first-time users to follow due to the large amount of information and the variety of supported scenarios. This article focuses on a specific use case from the User's Guide and provides a detailed, step-by-step walkthrough with screenshots, configuration examples, expected results, and troubleshooting tips. The goal is to help users better understand the setup process and successfully evaluate the GenAVB/TSN stack on NXP platforms. This article walks through Section 4.4, TSN Network Only with TSN Bridge and Standalone Endpoint i.MX RT1180, from the GenAVB/TSN Stack FreeRTOS Evaluation User's Guide. It explains the required hardware setup, firmware build and flashing procedure, board configuration, TSN configuration, execution steps, expected results, and basic troubleshooting tips. 2. Setup 2.1 Hardware Preparation Two i.MX RT1180 boards A PC with a serial terminal emulator. MobaXterm Portable is recommended. At least two USB cables and three Ethernet cables   2.2 Firmware Preparation 2.2.1 Setup IDE and SDK Refer to the NXP GenAVB/TSN MCUXpresso User's Guide to install the required software environment for the selected platform and project. A successful project build confirms that the build environment has been installed and configured correctly. VS Code and MCUXpresso for Visual Studio Code are recommended. 2.2.2 Build Image Note:  The specific operating procedures should still be based on GenAVB/TSN MCUXpresso User's Guide . The explanation below is intended only as a supplement to the original document. For GenAVB_TSN-rtos-apps version 8.0, the CM7 Kconfig file needs to be fixed manually before building the image. Kconfig file path:   Add two lines like the following: Set the Build Configurations of the CM33 project to release_no_enetc0, and then build the project. Set the Build Configurations of the CM7 project to release_enetc0, and then build the project. Note: If you are using MCUXpresso for VS Code, you may not be able to import both the CM33 and CM7 projects of the TSN application into the same workspace at the same time, like the following: If this occurs, remove the existing project from the workspace before importing the project for the other core. This issue is expected to be fixed in a future release. After both the CM33 and CM7 projects are built successfully, the generated .bin files and .elf files can be found in the corresponding output directories:   2.2.3 Flash Image Make sure the board's boot configuration switch is set to Serial Downloader mode. For SDP mode, SW5[1..4] should be set to 0001. Set jumper J1 to position 7–8 so that the evaluation board can be powered through the Debug USB port. Connect one USB cable between the PC and the USB_OTG1 port , which is used for firmware downloading. Connect another USB cable between the PC and the Debug USB port, which is used for power supply and serial communication. Then reset the board. Refer to Chapter 10, "Multi core (Cortex-M33 + Cortex-M7) images flashing" in the GenAVB/TSN MCUXpresso User's Guide. Flash the following generated binaries to the target device: genavb_tsn_rtos_apps\...\release_no_enetc0\evkmimxrt1180_tsn_app_cm33_cm33.bin genavb_tsn_rtos_apps\...\release_enetc0\evkmimxrt1180_tsn_app_cm7_cm7.bin 2.3 Check the Status of the Boards After the flashing operation is completed on both boards, restore the boot configuration switch on each board to Quad SPI mode. For QSPI mode, SW5[1..4] should be set to 0100. Then reset both boards. Remove the jumper on JP7 so that the debug port on each board can enumerate two serial ports. The CM33 and CM7 serial terminal interfaces are provided through the two serial ports enumerated by the debug port. After the boards restart, the red LED D7 should blink, indicating that the TSN application is running. Then, check the hardware connection:     2.4 TSN Configuration and Evaluation   i.MX RT1180 Controller i.MX RT1180 IO Device 1 Step 1. Configure the Controller Standalone TSN Endpoint and IO Device Standalone TSN Endpoint respectively. CM33 shell: Press INSERT key mkdir -p /m7/tsn_app write /m7/boot 1 write /m7/tsn_app/role 0 write /m7/tsn_app/mode 2 write /m7/tsn_app/port_id 1 write /m7/tsn_app/num_io_devices 1 write /m7/tsn_app/period_ns 250000 CM33 shell: Press INSERT key mkdir -p /m7/tsn_app write /m7/boot 1 write /m7/tsn_app/role 1 write /m7/tsn_app/mode 2 write /m7/tsn_app/port_id 1 write /m7/tsn_app/period_ns 250000   Step 2. Reset the boards Reset Reset Step 3. Set hardware address CM33 shell: mkdir -p port0 mkdir -p port1 mkdir -p port2 mkdir -p port3 mkdir -p port4 mkdir -p port5 write port0/hw_addr 54:27:8D:00:00:00 write port1/hw_addr 54:27:8D:00:00:01 write port2/hw_addr 54:27:8D:00:00:02 write port3/hw_addr 54:27:8D:00:00:03 write port4/hw_addr 54:27:8D:00:00:04 write port5/hw_addr 54:27:8D:00:00:05 CM33 shell: mkdir -p port0 mkdir -p port1 mkdir -p port2 mkdir -p port3 mkdir -p port4 mkdir -p port5 write port0/hw_addr 54:27:8D:00:01:00 write port1/hw_addr 54:27:8D:00:01:01 write port2/hw_addr 54:27:8D:00:01:02 write port3/hw_addr 54:27:8D:00:01:03 write port4/hw_addr 54:27:8D:00:01:04 write port5/hw_addr 54:27:8D:00:01:05 Step 4. Set gPTP / (Devices without this command configured remain GM devices.)   CM33 shell: mkdir -p fgptp write fgptp/priority1 248   Step 5. VLAN and FDB entry settings BRIDGE>> vlan_update 2 3 -c 1 -p BRIDGE>> vlan_update 2 4 -c 1 -p BRIDGE>> fdb_update 91:e0:f0:00:fe:70 2 4 -c 1 -p BRIDGE>> fdb_update 91:e0:f0:00:fe:71 2 3 -c 1 -p /   Step 6. Scheduled Traffic settings CM33 shell:   BRIDGE>> cd / BRIDGE>> qbv_set 4 -b 35000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p BRIDGE>> qbv_set 3 -b 160000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p   CM7 shell:   CONTROLLER>> qbv_set 1 -b 35000 -c 250000 -C 0 -l 02,80000 -l fd,170000 CM7 shell:   IO_DEVICE_0>> qbv_set 1 -b 160000 -c 250000 -C 0 -l 02,80000 -l fd,170000 Step 7. Reset the boards and evaluate Scheduled Traffic /   Step 8. Configure Time-Specific Departure (TSD) CM33 shell: Press INSERT key   write /m7/tsn_app/tx_time_enabled 1 write /m7/tsn_app/tx_time_offset_ns 38000 CM33 shell: Press INSERT key   write /m7/tsn_app/tx_time_enabled 1 write /m7/tsn_app/tx_time_offset_ns 38000 Step 9. Reset the boards and evaluate Time-Specific Departure (TSD) /   Note: All use cases require the hardware address and gPTP configurations. The original User's Guide does not fully describe this part, so these steps are explicitly included in this article for clarity. 3. Conclusion This guide summarizes the complete workflow for evaluating the GenAVB/TSN Stack FreeRTOS use case on the i.MX RT1180 platform. It covers the required hardware preparation, firmware build process, image flashing procedure, board boot configuration, serial port verification, and TSN configuration steps. By following the configuration sequence in this document, users can set up the Controller and IO Device roles, configure gPTP, VLAN, FDB entries, Scheduled Traffic, and Time-Specific Departure, and then verify the expected TSN behavior between the two i.MX RT1180 boards.
View full article
ModelRunner is a benchmarking tool for running TensorFlow Lite models on NXP microcontrollers. It supports both HTTP and UART communication modes and provides detailed latency profiling for each model layer. The model profiling information is in JSON format and can be uploaded to the upcoming eIQ AI Toolkit and eIQ AI Hub tools for more detailed analysis.  ModelRunner is available on the following MCU devices: FRDM-MCXN947 MCX-N5XX-EVK MCX-N9XX-EVK MIMXRT700-EVK MIMXRT595-EVK MIMXRT685-EVK MIMXRT1060-EVK MIMXRT1170-EVK There are two methods for using ModelRunner: Via an Ethernet connection to the board Via UART using an emulated network connection  - useful for devices without Ethernet like i.MX RT700   The attached guide walks through how to use both methods. A Windows Powershell or Linux prompt should be used for this lab as a normal Windows command prompt will not parse the commands correctly.   
View full article
There are some items to be aware of when using eIQ projects in VSCode with MCUXpresso SDK 26.03   Debugger hangs when debugging eIQ examples on i.MX RT700 in VSCode There are two work-arounds available: 1) Use a JLink to debug the project instead of the default CMSIS-DAP interface. To do this: Install LinkServer Put a jumper on JP20 on the i.MX RT700 EVK, Update the MCULink firmware to use JLink by running C:\NXP\LinkServer_25.12.83\MCU-LINK_installer\scripts\program_JLINK.cmd Take off the jumper on JP20.    2) Alternatively update the linker file in the eIQ project:  Open the MIMXRT798Sxxxx_cm33_core0_flash.ld linker file in Repository->mcusdk->examples->_boards->mimxrt700evk->eiq_examples->tflm_label_image->cm33_core0->gcc  (use the path based on the eIQ project name that you are trying to use) In that linker file go to line 198 to 203 and replace the .ncache section with the code below:   .npu_ncache (NOLOAD) :   {       KEEP(*(.npu_ncache_data))       KEEP(*(.npu_ncache_data*))   } > m_ncache   ASSERT(. < 0x20580000, "Error: .npu_ncache cannot go beyond SRAM P18")   .ncache (NOLOAD) :   {     *(NonCacheable)     . = ALIGN(4);     __noncachedata_end__ = .;     /* define a global symbol at ncache data end */   } > m_ncache       i.MX RT700 eIQ HiFi4 and HiFi1 projects cannot be imported or compiled in VSCode or command line GCC. In VSCode use the "Repository" import option. To compile the projects you must install Xtensa Xplorer, the RT700 license, and RT700 NewLib DSP Configuration file. Then add the following environmental variables: XCC_DIR=/<Xtensa Install Path>/XtDevTools/install/tools/RI-2023.11-win32/XtensaTools XTENSA_CORE=rt700_hifi4_RI23_11_nlib The project can then be compiled with command-line GCC with: west build -p always --sysbuild examples/eiq_examples/tflm_cifar10_hifi4/cm --toolchain armgcc --config flash_debug -b mimxrt700evk -Dcore_id=cm33_core0 Note that if using HiFi1 projects then XTENSA_CORE should be set to rt700_hifi1_RI23_11_nlib   Also an additional compile option called -mlongcalls needs to be used to avoid issues when adding additional operators the ops list. Inside \mcuxsdk\examples\_boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4\hifi4 edit the reconfig.cmake file in the mcux_add_xtensa_configuration options:   mcux_add_xtensa_configuration( CC "-DXOS_CLOCK_FREQ=237500000 -std=c99 -mlongcalls" CX "-stdlib=libc++ \ -mlongcalls \ -std=c++17" ) A warning message comes up in eIQ Neutron SDK 3.1.2 If using eIQ Neutron SDK 3.1.2 then the follow warning will appear on the serial terminal during the model initialization: Unable to save model handle, call neutronModelUnprepare() when done This warning is not relevant for Neutron C devices like RT700 and MCX N and can be ignored as it does not impact inference time or accuracy. It will be fixed in the next eIQ Neutron SDK release. Some eIQ files that are commonly modified are shared among all eIQ examples For example, the Neutron libraries are shared among all eIQ examples. This can cause version compatibility issues with the default eIQ examples if the eIQ Neutron libraries are updated with eIQ Neutron SDK. This is because the eIQ projects in MCUXPresso SDK were converted using Neutron Converter 3.0.0 and the Neutron libraries in the SDK are shared among all eIQ projects.  To work around this, either revert the Neutron libraries back to version 3.0.0 or else download a separate repository to use the default eIQ examples. 
View full article
This article describes the end-to-end procedure for booting a non-XIP application from SEMC parallel NAND flash on the MIMXRT1170-EVKB.
View full article
There are two important memory locations used during eIQ inferencing on microcontrollers: modeldata: Location of the model in memory. Can be located in RAM or Flash. Inference time will be faster if it is located in RAM. s_tensorArena: Memory area that is used for input, output, and intermediate arrays. Must be located in RAM. The MCUXpresso SDK eIQ projects create a s_tensorArena buffer that is placed in RAM and used by the model. In the MCUXpresso SDK projects, the default size for this buffer is 256 KB in size and the size is set by the kTensorArenaSize variable, which is declared in the model_data.h header file in the MCUXpresso SDK examples:   The s_tensorArena buffer is declared in the eIQ MCUXpresso SDK projects in the model.cpp file   Size of TensorArena for a model is based on the input, output, and scratch memory of the largest operator in the model:     It is estimated during Neutron Conversion in the last Total Data field. However it’s always slightly smaller than actual amount required.     The actual buffer size used is printed out during inference by using the s_interpreter- >arena_used_bytes(); API call after model initialization. This is automatically done in the MCUXpresso SDK eIQ examples:   Thus the tensorArena buffer size can be optimized in a project for the particular model by running the project at least once and then the kTensorArenaSize variable can be set to the actual used size as it will remain constant for a particular model. Buffer size requirements are model-specific and will depend on the structure and complexity of each model.   The TensorArena size required is often the same regardless of using the original unconverted model or a NPU converted model, but sometimes the NPU reduces the required size. And occasionally the buffer size must be larger for an NPU converted model so it is quite model dependent. Beyond the model inferencing specific memory requirements, there will also be RAM and Flash required for generating the input data for a model (camera, sensor, etc) and any output handling (LCD, notification, etc).  MCX N Specific Memory Details for Neutron NPU: By default the model is placed into the internal flash because in model_data.h it is declared with: static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {   By removing the const keyword, then the model will be placed into RAM during runtime and slightly improve the inference time. static uint8_t model_data[] __ALIGNED(16) __PLACEMENT = { As an example, doing this in the CIFAR10 MCUXpresso SDK example improves the inference time from 7.032ms to 5.524ms. Note that the kTensorArena variable must also be reduced from the default 256,000 bytes to 44,848 in order to fit in the internal RAM. The inference time improvement is model specific. However putting the model into RAM could not be done for the Label Image MCUXpresso SDK example because that model is too big and there is not enough RAM available for the model plus the tesnorArena buffer (which must be in internal RAM).  i.MX RT700 Specific Memory Details for Neutron NPU: See the i.MX RT700 eIQ Neutron NPU Enablement and Performance app note (AN14700) for more details about using eIQ Neutron NPU on i.MX RT700.  On i.MX RT700 the NPU has access to 5.5 MB of internal RAM from address 0x2000_0000 to 0x2058_0000 which consists of partitions SRAM P0 to SRAM P17. The model should be located inside this RAM area if it is placed in internal RAM. If using external memory, then the eIQ libraries will automatically copy the necessary model data to that internal memory location (see section below). The s_tensorArena buffer must also be within this 5.5MB RAM memory area. If the tensorArena buffer is located outside this 5.5MB area the model will still run but the inference results will be incorrect.      For i.MX RT700 eIQ projects, by default the model is placed at location 0x2040_0000 in RAM using the modeldata location name. For larger models, the RAM allocated by default in the eIQ SDK example projects for the s_tensorArena buffer or modeldata area may not be sufficient. In such case, the NCACHE_REGION size (where the s_tensorArena buffer is located) and modeldata size can be increased in the SDK project settings by modifying the linker file. The tensorArena buffer for RT700 internal memory models that use the NPU must also be in noncachable memory space. The model will still run if it is in cachable memory space but the results may be incorrect.  As a side note, for non-converted models that only run on the CM33 Core0 and do not use the NPU at all (mostly only done for benchmarking comparisons) then the tensorArena can be in cachable RAM and will see better performance if it's in that cachable RAM and is located between 0x2000_0000 and 0x2058_0000 since that RAM is the main System RAM for Core0.    i.MX RT700 eIQ Neutron NPU with External Memory For large models, or in cases where RAM is limited due to other uses in the application, the model can be stored in external flash memory via XSPI0. Placing the model in the external memory has an impact on performance, however. An example of this can be found in the tflm_label_image_ext_mem example in the MCUXpresso SDK where the model is at address 0x2820_0000. When the model is in external flash, then during inference a fragmented copy of the model is done to bring in chunks of the model into the internal RAM. This does have an impact on performance of the model and an example is given in the app note. Note: If placed in external memory then the --fetch_constants_to_sram option must be used during NPU conversion of the model to let the Neutron library know that it needs to do this fragmented copy during inference.      The scratch_weights buffer size required for this operation is printed out in the Scratch field during the model conversion when using the required --fetch-constants-to-sram argument:   And the scratchWeightsBuffer is created in the \eiq\tensorflow-lite\tensorflow\lite\micro\kernels\neutron\neutron.cpp file and the size can be modified by editing: #define SCRATCH_WEIGHTS_SRAM_SIZE  1200*1024 static uint8_t scratchWeightsBuffer[SCRATCH_WEIGHTS_SRAM_SIZE] __attribute__((aligned(16))) __attribute__((section("NonCacheable")));   If the scratch memory buffer size is too small for the model then there will not be an error message but the model output may be incorrect.  Also note that the Scratch Memory buffer is only needed when running a Neutron enabled model in external memory on i.MX RT700. If using a non-Neutron enabled model that only uses the CM33 core to run, then it is not needed. 
View full article
There are two new LCD panels that are now available for i.MX RT EVKs: The original RK043FN02H-CT panel is being replaced with the newer RK043FN66HS-CTG panel, which will affect the following EVKs: i.MX RT1050 i.MX RT1060 i.MX RT1064   The original RK055HDMIPI4M panel is being replaced with the newer RK055HDMIPI4MA0 panel, which will affect the following EVKs: i.MX RT595 i.MX RT1160 i.MX RT1170   These changes are due to the previous panels being EOL by the LCD panel manufacturer. These new LCDs have the same dimensions and screen size as their original versions (4.3” 480x272 and 5.5” 720x1280 respectively) and the physical connections are the same. The version name can be found on the back of the LCD. Some of these panels have multiple names that are used interchangeably across different documents.  The old i.MX RT1170 panel has multiple names and all these names refer to the exact same panel: RK055HDMIPI4M RK055AHD091 RK055AHD091‑CTG The new i.MX RT1170 panel has multiple names and all these names refer to the exact same panel: RK055HDMIPI4MA0 RK055MHD091 RK055MHD091-CTG RK055MHD091A0-CTG There are modifications to the software that may need to be made or else the LCD panel will be dark or blank when running MCUXpresso SDK demos on i.MXRT EVKs. This updated code is already available in the latest MCUXpresso SDK and SDK demos are configured by default to use the new panels.   For the i.MX RT1050/1060/1064 panel RK043FN66HS-CTG: The touch controller has changed and the SDK software has been modified to support the new touch controller. The LCD panel also has slightly different specs but the same code used for the original LCD panel will also work with the new LCD panel, so no change is necessary for display-only demos.  LCD demos are configured to support the new panel by default in the latest MCUXpresso SDK. So if you have the original panel you will need to change in the SDK code from      #define DEMO_PANEL  DEMO_PANEL_RK043FN66HS    //new panel (default SDK setting)           to       #define DEMO_PANEL  DEMO_PANEL_RK043FN02H     //older panel   For the i.MX RT595/RT1160/RT1170 panel RK055HDMIPI4MA0: Both the touch and display SDK software had to be updated to support this new panel. LCD demos are configured to support the new panel by default in the latest MCUXpresso SDK. So if you have the original panel you will need to change in the SDK code from:       #define DEMO_PANEL DEMO_PANEL_RK055MHD091    //new panel (default SDK setting)           to       #define DEMO_PANEL DEMO_PANEL_RK055AHD091    //older panel
View full article
This guide will walk through how to do connect the camera and LCD modules to i.MX RT boards and how to test to ensure the camera and LCD are connected properly. Update May 2022: There are now updated versions of these LCD panels that have an impact on software. See this post for more details. The physical connections are the same for both the original and new panels however so there are no changes to this guide.   This first part of this guide is for the i.MX RT1050, i.MX RT1060, i.MX RT1064 EVKs. The second part of this guide is for i.MX RT595, i.MX RT1160 and i.MX RT1170 EVKs.      Part 1: Camera and LCD for i.MX RT1050, i.MX RT1060, and i.MX RT1064:  The camera used by the RT1050, RT1060, and RT1064 EVKs are the same. However this camera only comes with the RT1060 and RT1064 EVKs. There are alternatives available for the RT1050 as discussed in this blog post.    The LCD screen compatible with these boards is the RK043FN66HS-CTG    Camera:  1) The camera connector is on the front of the board. Flip the black connector up so it's 90 degrees from its original position.  2) Then slide in the flat ribbon connector of the camera 3) Flip the black connector back down. It should keep the ribbon cable snug.   LCD: 1) On the back of the board, slide the black connector for the LCD ribbon forward. 2) Then slide in the flat LCD ribbon cable underneath the black connector. 3) Slide the black connector back to its original position. The cable should be snug. 4) Do the same for the touch controller connector and slide the black connector forward Then insert the cable between the black connector and the white top so that the cable is in the middle. It might take a few tries as its somewhat difficult. You could also use needle nose pliers to help guide in the cable but be careful about damaging the cable. 5) Then slide the black connector back to the original position. The cable should be snug. 6) It should look like the following when complete.   Testing: 1) To test the camera and LCD, use the CSI driver examples in the MCUXpresso SDK.  2) The camera will likely be out of focus the first time you use it. Adjust it by rotating the lens clockwise until the image is in focus. You can use your fingers or some needle nose pliers. It could take up to two rotations and it should turn easily. Also remove the plastic cover.    3) To test the touch controller, use the emwin temperature control example in the MCUXpresso SDK   Tape: 1) Once the LCD has been confirmed to work, you can use two layers of thick double sided foam tape to securely attach it to the board.      Part 2: Camera and LCD for i.MX 700, i.MX RT595, i.MX RT1160 and i.MX RT1170 EVKs:  The i.MX RT1160 and i.MX RT1170 EVKs both come with a OV5640 MIPI camera module in the box.    The LCD screen compatible with the i.MX RT1160, i.MX RT1170, i.MX RT595, and i.MX RT700 is the RK055HDMIPI4MA0 and it can be found here.  There are multiple alternative names for this panel and all these names refer to the exact same panel: RK055HDMIPI4MA0 RK055MHD091 RK055MHD091-CTG RK055MHD091A0-CTG   Instructions for i.MX RT1170 are below: i.MX RT1170-EVK Camera:  1) The camera connector is on the front of the board at J2. It connects by simply pressing the camera down onto the connector. It takes a bit of force but should not be too difficult.    i.MX RT1170-EVK LCD: 1) On the back of the board, slide the black connector (J40) for the LCD ribbon forward towards the edge of the board.    2) Then carefully slide in the flat LCD ribbon cable into the connector. The blue writing should be facing up like in the photo. It should go above the black part of the connector that you just slid out, and under the white part of the connector.  3) Slide the black plastic connector back to its original position. The cable should be snug if pulled. It should look like the following:    i.MX RT1170-EVK Power: 1) If using the LCD, then the external power adapter must be used with the board. Connect the barrel connector to J43 on the board. 2) Also change the jumper on J38 to be on pins 1-2 so that it uses the external power.  3) Connect a micro-USB cable to J11, which will cause the board to enumerate as a COM port and as a debug interface for downloading and debugging code   i.MX RT1170-EVK Camera and LCD Testing: 1) To test the camera and LCD, use the csi_mipi_rgb_cm7 driver example that can be found in the MCUXpresso SDK for i.MX RT1170. The camera input should be displayed on the LCD screen if everything is connected properly.          
View full article
There are two version of the i.MX RT1170 Evaluation Kit:  MIMXRT1170-EVK (no longer available for purchase) MIMXRT1170-EVKB   The key differences between the two versions of are laid out in the MIMXRT1170-EVKB Board Hardware User Guide:    One important change is the QuadSPI flash used on each board. This means that if you attempt to use SDK projects created for the RT1170-EVKB, it will not run properly on an older RT1170-EVK board due to using the mismatched QSPI configuration data. And new releases of MCUXpresso SDK only support the newer EVKB board.  However there is a simple fix to get those newer i.MX RT1170 EVKB MCUXpresso SDK projects to run on the older i.MX RT1170 EVK hardware. Simply download the MCUXpresso SDK 2.16.00 for the original RT1170-EVK board, unzip the archive file, and then copy the evkmimxrt1170_flexspi_nor_config.h and evkmimxrt1170_flexspi_nor_config.c files found in \SDK_2_16_000_MIMXRT1170-EVK\boards\evkmimxrt1170\xip into your EVKB project's xip folder. Then either delete/rename the EVKB version of the evkbmimxrt1170_flexspi_nor_config.c and evkbmimxrt1170_flexspi_nor_config.h files from the project to avoid compiler conflicts. This will update the QSPI configuration for that project to be compatible with the QSPI hardware on the original EVK. As an exmaple, here is the RT1170 Hello World project with that change - the EVKB files were renamed with a .orig extension so they would not be included in the compilation:    Note that due to the new hardware features found on the EVKB board there are some EVKB SDK projects that simply can't be supported on the original EVK board. But this work-around will provide support for many MCUXpresso SDK projects that don't require those new EVKB board features.    VSCode: For VSCode projects the repo\mimxrt1170_evkb\boards\xip\board_boot_header.make file will need to be modified to comment out the evkbmimxrt1170_flexspi_nor_config.c file and add the evkmimxrt1170_flexspi_nor_config.c   
View full article
目录 一、概述 二、环境准备   2.1 虚拟环境   2.2 使用Google Colab 三、核心步骤   3.1 CIFAR10数据集   3.2 模型创建   3.3 模型训练   3.4 模型转换   3.5 推理验证   3.6 benchmark性能   3.7 完整实现   3.7 简化版本(Colab) 四、TFLite Micro部署 五、快速验证 六、应用示例 七、结论 八、参考 more details, please see the attachment. 一、概述 CIFAR-10: 多伦多大学Alex Krizhevsky CIFAR-10公开数据集,也是计算机视觉领域最经典、最常用的入门级基准数据集之一,包含10个类别的6万张32x32彩色图像(5万训练,1万测试),例如飞机、汽车、鸟、猫等。 tflm_cifar10:演示了如何在恩智浦的微控制器上使用TensorFlow Lite Micro框架,实时运行CIFAR-10图像分类模型。即将一个预先训练好的、针对CIFAR-10数据集的卷积神经网络模型部署到MCU上,让其具备了识别10类常见物体(飞机、汽车、鸟、猫等)的能力。 模型:一个轻量级CNN模型,包含3个卷积层、ReLU激活层、池化层和一个全连接层。 输入: 32x32像素的彩色图像。 输出:图像属于CIFAR-10中10个类别的概率。 本文档:提供针对CIFAR10数据集搭建的完整流程,从数据集、模型训练转换、部署推理的快速实现方案,可作为示例tflm_cifar10(推理为主)的前置补充,本文不涉及到端侧的部署与优化。  ... """ CIFAR10 快速训练、测试、部署与推理完整流程 """ import os os.environ['TF_CPP_MIN_LOG_LEVEL'] = '2' # 减少TensorFlow日志 import tensorflow as tf import numpy as np import time import matplotlib.pyplot as plt print(f"TensorFlow版本: {tf.__version__}") print(f"NumPy版本: {np.__version__}") class CIFAR10QuickPipeline: def __init__(self): """初始化管道""" self.model = None self.tflite_model = None def load_data(self, sample_size=1000): """加载简化数据集""" print("\n1. 加载CIFAR10数据集...") (x_train, y_train), (x_test, y_test) = tf.keras.datasets.cifar10.load_data() # 预处理 x_train = x_train.astype('float32') / 255.0 x_test = x_test.astype('float32') / 255.0 # 使用少量数据(快速训练) x_train_small = x_train[:sample_size] y_train_small = y_train[:sample_size] x_test_small = x_test[:200] y_test_small = y_test[:200] # 转换为独热编码 y_train_onehot = tf.keras.utils.to_categorical(y_train_small, 10) y_test_onehot = tf.keras.utils.to_categorical(y_test_small, 10) print(f"训练数据: {x_train_small.shape}") print(f"测试数据: {x_test_small.shape}") return (x_train_small, y_train_onehot), (x_test_small, y_test_onehot) def create_simple_model(self): """创建简化CNN模型""" print("\n2. 创建简单CNN模型...") model = tf.keras.Sequential([ # 输入层 tf.keras.layers.Input(shape=(32, 32, 3)), # 卷积层1 tf.keras.layers.Conv2D(8, (3, 3), padding='same', activation='relu'), tf.keras.layers.MaxPooling2D((2, 2)), # 卷积层2 tf.keras.layers.Conv2D(16, (3, 3), padding='same', activation='relu'), tf.keras.layers.MaxPooling2D((2, 2)), # 全连接层 tf.keras.layers.Flatten(), tf.keras.layers.Dense(32, activation='relu'), tf.keras.layers.Dropout(0.2), tf.keras.layers.Dense(10, activation='softmax') ]) model.compile( optimizer='adam', loss='categorical_crossentropy', metrics=['accuracy'] ) model.summary() self.model = model return model def train_model(self, x_train, y_train, x_test, y_test, epochs=10): """训练模型""" print("\n3. 训练模型...") # 回调函数:早停 callbacks = [ tf.keras.callbacks.EarlyStopping( monitor='val_loss', patience=3, restore_best_weights=True ) ] history = self.model.fit( x_train, y_train, epochs=epochs, batch_size=32, validation_data=(x_test, y_test), callbacks=callbacks, verbose=1 ) # 评估模型 test_loss, test_acc = self.model.evaluate(x_test, y_test, verbose=0) print(f"\n测试准确率: {test_acc:.4f}") return history def convert_to_tflite(self): """转换为TFLite格式""" print("\n4. 转换为TFLite格式...") # 转换为TFLite converter = tf.lite.TFLiteConverter.from_keras_model(self.model) # 优化配置 converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.target_spec.supported_types = [tf.float32] # 转换 tflite_model = converter.convert() # 保存模型 with open('cifar10_model.tflite', 'wb') as f: f.write(tflite_model) # 保存为字节数组(用于嵌入式部署) self.save_as_c_array(tflite_model) self.tflite_model = tflite_model model_size = len(tflite_model) / 1024 print(f"模型大小: {model_size:.1f} KB") return tflite_model def save_as_c_array(self, tflite_model): """保存为C数组格式""" c_array = '// 自动生成的CIFAR10模型数组\n' c_array += '#include <stdint.h>\n\n' c_array += 'const unsigned char cifar10_model_tflite[] = {\n' # 每行显示12个字节 for i in range(0, len(tflite_model), 12): line_bytes = tflite_model[i:i+12] c_array += ' ' + ', '.join(f'0x{b:02x}' for b in line_bytes) + ',\n' c_array += '};\n\n' c_array += f'const unsigned int cifar10_model_tflite_len = {len(tflite_model)};\n' with open('cifar10_model_array.h', 'w') as f: f.write(c_array) print("C数组已保存: cifar10_model_array.h") def test_tflite_inference(self, x_test, y_test, num_tests=10): """测试TFLite推理""" print(f"\n5. 测试TFLite推理 ({num_tests}个样本)...") if self.tflite_model is None: with open('cifar10_model.tflite', 'rb') as f: self.tflite_model = f.read() # 加载TFLite模型 interpreter = tf.lite.Interpreter(model_content=self.tflite_model) interpreter.allocate_tensors() input_details = interpreter.get_input_details() output_details = interpreter.get_output_details() # 类别名称 class_names = ['飞机', '汽车', '鸟', '猫', '鹿', '狗', '青蛙', '马', '船', '卡车'] correct = 0 times = [] for i in range(min(num_tests, len(x_test))): # 准备输入 input_data = x_test[i:i+1] # 推理 start_time = time.perf_counter() interpreter.set_tensor(input_details[0]['index'], input_data) interpreter.invoke() inference_time = time.perf_counter() - start_time times.append(inference_time) # 获取输出 output = interpreter.get_tensor(output_details[0]['index']) predicted_class = np.argmax(output[0]) actual_class = np.argmax(y_test[i]) # 检查是否正确 if predicted_class == actual_class: correct += 1 print(f"样本 {i+1}: 预测={class_names[predicted_class]:<5} " f"实际={class_names[actual_class]:<5} " f"时间={inference_time*1000:.1f}ms " f"{'✓' if predicted_class == actual_class else '✗'}") accuracy = correct / num_tests avg_time = np.mean(times) * 1000 print(f"\n推理统计:") print(f" 准确率: {accuracy:.1%} ({correct}/{num_tests})") print(f" 平均推理时间: {avg_time:.1f}ms") print(f" 推理速度: {1000/avg_time:.0f} FPS") return accuracy, avg_time def benchmark_performance(self, x_test): """性能基准测试""" print("\n6. 性能基准测试...") interpreter = tf.lite.Interpreter(model_content=self.tflite_model) interpreter.allocate_tensors() input_details = interpreter.get_input_details() # 预热 test_input = x_test[0:1] for _ in range(10): interpreter.set_tensor(input_details[0]['index'], test_input) interpreter.invoke() # 基准测试 num_runs = 100 start_time = time.perf_counter() for _ in range(num_runs): interpreter.invoke() total_time = time.perf_counter() - start_time avg_time = total_time / num_runs * 1000 print(f"基准测试结果:") print(f" 总推理次数: {num_runs}") print(f" 总时间: {total_time*1000:.1f}ms") print(f" 平均推理时间: {avg_time:.1f}ms") print(f" 推理速度: {1000/avg_time:.0f} FPS") return avg_time def save_model_summary(self): """保存模型摘要""" summary = [] self.model.summary(print_fn=lambda x: summary.append(x)) with open('model_summary.txt', 'w') as f: f.write('\n'.join(summary)) f.write(f"\n\n模型信息:") f.write(f"\n参数数量: {self.model.count_params():,}") f.write(f"\n保存时间: {time.ctime()}") print("模型摘要已保存: model_summary.txt") def main(): """主函数""" print("=" * 60) print("CIFAR10 快速训练、测试、部署管道") print("=" * 60) # 创建管道 pipeline = CIFAR10QuickPipeline() # 1. 加载数据 (x_train, y_train), (x_test, y_test) = pipeline.load_data(sample_size=2000) # 2. 创建模型 pipeline.create_simple_model() # 3. 训练模型 history = pipeline.train_model(x_train, y_train, x_test, y_test, epochs=15) # 4. 保存模型摘要 pipeline.save_model_summary() # 5. 转换为TFLite pipeline.convert_to_tflite() # 6. 测试推理 pipeline.test_tflite_inference(x_test, y_test, num_tests=20) # 7. 性能测试 pipeline.benchmark_performance(x_test) print("\n" + "=" * 60) print("流程完成!生成的文件:") print(" 1. cifar10_model.tflite - TFLite模型") print(" 2. cifar10_model_array.h - C数组格式") print(" 3. model_summary.txt - 模型摘要") print("=" * 60) if __name__ == "__main__": main() ... 七、结论 本文旨在以常见图像分类场景(CIFAR10)为例,让读者快速了解从数据搭建、模型创建、训练、推理和验证的完整流程,可作为示例tflm_cifar10(端推理为主)的前置补充,本文不涉及到端侧部署与优化。
View full article
1 背景 2 开发搭建    2.1 软件    2.2 硬件 3 性能优化    3.1 原始性能    3.2 优化1:编译优化    3.3 优化2:外部SDRAM    3.4 优化3:VGLite加速    3.5 优化对比 4 结论 5 参考       1 背景 LVGL (Light and Versatile Graphics Library)是一款高性能、低资源占用的轻量级嵌入式图形库,凭借其强大的开源生态与广泛的操作系统适配支持,能够覆盖从低功耗的ARM Cortex-M系列微控制器(主频可低至100MHz)到运行Linux的高性能MPU等多种硬件平台,已成为嵌入式开源方案中的首选。许多芯片厂商已为其提供“开箱即用”级支持。 恩智浦(NXP)为其主流平台(如MCX、i.MX RT和LPC系列)提供了配套的软硬件示例,并在MCUXpresso SDK中集成了LVGL示例,这些示例对各类场景进行基准指标量化。然而,在实际应用中,因软、硬件配置与规格差异,性能表现往往存在波动,需结合具体场景进行针对性优化。 本文基于i.MX RT1170相关实践案例,旨在帮助NXP用户快速理解并选用适当的优化策略,以达成LVGL应用性能提升的目标。     4    结论 本文档针对NXP官方示例LVGL的 benchmark性能进行逐步优化,如CPU Usage, FPS, Render时间,Flush时间等,并提供了各个优化方案的量化数据对比以’Widgets demo’为例,其CPU使用率由原始的97%逐步降低至17%,而FPS帧率则由原始的2帧/秒提升至59帧/秒。 另外,这些优化方法和思路并不局限在该场景应用,对于常规的系统级的性能提升亦可作为参考。
View full article
  1 Background 2 Development Setup   2.1 Software   2.2 Hardware 3 Performance Optimization   3.1 Baseline Performance   3.2 Optimization 1: Compiler Optimization   3.3 Optimization 2: External SDRAM   3.4 Optimization 3: VGLite Acceleration   3.5 Optimization Comparison 4 Conclusion 5 References 1. Background LVGL (Light and Versatile Graphics Library) is a high-performance, low-resource embedded graphics library. Thanks to its robust open-source ecosystem and broad OS compatibility, it supports a wide range of hardware platforms—from low-power ARM Cortex-M microcontrollers (with clock speeds as low as 100 MHz) to high-performance MPUs running Linux—making it a preferred choice in embedded open-source solutions. Many silicon vendors now offer “out-of-the-box” support for LVGL.   NXP provides ready-to-use software and hardware examples for its mainstream platforms—including MCX, i.MX RT, and LPC series—and integrates LVGL examples into the MCUXpresso SDK. These examples include quantified benchmark metrics for various scenarios. However, due to differences in software/hardware configurations and specifications, actual performance may vary significantly and often requires scenario-specific tuning.   This document, based on practical experience with the i.MX RT1170 platform, aims to help NXP users quickly understand and apply appropriate optimization strategies to enhance LVGL application performance.         4. Conclusion This document presents a step-by-step optimization of NXP’s official LVGL benchmark example, with quantified improvements in CPU usage, FPS, render time, and flush time. Taking the Widgets demo as an example: CPU usage dropped from 96% → 12% FPS increased from 2 → 59 These optimization techniques—not limited to LVGL—are broadly applicable to system-level performance tuning on i.MX RT platforms.
View full article
This is a guide line to run both the master core and slave core projects as XIP targets from one flash.
View full article
4-TX Line Audio Playback via SAI1 on MIMXRT1170 and CS42448 1. Introduction This document focuses on utilizing the MIMXRT1170-EVKB development board and the CS42448 audio expansion board to achieve specific audio playback functionality through four TX data lines of the SAI1 module. With its real-time performance and high integration, the i.MX RT1170 is widely used in automotive, industrial, and IoT fields. The Arm Cortex-M7 core runs at up to 1GHz, features 2MB on-chip RAM, and offers various memory and connectivity interfaces. It supports multiple audio interfaces, including SAI-1, SAI-2, SAI-3, SAI-4, PDM, ASRC, SPDIF, and MQS. This document details the implementation of 8-channel audio output using the RT1170 EVKB development board and CS42448 Audio Card via four TX data lines of the SAI1 module. It also explains how to generate 8-channel audio data compatible with SDK example requirements. The CS42448 Audio Card can be directly connected to the RT1170 EVKB board, enabling developers to build more complex audio applications. The NXP SDK provides the example 'evkbmimxrt1170_sai_edma_multi_channel_transfer_cm7,' which by default enables two transmission channels (TX_DATA0 and TX_DATA1). When running, 1kHz sine wave audio signals can be heard from the J6 and J7 interfaces of the CS42448 Audio Card. However, when customer requirements demand four TX data lines (TX_DATA0 to TX_DATA3), each transmitting different audio, how can this be achieved? This document explores and validates this scenario in depth. 2. SAI Overview (1) RT1170 Chip SAI Module Features According to the IMXRT1170RM datasheet, SAI2, SAI3, and SAI4 modules each have only one data line for input/output, while SAI1 has four, making it the only module supporting multi-line communication. (2) Configuration Highlights To implement the four TX data line solution, it is crucial to configure the Transmit Configuration 3 (TCR3) TCE register correctly. According to IMXRT1170RM Table 54-2, Option0 should be selected for pin configuration. To enable TX_DATA0 to TX_DATA3, set bits 16–19 of the SAI1 TCR3 register to '1111'. Similarly, for multiple Rx data lines, configure bits 16–19 of the SAI1 RCR3 register (RCE).   3. Hardware Preparation (1) Required Hardware - Mini/micro USB cable - MIMXRT1170-EVKB development board - Personal computer - Headphones (OMTP standard) - CS42448 Audio Card (2) Hardware Modifications on MIMXRT1170-EVKB Solder Resistors: R2008, R2022, R2011, R2021, R2009, R2010, R2012, R2016, R1998, R2013, R2014, R2018, R2017, R2000 Remove Resistors: R2001, R2002, R2003, R2004, R2005, R2006, R2007 After completing the hardware modifications, connect the CS42448 Audio Card to the J76 interface of the MIMXRT1170-EVKB board. 4. Audio Source Preparation The free and powerful audio editing software Audacity is used to convert MP3 files to .wav format. Since each TX data line transmits two audio channels, a total of 8 channels are needed. (1) Audio Channel Allocation Strategy Using Audacity, multiple audio channels were generated. 'HelloWorld' is mono and reused. Allocation is as follows: - TX_DATA0: HelloWorld → Channel 1 & Channel 5 - TX_DATA1: Audio1 → Left: Channel 2, Right: Channel 6 - TX_DATA2: Audio2 → Left: Channel 3, Right: Channel 7 - TX_DATA3: Audio3 → Left: Channel 4, Right: Channel 8 On the CS42448 Audio Card: - J6 plays TX_DATA0 (HelloWorld) - J7 plays  TX_DATA1(Audio1) - J8 plays TX_DATA2(Audio2) - J9 plays TX_DATA3(Audio3) (2) Audio Format Requirements The converted .wav files must match the format used in the NXP SDK example: 48kHz sampling rate and 16-bit width. Ensure these parameters are correctly set in Audacity during conversion. (3) Audio Data Processing To convert the generated HelloWorld-8-channel.wav file into a C language array using WinHex, you need to remove the first 44 bytes, which constitute the standard WAV file header. This step is crucial because the SDK example utilizes raw audio data. For those interested, examining the structure of a WAV file can provide deeper insight into this process. Alternatively, this conversion from WAV format to a C array can also be accomplished using other tools or methods. 5. Software Modifications (1) Configure SAI1 Module Registers To enable four TX data lines, set the TCE bits in the SAI1 TCR3 register. In the NXP SDK code, modify the macro DEMO_SAI_CHANNEL_MASK and configure saiConfig in I2S mode. The function SAI_TransferSendEDMA will set the TCR3 TCE register accordingly. (2) Replace Audio Data and Modify Macros Replace the uint8_t music[] array in the SDK example’s music.h file with the C array generated earlier. Also, update the macro MUSIC_LEN to match the byte length of the new array, ensuring it is a multiple of 1600. After completing all steps, compile and flash the program to the MIMXRT1170-EVKB board. Connect headphones to the CS42448 Audio Card’s J6,J7,J8,J9 interfaces to hear the respective audio outputs.   6. Conclusion This project successfully implements the transmission of four TX data lines via the SAI1 module using the CS42448 Audio Card and MIMXRT1170-EVKB development board. Experimental validation confirms support for multi-channel independent audio output. Each TX data line can output distinct audio content through the CS42448’s physical interfaces (J6–J9), meeting the needs of complex audio scenarios.
View full article