Step-by-Step Guide to Running the GenAVB/TSN Stack FreeRTOS Evaluation Use Case on i.MX RT1180

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Step-by-Step Guide to Running the GenAVB/TSN Stack FreeRTOS Evaluation Use Case on i.MX RT1180

Step-by-Step Guide to Running the GenAVB/TSN Stack FreeRTOS Evaluation Use Case on i.MX RT1180

1. Abstract

The GenAVB/TSN Stack FreeRTOS Evaluation User's Guide (version:8.0 Release) covers multiple hardware platforms, software configurations, and evaluation use cases. While comprehensive, the document can be challenging for first-time users to follow due to the large amount of information and the variety of supported scenarios.

This article focuses on a specific use case from the User's Guide and provides a detailed, step-by-step walkthrough with screenshots, configuration examples, expected results, and troubleshooting tips. The goal is to help users better understand the setup process and successfully evaluate the GenAVB/TSN stack on NXP platforms.

This article walks through Section 4.4, TSN Network Only with TSN Bridge and Standalone Endpoint i.MX RT1180, from the GenAVB/TSN Stack FreeRTOS Evaluation User's Guide. It explains the required hardware setup, firmware build and flashing procedure, board configuration, TSN configuration, execution steps, expected results, and basic troubleshooting tips.

2. Setup

2.1 Hardware Preparation

  • Two i.MX RT1180 boards
  • A PC with a serial terminal emulator. MobaXterm Portable is recommended.
  • At least two USB cables and three Ethernet cables
ShellyZhang_0-1783325043864.jpeg

 

2.2 Firmware Preparation

2.2.1 Setup IDE and SDK

Refer to the NXP GenAVB/TSN MCUXpresso User's Guide to install the required software environment for the selected platform and project. A successful project build confirms that the build environment has been installed and configured correctly.

VS Code and MCUXpresso for Visual Studio Code are recommended.

2.2.2 Build Image

Note:  The specific operating procedures should still be based on GenAVB/TSN MCUXpresso User's Guide . The explanation below is intended only as a supplement to the original document.

For GenAVB_TSN-rtos-apps version 8.0, the CM7 Kconfig file needs to be fixed manually before building the image.

Kconfig file path:

ShellyZhang_0-1783326438663.png

 

Add two lines like the following:

ShellyZhang_2-1783325043922.png

Set the Build Configurations of the CM33 project to release_no_enetc0, and then build the project.

ShellyZhang_3-1783325043942.png

Set the Build Configurations of the CM7 project to release_enetc0, and then build the project.

ShellyZhang_4-1783325043961.png

Note: If you are using MCUXpresso for VS Code, you may not be able to import both the CM33 and CM7 projects of the TSN application into the same workspace at the same time, like the following:

ShellyZhang_5-1783325044093.png

If this occurs, remove the existing project from the workspace before importing the project for the other core. This issue is expected to be fixed in a future release.

ShellyZhang_6-1783325044123.png

After both the CM33 and CM7 projects are built successfully, the generated .bin files and .elf files can be found in the corresponding output directories:

ShellyZhang_7-1783325044157.png
ShellyZhang_8-1783325044188.png

 

2.2.3 Flash Image

Make sure the board's boot configuration switch is set to Serial Downloader mode. For SDP mode, SW5[1..4] should be set to 0001.

Set jumper J1 to position 7–8 so that the evaluation board can be powered through the Debug USB port.

Connect one USB cable between the PC and the USB_OTG1 port , which is used for firmware downloading.

Connect another USB cable between the PC and the Debug USB port, which is used for power supply and serial communication.

Then reset the board.

Refer to Chapter 10, "Multi core (Cortex-M33 + Cortex-M7) images flashing" in the GenAVB/TSN MCUXpresso User's Guide. Flash the following generated binaries to the target device:

  • genavb_tsn_rtos_apps\...\release_no_enetc0\evkmimxrt1180_tsn_app_cm33_cm33.bin
  • genavb_tsn_rtos_apps\...\release_enetc0\evkmimxrt1180_tsn_app_cm7_cm7.bin

2.3 Check the Status of the Boards

After the flashing operation is completed on both boards, restore the boot configuration switch on each board to Quad SPI mode. For QSPI mode, SW5[1..4] should be set to 0100. Then reset both boards.

Remove the jumper on JP7 so that the debug port on each board can enumerate two serial ports. The CM33 and CM7 serial terminal interfaces are provided through the two serial ports enumerated by the debug port.

After the boards restart, the red LED D7 should blink, indicating that the TSN application is running.

Then, check the hardware connection:

ShellyZhang_14-1783325045000.png

 

ShellyZhang_15-1783325045041.jpeg

 

2.4 TSN Configuration and Evaluation

 

i.MX RT1180 Controller

i.MX RT1180 IO Device 1

Step 1.

Configure the Controller Standalone TSN Endpoint

and

IO Device Standalone TSN Endpoint

respectively.

CM33 shell:
Press INSERT key


mkdir -p /m7/tsn_app
write /m7/boot 1
write /m7/tsn_app/role 0
write /m7/tsn_app/mode 2
write /m7/tsn_app/port_id 1
write /m7/tsn_app/num_io_devices 1
write /m7/tsn_app/period_ns 250000

CM33 shell:
Press INSERT key


mkdir -p /m7/tsn_app
write /m7/boot 1
write /m7/tsn_app/role 1
write /m7/tsn_app/mode 2
write /m7/tsn_app/port_id 1
write /m7/tsn_app/period_ns 250000

 

Step 2. Reset the boards

Reset

Reset

Step 3. Set hardware address

CM33 shell:

mkdir -p port0

mkdir -p port1

mkdir -p port2

mkdir -p port3

mkdir -p port4

mkdir -p port5

write port0/hw_addr 54:27:8D:00:00:00

write port1/hw_addr 54:27:8D:00:00:01

write port2/hw_addr 54:27:8D:00:00:02

write port3/hw_addr 54:27:8D:00:00:03

write port4/hw_addr 54:27:8D:00:00:04

write port5/hw_addr 54:27:8D:00:00:05

CM33 shell:

mkdir -p port0

mkdir -p port1

mkdir -p port2

mkdir -p port3

mkdir -p port4

mkdir -p port5

write port0/hw_addr 54:27:8D:00:01:00

write port1/hw_addr 54:27:8D:00:01:01

write port2/hw_addr 54:27:8D:00:01:02

write port3/hw_addr 54:27:8D:00:01:03

write port4/hw_addr 54:27:8D:00:01:04

write port5/hw_addr 54:27:8D:00:01:05

Step 4. Set gPTP

/ (Devices without this command configured remain GM devices.)

 

CM33 shell:

mkdir -p fgptp

write fgptp/priority1 248

 

Step 5. VLAN and FDB entry settings

BRIDGE>> vlan_update 2 3 -c 1 -p

BRIDGE>> vlan_update 2 4 -c 1 -p

BRIDGE>> fdb_update 91:e0:f0:00:fe:70 2 4 -c 1 -p

BRIDGE>> fdb_update 91:e0:f0:00:fe:71 2 3 -c 1 -p

/

 

Step 6. Scheduled Traffic settings

CM33 shell:

 

BRIDGE>> cd /

BRIDGE>> qbv_set 4 -b 35000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p

BRIDGE>> qbv_set 3 -b 160000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p

 

CM7 shell:

 

CONTROLLER>> qbv_set 1 -b 35000 -c 250000 -C 0 -l 02,80000 -l fd,170000

CM7 shell:

 

IO_DEVICE_0>> qbv_set 1 -b 160000 -c 250000 -C 0 -l 02,80000 -l fd,170000

Step 7. Reset the boards and evaluate Scheduled Traffic

/

ShellyZhang_16-1783325045104.png

 

Step 8. Configure Time-Specific Departure (TSD)

CM33 shell:

Press INSERT key

 

write /m7/tsn_app/tx_time_enabled 1

write /m7/tsn_app/tx_time_offset_ns 38000

CM33 shell:

Press INSERT key

 

write /m7/tsn_app/tx_time_enabled 1

write /m7/tsn_app/tx_time_offset_ns 38000

Step 9. Reset the boards and evaluate Time-Specific Departure (TSD)

/

ShellyZhang_17-1783325045170.png

 

Note: All use cases require the hardware address and gPTP configurations. The original User's Guide does not fully describe this part, so these steps are explicitly included in this article for clarity.

3. Conclusion

This guide summarizes the complete workflow for evaluating the GenAVB/TSN Stack FreeRTOS use case on the i.MX RT1180 platform. It covers the required hardware preparation, firmware build process, image flashing procedure, board boot configuration, serial port verification, and TSN configuration steps.

By following the configuration sequence in this document, users can set up the Controller and IO Device roles, configure gPTP, VLAN, FDB entries, Scheduled Traffic, and Time-Specific Departure, and then verify the expected TSN behavior between the two i.MX RT1180 boards.

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎07-06-2026 07:01 PM
更新者: