rt1170 jlink issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,728件の閲覧回数
sukyeong
Contributor III

MCU : IMXRT1170-EVB

J-LINK , i want to use JTAG mode

swd mode works fine, but jtag mode is error.

I've referred to the posts below, but it doesn't work out.

help me please

 

https://community.nxp.com/t5/i-MX-RT/RT1176-connect-to-JLINK-with-a-warning/m-p/1599341

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1160-EVK-or-MIMXRT1170-E...

 

sukyeong_0-1686792722753.png

1. i try j6,j7 jumper remove

2. Is there anything in the circuit that needs to be changed?

sukyeong_1-1686792812321.png

sukyeong_2-1686792840297.png

 

0 件の賞賛
返信
1 解決策
7,643件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing

元の投稿で解決策を見る

7 返答(返信)
7,702件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

Please try to remove R2152 and  R2038.

 

Regards,

Jing

0 件の賞賛
返信
7,698件の閲覧回数
sukyeong
Contributor III

R2152, R2038을 찾을 수 없습니다..
자세한 내용을 알려주실 수 있나요?

 

@jingpan 

タグ(1)
0 件の賞賛
返信
7,674件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

You can search to this doc.

0 件の賞賛
返信
7,664件の閲覧回数
sukyeong
Contributor III
0 件の賞賛
返信
7,661件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

What is your board, EVK or EVKB?

 

Regards,

Jing

0 件の賞賛
返信
7,655件の閲覧回数
sukyeong
Contributor III
My board is EVK.
sorry for the confusion
@jingpan
0 件の賞賛
返信
7,644件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing