low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

跳至解决方案
1,356 次查看
roidimor
Contributor I

hey,

i am running yocto's fsl-image-clutter image on boundary devices Nitrogen6x.

i have written a simple Clutter application which draws a few rectanlges on the screen, and when i'm running it, it seems like the performance is extremely low. when running the application with the --clutter-show-fps flag it says the application is running on 1-3 fps.

lsmod mod doesn't list vivante's gpu drivers and 'modprobe galcore' doesn't seem to be doing anything. am i missing something? should i load the drivers or do something else in a different way?

any help would be appreciated!

thanks,

roi.

标记 (4)
0 项奖励
回复
1 解答
1,108 次查看
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,109 次查看
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

0 项奖励
回复