low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

Jump to solution
1,363 Views
roidimor
Contributor I

hey,

i am running yocto's fsl-image-clutter image on boundary devices Nitrogen6x.

i have written a simple Clutter application which draws a few rectanlges on the screen, and when i'm running it, it seems like the performance is extremely low. when running the application with the --clutter-show-fps flag it says the application is running on 1-3 fps.

lsmod mod doesn't list vivante's gpu drivers and 'modprobe galcore' doesn't seem to be doing anything. am i missing something? should i load the drivers or do something else in a different way?

any help would be appreciated!

thanks,

roi.

0 Kudos
Reply
1 Solution
1,115 Views
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

View solution in original post

0 Kudos
Reply
1 Reply
1,116 Views
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

0 Kudos
Reply