low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

low performance with Clutter on yocto's fsl-image-clutter (Nitrogen6x)

ソリューションへジャンプ
1,383件の閲覧回数
roidimor
Contributor I

hey,

i am running yocto's fsl-image-clutter image on boundary devices Nitrogen6x.

i have written a simple Clutter application which draws a few rectanlges on the screen, and when i'm running it, it seems like the performance is extremely low. when running the application with the --clutter-show-fps flag it says the application is running on 1-3 fps.

lsmod mod doesn't list vivante's gpu drivers and 'modprobe galcore' doesn't seem to be doing anything. am i missing something? should i load the drivers or do something else in a different way?

any help would be appreciated!

thanks,

roi.

ラベル(4)
タグ(4)
0 件の賞賛
返信
1 解決策
1,135件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,136件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please post this to meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenGLES could try to assist you.

0 件の賞賛
返信