Hi, we are using i.MX8M Nano with U-Boot 2020.04 and our design is custom but based on DDR4 Audio board 2.0.
Our QSPI NOR flash is a n25q512a from Micron and is supported by U-Boot in general.
So far everything looks ok except that we can not properly access addresses beyond the lower 32 Megabytes (so >0x02000000).
When we boot from SPI flash and try to access the higher addresses, we run into a reset.
When we boot from USB (using uuu), we do not get a reset but the content of those upper 32 Megabytes is rubbish.
Using Linux we can access the entire flash range without restrictions.
It seems there is a limitation (e.g. memory mapping) for iMX8MN and U-Boot accessing addresses >32MiB on SPI NOR flashes.
Does anybody know a reason ?
已解决! 转到解答。
Hi,
I found the issue - the flash size is not taken from the SPI NOR ID table but has to be defined separately inside imx8mn_ab2.h which is of course not very nice but looks like solves my issue.
Regards,
Sebastian
Hi Sebastian
for that issue one can try to enable 4-byte address mode (3-byte is used by default)
which can be enabled through the nonvolatile configuration register. Details can be found
in n25q512a datasheet.
Best regards
igor
Hi Igor,
thanks for your reply.
I assume we are already using 4-Byte addressing because we can access addresses >16MiB (which exceeds 3-Byte address range).
I suspect the issue is more related to mapping the QSPI flash addresses to the memory range of the iMX8MN.
Regards,
Sebastian
Hi,
I found the issue - the flash size is not taken from the SPI NOR ID table but has to be defined separately inside imx8mn_ab2.h which is of course not very nice but looks like solves my issue.
Regards,
Sebastian