NNAPI: using a delegate that only supports static-sized tensors with a graph that has dynamic tensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NNAPI: using a delegate that only supports static-sized tensors with a graph that has dynamic tensor

4,408件の閲覧回数
jasonliu1
Contributor I

Hi, 

I started training a fpn-ssd-mobilenetv2 model(which is one of the base models provided by the eIQ software) using custom dataset on the software recently. However, when I converted it into a tflite model and implemented it on a board with NNAPI delegate, it tells me that I'm "attempting to use a delegate that only supports static-sized tensors with a graph that has dynamic-sized tensors" and it failed to apply NNAPI delegate.  

I was just wondering what is the cause of this problem and what should I do to avoid it?

Thanks very much!

ラベル(1)
0 件の賞賛
返信
1 返信

4,368件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jasonliu1,

One possible reason here is that when you use eIQ software to convert the custom model, you choose MLIR as tflite converter. I will recommend to use TOCO instead and see whether this problem is avoided. Thank you.

 

0 件の賞賛
返信