iMX6 stress tester v2.70 stress test fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 stress tester v2.70 stress test fails

ソリューションへジャンプ
2,404件の閲覧回数
pranavparmar
Contributor III

Hi LinWang‌,

As discussed in the calibration failure post i.MX6 DDR Stress Test Tool V2.70 calibration fails. I tried running the stress test. I got the following results:

============================================
DDR Stress Test (2.6.0)
Build: Aug 1 2017, 17:33:25
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO1.2
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000000
SRC_SBMR2(0x020d801c) = 0x21000001
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================


DDR Stress Test Iteration 1
Current Temperature: 40
============================================

DDR Freq: 0 MHz
t0.1: data is addr test
Address of failure(step2): 0x10002000
Data was: 0x10000000
But pattern should match address
Error: failed to run stress test!!!

1.png

2.png

Here as per the test result the data should be 0x10000000 which is same written at the address 0x10002000.

Can you please describe the failure reason at 0x10002000?

ラベル(2)
1 解決策
1,920件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please verify board : if  data bit 0x2000 is short-circuited with other signal.

  Also,  the following may be helpful.

DDR stress test error 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,921件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please verify board : if  data bit 0x2000 is short-circuited with other signal.

  Also,  the following may be helpful.

DDR stress test error 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,920件の閲覧回数
pranavparmar
Contributor III

Hi YuriMuhin_ng

I populated the new board and the stress test is successful. But still u-boot is not booting. 

0 件の賞賛
返信
1,920件の閲覧回数
pranavparmar
Contributor III

Problem solved. I have configured wrong uart.