iMX6 PCIe capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,086件の閲覧回数
torus1000
Contributor V

Hi guys.


I'm not familiar with i.MX6 PCIe and I want to know several things as following.

* How many virtual channels(VC) can be handle by PCIe?

* Is there any possibility to occur cache incoherence when PCIe access to DRAM?

If someone knows, please let me know.

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,849件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

there are 8 VC [in particular sect.48.9.22 VCn.. IMX6DQRM points on this].

Regarding "possibility to occur cache incoherence" I think

no, because PCIe is serviced by arm core, it has not own DMA engine.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,850件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

there are 8 VC [in particular sect.48.9.22 VCn.. IMX6DQRM points on this].

Regarding "possibility to occur cache incoherence" I think

no, because PCIe is serviced by arm core, it has not own DMA engine.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信