iMX6 PCIe capability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 PCIe capability

Jump to solution
2,111 Views
torus1000
Contributor V

Hi guys.


I'm not familiar with i.MX6 PCIe and I want to know several things as following.

* How many virtual channels(VC) can be handle by PCIe?

* Is there any possibility to occur cache incoherence when PCIe access to DRAM?

If someone knows, please let me know.

Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,874 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

there are 8 VC [in particular sect.48.9.22 VCn.. IMX6DQRM points on this].

Regarding "possibility to occur cache incoherence" I think

no, because PCIe is serviced by arm core, it has not own DMA engine.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,875 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

there are 8 VC [in particular sect.48.9.22 VCn.. IMX6DQRM points on this].

Regarding "possibility to occur cache incoherence" I think

no, because PCIe is serviced by arm core, it has not own DMA engine.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply