iMX280 : Input leakage Current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX280 : Input leakage Current

跳至解决方案
1,759 次查看
koichisakagami
Contributor II

Dear community,

I checked the i.MX28 Data Sheet (IMX23CEC Rev3) .
However, I can not find an Input leakage Current value .

How much is the Input leakage Current value ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,667 次查看
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,668 次查看
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复