iMX280 : Input leakage Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX280 : Input leakage Current

ソリューションへジャンプ
1,746件の閲覧回数
koichisakagami
Contributor II

Dear community,

I checked the i.MX28 Data Sheet (IMX23CEC Rev3) .
However, I can not find an Input leakage Current value .

How much is the Input leakage Current value ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,654件の閲覧回数
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,655件の閲覧回数
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信