iMX280 : Input leakage Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX280 : Input leakage Current

Jump to solution
1,760 Views
koichisakagami
Contributor II

Dear community,

I checked the i.MX28 Data Sheet (IMX23CEC Rev3) .
However, I can not find an Input leakage Current value .

How much is the Input leakage Current value ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,668 Views
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,669 Views
art
NXP Employee
NXP Employee

The input leakage current of typical i.MX28 GPIO cell itself (configured as input) is very low, only some units of nanoamperes. However, an internal pullup resistor can be enabled on most of I/O cells. In that case, the input current depends on input voltage. The pullup resistor value is 47kOhm or 10kOhm depending on pin, please refer to the Table 9-3 of the i.MX28 Reference Manual Rev.2 document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply