About the KITPF0100EPEVBE: Evaluation Kit - MMPF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the KITPF0100EPEVBE: Evaluation Kit - MMPF0100

Jump to solution
656 Views
patcharasirigul
Contributor II

Hello everyone,

I bought the KITPF0100EPEVBE: Evaluation Kit - MMPF0100 for developing project. My problem is when I try to follow the KTP0100UG document in page 8. I can not find the NI-VISA 5.1.2 for installing. I used NI-VISA 14.01 replaced NI-VISA 5.1.2.

NI-VISA 14.01, It's ok?  I use win7-64 bit.

When I installed NI-VISA 14.01 already. I follow in page 9 -12 on the KTP0100UG document. I think the result should be same page 13, but It found the device is USB Input Device in Human Interface Devices.


I can connect with KTPGUI_4.0 only, which I would like to connect with KTP0100GUI.


And when I try to setup the KTP0100GUI, It shows "Application cannot be started. Contact the application vendor.


Please help me


Thank you so much.

0 Kudos
Reply
1 Solution
524 Views
art
NXP Employee
NXP Employee

The KTPF0100GUI software package is some early one, and it may not work correctly under Windows 7. Please use the latest KITPFGUI_4.0 software package:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITPF0100EPEVBE&fpsp=1&tab=Design_Too...

and refer to the KTPFSWUG4 document for instructions:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITPF0100EPEVBE&fpsp=1&tab=Documentat...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
525 Views
art
NXP Employee
NXP Employee

The KTPF0100GUI software package is some early one, and it may not work correctly under Windows 7. Please use the latest KITPFGUI_4.0 software package:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITPF0100EPEVBE&fpsp=1&tab=Design_Too...

and refer to the KTPFSWUG4 document for instructions:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITPF0100EPEVBE&fpsp=1&tab=Documentat...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply