i.MX8QM MIPI CSI2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM MIPI CSI2

Jump to solution
1,454 Views
xu_ji1
Contributor V

Hi,

I want to know does i.MX8QM MIPI lanes data rate support four 1080P@30fps camera sensors with one deserializer

out to i.MX8QM?

What is the max MIPI data rate (Gbps?)with i.MX8QM 4lanes? 

Thanks

0 Kudos
Reply
1 Solution
1,416 Views
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

View solution in original post

0 Kudos
Reply
3 Replies
1,416 Views
art
NXP Employee
NXP Employee

The maximum data rate, supported on the MIPI CSI2 interfaces of the i.MX8QM processor, is 1.5Gbps per lane or 6Gbps on 4 lanes.

Best Regards,
Artur

0 Kudos
Reply
1,416 Views
xu_ji1
Contributor V

Does 4 lanes support 4X1920X1080@30fps  output data?

0 Kudos
Reply
1,417 Views
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

0 Kudos
Reply