i.MX8QM MIPI CSI2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8QM MIPI CSI2

跳至解决方案
1,453 次查看
xu_ji1
Contributor V

Hi,

I want to know does i.MX8QM MIPI lanes data rate support four 1080P@30fps camera sensors with one deserializer

out to i.MX8QM?

What is the max MIPI data rate (Gbps?)with i.MX8QM 4lanes? 

Thanks

0 项奖励
回复
1 解答
1,415 次查看
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,415 次查看
art
NXP Employee
NXP Employee

The maximum data rate, supported on the MIPI CSI2 interfaces of the i.MX8QM processor, is 1.5Gbps per lane or 6Gbps on 4 lanes.

Best Regards,
Artur

0 项奖励
回复
1,415 次查看
xu_ji1
Contributor V

Does 4 lanes support 4X1920X1080@30fps  output data?

0 项奖励
回复
1,416 次查看
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

0 项奖励
回复