i.MX8QM MIPI CSI2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,449件の閲覧回数
xu_ji1
Contributor V

Hi,

I want to know does i.MX8QM MIPI lanes data rate support four 1080P@30fps camera sensors with one deserializer

out to i.MX8QM?

What is the max MIPI data rate (Gbps?)with i.MX8QM 4lanes? 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,411件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,411件の閲覧回数
art
NXP Employee
NXP Employee

The maximum data rate, supported on the MIPI CSI2 interfaces of the i.MX8QM processor, is 1.5Gbps per lane or 6Gbps on 4 lanes.

Best Regards,
Artur

0 件の賞賛
返信
1,411件の閲覧回数
xu_ji1
Contributor V

Does 4 lanes support 4X1920X1080@30fps  output data?

0 件の賞賛
返信
1,412件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the MIPI CSI2 interface can support the 4X1920X1080@30fps data on 4 lanes.

0 件の賞賛
返信