i.MX8M mini TMU SW calibration code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M mini TMU SW calibration code

Jump to solution
2,175 Views
Tori-san
Contributor III
Hello, Is imx8mm_thermal.c the code to perform SW calibration? Current version is "imx_5.4.70_2.3.0", but are there any plans to update it for TMU SW calibration?
0 Kudos
Reply
1 Solution
2,167 Views
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  Generally the calibration points are measured during the manufacturing testing,
and are programmed in the fuse registers - no need for customers to implement
the calibration.

Regards,
Yuri.

View solution in original post

2 Replies
2,168 Views
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  Generally the calibration points are measured during the manufacturing testing,
and are programmed in the fuse registers - no need for customers to implement
the calibration.

Regards,
Yuri.

2,153 Views
Tori-san
Contributor III
Hi Yuri, Thank you for your reply. I interpret that I don't need to calibrate with the default setting. However, if more accurate calibration is required, it should be implemented in the driver(imx8mm_thermal.c) using the equation desribed in RM. Best regards, Tori-san.